BLE Secure#

This module includes functions that control BLE Secure (TLS over BLE) communication.

This module includes functions that implement TCAT communication.

The functions in this module are available when BLE Secure API feature (OPENTHREAD_CONFIG_BLE_TCAT_ENABLE) is enabled.

The functions in this module are available when TCAT feature (OPENTHREAD_CONFIG_BLE_TCAT_ENABLE) is enabled.

Modules#

otTcatAdvertisedDeviceId

otTcatGeneralDeviceId

otTcatVendorInfo

Enumerations#

enum
OT_TCAT_STATUS_SUCCESS = 0
OT_TCAT_STATUS_UNSUPPORTED = 1
OT_TCAT_STATUS_PARSE_ERROR = 2
OT_TCAT_STATUS_VALUE_ERROR = 3
OT_TCAT_STATUS_GENERAL_ERROR = 4
OT_TCAT_STATUS_BUSY = 5
OT_TCAT_STATUS_UNDEFINED = 6
OT_TCAT_STATUS_HASH_ERROR = 7
OT_TCAT_STATUS_UNAUTHORIZED = 16
}

Represents TCAT status code.

enum
OT_TCAT_APPLICATION_PROTOCOL_NONE = 0
OT_TCAT_APPLICATION_PROTOCOL_STATUS = 1
OT_TCAT_APPLICATION_PROTOCOL_TCP = 2
}

Represents TCAT application protocol.

enum
OT_TCAT_COMMAND_CLASS_GENERAL = 0
OT_TCAT_COMMAND_CLASS_COMMISSIONING = 1
OT_TCAT_COMMAND_CLASS_EXTRACTION = 2
OT_TCAT_COMMAND_CLASS_DECOMMISSIONING = 3
OT_TCAT_COMMAND_CLASS_APPLICATION = 4
}

Represents a TCAT command class.

enum
OT_TCAT_DEVICE_ID_EMPTY = 0
OT_TCAT_DEVICE_ID_OUI24 = 1
OT_TCAT_DEVICE_ID_OUI36 = 2
OT_TCAT_DEVICE_ID_DISCRIMINATOR = 3
OT_TCAT_DEVICE_ID_IANAPEN = 4
OT_TCAT_DEVICE_ID_MAX = 5
}

Represents Advertised Device ID type.

Typedefs#

typedef void(*
otHandleBleSecureConnect)(otInstance *aInstance, bool aConnected, bool aBleConnectionOpen, void *aContext)

Pointer to call when ble secure connection state changes.

Pointer to call when data was received over a BLE Secure TLS connection.

typedef enum otTcatStatusCode

Represents TCAT status code.

Represents TCAT application protocol.

typedef enum otTcatCommandClass

Represents a TCAT command class.

Represents Advertised Device ID type.

typedef struct otTcatGeneralDeviceId

Represents General Device ID type.

typedef struct otTcatVendorInfo

This structure represents a TCAT vendor information.

typedef void(*
otHandleTcatApplicationDataReceive)(otInstance *aInstance, const otMessage *aMessage, int32_t aOffset, otTcatApplicationProtocol aTcatApplicationProtocol, const char *aServiceName, void *aContext)

Pointer to call when application data was received over a TCAT TLS connection.

typedef void(*
otHandleTcatJoin)(otError aError, void *aContext)

Pointer to call to notify the completion of a join operation.

Functions#

otBleSecureStart(otInstance *aInstance, otHandleBleSecureConnect aConnectHandler, otHandleBleSecureReceive aReceiveHandler, bool aTlvMode, void *aContext)

Starts the BLE Secure service.

otBleSecureSetTcatVendorInfo(otInstance *aInstance, const otTcatVendorInfo *aVendorInfo)

Sets TCAT vendor info.

otBleSecureTcatStart(otInstance *aInstance, otHandleTcatJoin aHandler)

Enables the TCAT protocol over BLE Secure.

void
otBleSecureStop(otInstance *aInstance)

Stops the BLE Secure server.

void
otBleSecureSetPsk(otInstance *aInstance, const uint8_t *aPsk, uint16_t aPskLength, const uint8_t *aPskIdentity, uint16_t aPskIdLength)

Sets the Pre-Shared Key (PSK) and cipher suite TLS_PSK_WITH_AES_128_CCM_8.

otBleSecureGetPeerCertificateBase64(otInstance *aInstance, unsigned char *aPeerCert, size_t *aCertLength)

Returns the peer x509 certificate base64 encoded.

otBleSecureGetPeerCertificateDer(otInstance *aInstance, unsigned char *aPeerCert, size_t *aCertLength)

Returns the DER encoded peer x509 certificate.

otBleSecureGetPeerSubjectAttributeByOid(otInstance *aInstance, const char *aOid, size_t aOidLength, uint8_t *aAttributeBuffer, size_t *aAttributeLength, int *aAsn1Type)

Returns an attribute value identified by its OID from the subject of the peer x509 certificate.

otBleSecureGetThreadAttributeFromPeerCertificate(otInstance *aInstance, int aThreadOidDescriptor, uint8_t *aAttributeBuffer, size_t *aAttributeLength)

Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the peer x509 certificate, where the last digit x is set to aThreadOidDescriptor.

otBleSecureGetThreadAttributeFromOwnCertificate(otInstance *aInstance, int aThreadOidDescriptor, uint8_t *aAttributeBuffer, size_t *aAttributeLength)

Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the own x509 certificate, where the last digit x is set to aThreadOidDescriptor.

void
otBleSecureSetSslAuthMode(otInstance *aInstance, bool aVerifyPeerCertificate)

Sets the authentication mode for the BLE secure connection.

void
otBleSecureSetCertificate(otInstance *aInstance, const uint8_t *aX509Cert, uint32_t aX509Length, const uint8_t *aPrivateKey, uint32_t aPrivateKeyLength)

Sets the local device's X509 certificate with corresponding private key for TLS session with TLS_ECDHE_ECDSA_WITH_AES_128_CCM_8.

void
otBleSecureSetCaCertificateChain(otInstance *aInstance, const uint8_t *aX509CaCertificateChain, uint32_t aX509CaCertChainLength)

Sets the trusted top level CAs.

otBleSecureConnect(otInstance *aInstance)

Initializes TLS session with a peer using an already open BLE connection.

void
otBleSecureDisconnect(otInstance *aInstance)

Stops the BLE and TLS connection.

bool
otBleSecureIsConnectionActive(otInstance *aInstance)

Indicates whether or not the TLS session is active (connected or connecting).

bool
otBleSecureIsConnected(otInstance *aInstance)

Indicates whether or not the TLS session is connected.

bool
otBleSecureIsTcatEnabled(otInstance *aInstance)

Indicates whether or not the TCAT agent is enabled.

bool
otBleSecureIsCommandClassAuthorized(otInstance *aInstance, otTcatCommandClass aCommandClass)

Indicates whether or not a TCAT command class is authorized.

otBleSecureSendMessage(otInstance *aInstance, otMessage *aMessage)

Sends a secure BLE message.

otBleSecureSend(otInstance *aInstance, uint8_t *aBuf, uint16_t aLength)

Sends a secure BLE data packet.

otBleSecureSendApplicationTlv(otInstance *aInstance, uint8_t *aBuf, uint16_t aLength)

Sends a secure BLE data packet containing a TCAT Send Application Data TLV.

otBleSecureFlush(otInstance *aInstance)

Flushes the send buffer.

bool

Gets the Install Code Verify Status during the current session.

Macros#

#define

Maximum string length of a UDP or TCP service name (does not include null char).

#define

Maximum length of TCAT advertisement.

#define

TCAT Advertisement Operation Code.

#define

TCAT max size of any type of advertised Device ID.

#define

TCAT max size of device ID.

Enumeration Documentation#

otTcatStatusCode#

otTcatStatusCode

Represents TCAT status code.

Enumerator
OT_TCAT_STATUS_SUCCESS

Command or request was successfully processed.

OT_TCAT_STATUS_UNSUPPORTED

Requested command or received TLV is not supported.

OT_TCAT_STATUS_PARSE_ERROR

Request / command could not be parsed correctly.

OT_TCAT_STATUS_VALUE_ERROR

The value of the transmitted TLV has an error.

OT_TCAT_STATUS_GENERAL_ERROR

An error not matching any other category occurred.

OT_TCAT_STATUS_BUSY

Command cannot be executed because the resource is busy.

OT_TCAT_STATUS_UNDEFINED

The requested value, data or service is not defined (currently) or not present.

OT_TCAT_STATUS_HASH_ERROR

The hash value presented by the commissioner was incorrect.

OT_TCAT_STATUS_UNAUTHORIZED

Sender does not have sufficient authorization for the given command.


otTcatApplicationProtocol#

otTcatApplicationProtocol

Represents TCAT application protocol.

Enumerator
OT_TCAT_APPLICATION_PROTOCOL_NONE

Message which has been sent without activating the TCAT agent.

OT_TCAT_APPLICATION_PROTOCOL_STATUS

Message directed to a UDP service.

OT_TCAT_APPLICATION_PROTOCOL_TCP

Message directed to a TCP service.


otTcatCommandClass#

otTcatCommandClass

Represents a TCAT command class.

Enumerator
OT_TCAT_COMMAND_CLASS_GENERAL

TCAT commands related to general operations.

OT_TCAT_COMMAND_CLASS_COMMISSIONING

TCAT commands related to commissioning.

OT_TCAT_COMMAND_CLASS_EXTRACTION

TCAT commands related to key extraction.

OT_TCAT_COMMAND_CLASS_DECOMMISSIONING

TCAT commands related to de-commissioning.

OT_TCAT_COMMAND_CLASS_APPLICATION

TCAT commands related to application layer.


otTcatAdvertisedDeviceIdType#

otTcatAdvertisedDeviceIdType

Represents Advertised Device ID type.

(used during TCAT advertisement)

Enumerator
OT_TCAT_DEVICE_ID_EMPTY

Vendor device ID type not set.

OT_TCAT_DEVICE_ID_OUI24

Vendor device ID type IEEE OUI-24.

OT_TCAT_DEVICE_ID_OUI36

Vendor device ID type IEEE OUI-36.

OT_TCAT_DEVICE_ID_DISCRIMINATOR

Vendor device ID type Device Discriminator.

OT_TCAT_DEVICE_ID_IANAPEN

Vendor device ID type IANA PEN.

OT_TCAT_DEVICE_ID_MAX

Vendor device ID type size.


Typedef Documentation#

otHandleBleSecureConnect#

typedef void(* otHandleBleSecureConnect) (otInstance *aInstance, bool aConnected, bool aBleConnectionOpen, void *aContext) )(otInstance *aInstance, bool aConnected, bool aBleConnectionOpen, void *aContext)

Pointer to call when ble secure connection state changes.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

A pointer to an OpenThread instance.

[in]aConnected

TRUE, if a secure connection was established, FALSE otherwise.

[in]aBleConnectionOpen

TRUE if a BLE connection was established to carry a TLS data stream, FALSE otherwise.

[in]aContext

A pointer to arbitrary context information.


otHandleBleSecureReceive#

typedef otHandleTcatApplicationDataReceive otHandleBleSecureReceive

Pointer to call when data was received over a BLE Secure TLS connection.


otTcatStatusCode#

typedef enum otTcatStatusCode otTcatStatusCode

Represents TCAT status code.


otTcatApplicationProtocol#

typedef enum otTcatApplicationProtocol otTcatApplicationProtocol

Represents TCAT application protocol.


otTcatCommandClass#

typedef enum otTcatCommandClass otTcatCommandClass

Represents a TCAT command class.


otTcatAdvertisedDeviceIdType#

typedef enum otTcatAdvertisedDeviceIdType otTcatAdvertisedDeviceIdType

Represents Advertised Device ID type.

(used during TCAT advertisement)


otTcatAdvertisedDeviceId#

typedef struct otTcatAdvertisedDeviceId otTcatAdvertisedDeviceId

otTcatGeneralDeviceId#

typedef struct otTcatGeneralDeviceId otTcatGeneralDeviceId

Represents General Device ID type.


otTcatVendorInfo#

typedef struct otTcatVendorInfo otTcatVendorInfo

This structure represents a TCAT vendor information.

The content of this structure MUST persist and remain unchanged while a TCAT session is running.


otHandleTcatApplicationDataReceive#

typedef void(* otHandleTcatApplicationDataReceive) (otInstance *aInstance, const otMessage *aMessage, int32_t aOffset, otTcatApplicationProtocol aTcatApplicationProtocol, const char *aServiceName, void *aContext) )(otInstance *aInstance, const otMessage *aMessage, int32_t aOffset, otTcatApplicationProtocol aTcatApplicationProtocol, const char *aServiceName, void *aContext)

Pointer to call when application data was received over a TCAT TLS connection.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

A pointer to an OpenThread instance.

[in]aMessage

A pointer to the message.

[in]aOffset

The offset where the application data begins.

[in]aTcatApplicationProtocol

The protocol type of the message received.

[in]aServiceName

The name of the service the message is direced to.

[in]aContext

A pointer to arbitrary context information.


otHandleTcatJoin#

typedef void(* otHandleTcatJoin) (otError aError, void *aContext) )(otError aError, void *aContext)

Pointer to call to notify the completion of a join operation.

Parameters
TypeDirectionArgument NameDescription
[in]aError

OT_ERROR_NONE if the join process succeeded. OT_ERROR_SECURITY if the join process failed due to security credentials.

[in]aContext

A pointer to arbitrary context information.


Function Documentation#

otBleSecureStart#

otError otBleSecureStart (otInstance * aInstance, otHandleBleSecureConnect aConnectHandler, otHandleBleSecureReceive aReceiveHandler, bool aTlvMode, void * aContext)

Starts the BLE Secure service.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otHandleBleSecureConnect[in]aConnectHandler

A pointer to a function that will be called when the connection state changes.

otHandleBleSecureReceive[in]aReceiveHandler

A pointer to a function that will be called once data has been received over the TLS connection.

bool[in]aTlvMode

A boolean value indicating if line mode shall be activated.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

When TLV mode is active, the function aReceiveHandler will be called once a complete TLV was received and the message offset points to the TLV value.


otBleSecureSetTcatVendorInfo#

otError otBleSecureSetTcatVendorInfo (otInstance * aInstance, const otTcatVendorInfo * aVendorInfo)

Sets TCAT vendor info.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otTcatVendorInfo *[in]aVendorInfo

A pointer to the Vendor Information (must remain valid after the method call.


otBleSecureTcatStart#

otError otBleSecureTcatStart (otInstance * aInstance, otHandleTcatJoin aHandler)

Enables the TCAT protocol over BLE Secure.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otHandleTcatJoin[in]aHandler

A pointer to a function that is called when the join operation completes.


otBleSecureStop#

void otBleSecureStop (otInstance * aInstance)

Stops the BLE Secure server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureSetPsk#

void otBleSecureSetPsk (otInstance * aInstance, const uint8_t * aPsk, uint16_t aPskLength, const uint8_t * aPskIdentity, uint16_t aPskIdLength)

Sets the Pre-Shared Key (PSK) and cipher suite TLS_PSK_WITH_AES_128_CCM_8.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const uint8_t *[in]aPsk

A pointer to the PSK.

uint16_t[in]aPskLength

The PSK length.

const uint8_t *[in]aPskIdentity

The Identity Name for the PSK.

uint16_t[in]aPskIdLength

The PSK Identity Length.

Note

  • Requires the build-time feature MBEDTLS_KEY_EXCHANGE_PSK_ENABLED to be enabled.


otBleSecureGetPeerCertificateBase64#

otError otBleSecureGetPeerCertificateBase64 (otInstance * aInstance, unsigned char * aPeerCert, size_t * aCertLength)

Returns the peer x509 certificate base64 encoded.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

unsigned char *[out]aPeerCert

A pointer to the base64 encoded certificate buffer.

size_t *[inout]aCertLength

On input, the size the max size of aPeerCert. On output, the length of the base64 encoded peer certificate.

Note

  • Requires the build-time features MBEDTLS_BASE64_C and MBEDTLS_SSL_KEEP_PEER_CERTIFICATE to be enabled.


otBleSecureGetPeerCertificateDer#

otError otBleSecureGetPeerCertificateDer (otInstance * aInstance, unsigned char * aPeerCert, size_t * aCertLength)

Returns the DER encoded peer x509 certificate.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

unsigned char *[out]aPeerCert

A pointer to the DER encoded certificate buffer.

size_t *[inout]aCertLength

On input, the size the max size of aPeerCert. On output, the length of the DER encoded peer certificate.

Note

  • Requires the build-time feature MBEDTLS_SSL_KEEP_PEER_CERTIFICATE to be enabled.


otBleSecureGetPeerSubjectAttributeByOid#

otError otBleSecureGetPeerSubjectAttributeByOid (otInstance * aInstance, const char * aOid, size_t aOidLength, uint8_t * aAttributeBuffer, size_t * aAttributeLength, int * aAsn1Type)

Returns an attribute value identified by its OID from the subject of the peer x509 certificate.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const char *[in]aOid

A pointer to the OID to be found.

size_t[in]aOidLength

The length of the OID.

uint8_t *[out]aAttributeBuffer

A pointer to the attribute buffer.

size_t *[inout]aAttributeLength

On input, the size the max size of aAttributeBuffer. On output, the length of the attribute written to the buffer.

int *[out]aAsn1Type

A pointer to the ASN.1 type of the attribute written to the buffer.

The peer OID is provided in binary format. The attribute length is set if the attribute was successfully read or zero if unsuccessful. The ASN.1 type as is set as defineded in the ITU-T X.690 standard if the attribute was successfully read.

Note

  • Requires the build-time feature MBEDTLS_SSL_KEEP_PEER_CERTIFICATE to be enabled.


otBleSecureGetThreadAttributeFromPeerCertificate#

otError otBleSecureGetThreadAttributeFromPeerCertificate (otInstance * aInstance, int aThreadOidDescriptor, uint8_t * aAttributeBuffer, size_t * aAttributeLength)

Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the peer x509 certificate, where the last digit x is set to aThreadOidDescriptor.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

int[in]aThreadOidDescriptor

The last digit of the Thread attribute OID.

uint8_t *[out]aAttributeBuffer

A pointer to the attribute buffer.

size_t *[inout]aAttributeLength

On input, the size the max size of aAttributeBuffer. On output, the length of the attribute written to the buffer.

The attribute length is set if the attribute was successfully read or zero if unsuccessful. Requires a connection to be active.

Note

  • Requires the build-time feature MBEDTLS_SSL_KEEP_PEER_CERTIFICATE to be enabled.


otBleSecureGetThreadAttributeFromOwnCertificate#

otError otBleSecureGetThreadAttributeFromOwnCertificate (otInstance * aInstance, int aThreadOidDescriptor, uint8_t * aAttributeBuffer, size_t * aAttributeLength)

Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the own x509 certificate, where the last digit x is set to aThreadOidDescriptor.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

int[in]aThreadOidDescriptor

The last digit of the Thread attribute OID.

uint8_t *[out]aAttributeBuffer

A pointer to the attribute buffer.

size_t *[inout]aAttributeLength

On input, the size the max size of aAttributeBuffer. On output, the length of the attribute written to the buffer.

The attribute length is set if the attribute was successfully read or zero if unsuccessful. Requires a connection to be active.


otBleSecureSetSslAuthMode#

void otBleSecureSetSslAuthMode (otInstance * aInstance, bool aVerifyPeerCertificate)

Sets the authentication mode for the BLE secure connection.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aVerifyPeerCertificate

true, to verify the peer certificate.

Disable or enable the verification of peer certificate. Must be called before start.


otBleSecureSetCertificate#

void otBleSecureSetCertificate (otInstance * aInstance, const uint8_t * aX509Cert, uint32_t aX509Length, const uint8_t * aPrivateKey, uint32_t aPrivateKeyLength)

Sets the local device's X509 certificate with corresponding private key for TLS session with TLS_ECDHE_ECDSA_WITH_AES_128_CCM_8.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const uint8_t *[in]aX509Cert

A pointer to the PEM formatted X509 certificate.

uint32_t[in]aX509Length

The length of certificate.

const uint8_t *[in]aPrivateKey

A pointer to the PEM formatted private key.

uint32_t[in]aPrivateKeyLength

The length of the private key.

Note

  • Requires MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1.


otBleSecureSetCaCertificateChain#

void otBleSecureSetCaCertificateChain (otInstance * aInstance, const uint8_t * aX509CaCertificateChain, uint32_t aX509CaCertChainLength)

Sets the trusted top level CAs.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const uint8_t *[in]aX509CaCertificateChain

A pointer to the PEM formatted X509 CA chain.

uint32_t[in]aX509CaCertChainLength

The length of chain.

It is needed for validating the certificate of the peer.

TLS mode "ECDHE ECDSA with AES 128 CCM 8" for secure BLE.

Note

  • Requires MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1.


otBleSecureConnect#

otError otBleSecureConnect (otInstance * aInstance)

Initializes TLS session with a peer using an already open BLE connection.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureDisconnect#

void otBleSecureDisconnect (otInstance * aInstance)

Stops the BLE and TLS connection.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureIsConnectionActive#

bool otBleSecureIsConnectionActive (otInstance * aInstance)

Indicates whether or not the TLS session is active (connected or connecting).

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureIsConnected#

bool otBleSecureIsConnected (otInstance * aInstance)

Indicates whether or not the TLS session is connected.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureIsTcatEnabled#

bool otBleSecureIsTcatEnabled (otInstance * aInstance)

Indicates whether or not the TCAT agent is enabled.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

otBleSecureIsCommandClassAuthorized#

bool otBleSecureIsCommandClassAuthorized (otInstance * aInstance, otTcatCommandClass aCommandClass)

Indicates whether or not a TCAT command class is authorized.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otTcatCommandClass[in]aCommandClass

A command class to check.


otBleSecureSendMessage#

otError otBleSecureSendMessage (otInstance * aInstance, otMessage * aMessage)

Sends a secure BLE message.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the message to send.

If the return value is OT_ERROR_NONE, OpenThread takes ownership of aMessage, and the caller should no longer reference aMessage. If the return value is not OT_ERROR_NONE, the caller retains ownership of aMessage, including freeing aMessage if the message buffer is no longer needed.


otBleSecureSend#

otError otBleSecureSend (otInstance * aInstance, uint8_t * aBuf, uint16_t aLength)

Sends a secure BLE data packet.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[in]aBuf

A pointer to the data to send as the Value of the TCAT Send Application Data TLV.

uint16_t[in]aLength

A number indicating the length of the data buffer.


otBleSecureSendApplicationTlv#

otError otBleSecureSendApplicationTlv (otInstance * aInstance, uint8_t * aBuf, uint16_t aLength)

Sends a secure BLE data packet containing a TCAT Send Application Data TLV.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[in]aBuf

A pointer to the data to send as the Value of the TCAT Send Application Data TLV.

uint16_t[in]aLength

A number indicating the length of the data buffer.


otBleSecureFlush#

otError otBleSecureFlush (otInstance * aInstance)

Flushes the send buffer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otBleSecureGetInstallCodeVerifyStatus#

bool otBleSecureGetInstallCodeVerifyStatus (otInstance * aInstance)

Gets the Install Code Verify Status during the current session.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


Macro Definition Documentation#

OT_TCAT_MAX_SERVICE_NAME_LENGTH#

#define OT_TCAT_MAX_SERVICE_NAME_LENGTH
Value:
    15

Maximum string length of a UDP or TCP service name (does not include null char).


OT_TCAT_ADVERTISEMENT_MAX_LEN#

#define OT_TCAT_ADVERTISEMENT_MAX_LEN
Value:
29

Maximum length of TCAT advertisement.


OT_TCAT_OPCODE#

#define OT_TCAT_OPCODE
Value:
0x2

TCAT Advertisement Operation Code.


OT_TCAT_MAX_ADVERTISED_DEVICEID_SIZE#

#define OT_TCAT_MAX_ADVERTISED_DEVICEID_SIZE
Value:
5

TCAT max size of any type of advertised Device ID.


OT_TCAT_MAX_DEVICEID_SIZE#

#define OT_TCAT_MAX_DEVICEID_SIZE
Value:
64

TCAT max size of device ID.