Running Multiprotocol Solution on Docker#
NOTICE: The Multiprotocol Docker Container is now deprecated
Raspberry Pi / ARM Host with Docker Setup#
The quickest method to set up a multiprotocol host is to use the pre-configured Multiprotocol Docker container on the Raspberry Pi. This container includes everything necessary to easily run the Z3Gateway Zigbee application, the OpenThread Border Router (OTBR) and the ot-cli application, and the BlueZ Bluetooth stack and bluetoothctl, an open source interactive CLI utility for sending commands to the BlueZ stack.
The Multiprotocol Docker container is hosted on DockerHub (hub.docker.com) in the siliconlabsinc/multiprotocol repository. Pulling the latest tag is generally the best way to get the latest release by issuing this command:
docker pull siliconlabsinc/multiprotocol:latestIf necessary, you can replace the latest tag with a specific version. To run the Docker container, a helpful run.sh script is provided in the SDK in the app/host/multiprotocol/zigbeed/multiprotocol-container directory. The script is meant to simplify the docker setup process. Copy it to your Raspberry Pi’s home directory. Make sure the RCP device is flashed and attached to the Raspberry Pi before starting the Docker container.
The Docker container by default uses CPCd security, make sure your RCP has CPC Security Enabled. Before running the docker container, a CPCd security commissioning step is required. CPC is now configured by default to encrypt the data over the SPI or UART serial connection between the host and the EFR32. For detailed information, see https://github.com/SiliconLabs/cpc-daemon/blob/main/readme.md.
The run.sh script provides a convenient shortcut to perform the security commissioning. After flashing the EFR32 with the desired image, simply execute run.sh -K on the host. This will pull and run the docker container, use cpcd inside the container to commission security and generate a binding key file, then copy the binding key file outside of the container and place it at /etc/binding-key.key on the host filesystem. This file will then be used for all subsequent runs of the container to establish a secure connection with the EFR32.
After CPCd security is commissioned, to start the Docker container, execute the run.sh script without any arguments. The container will start systemd, which is a process management utility. This will make sure that all the components are started in the proper sequence and are kept running. At startup, only CPCd is started.
The /tmp/multiprotocol-container/log/ directory on the host will be mounted to /var/log/ inside the Docker container. It contains the file syslog, which will contain log output from cpcd, zigbeed, zigbeed-socat, otbr-agent, and ot-cli, among other programs. Monitor the file live by issuing the following command:
tail -f /tmp/multiprotocol-container/log/syslogUse the standard journalctl utility to monitor the logs for a given systemd service. For example, to monitor the cpcd log from outside of the container, use the following command:
docker exec -it multiprotocol journalctl -fexu cpcdAs a convenience, the command can also be executed by typing run.sh -l. Note that by default, verbose cpcd logging is disabled. To enable it, see TODO LINK TO CPCD FILE CONFIGURATION. After starting the container, it is a good idea to verify that CPCd successfully connected to the EFR32 by running run.sh -l and looking for the log line “Daemon startup was successful”.
A special file /accept_silabs_msla will be created in the Docker container to indicate acceptance of the Silicon Labs Master Software License Agreement (MSLA) located at https://www.silabs.com/about-us/legal/master-software-license-agreement.
Once the Docker container is running, you can open a shell by issuing the command:
run.sh -oThe Zigbeed configuration file is located: /usr/local/etc/zigbeed.conf and the CPCd configuration file is located: /usr/local/etc/cpcd.conf. For more information, see TODO Link to CPCD CONF.
The cpcd, zigbeed, zigbee_z3_gateway, zigbee_z3_gateway_cpc, zigbee_host_xncp_led, otbr-agent, ot-ctl, ot-cli, and cpc-hci-bridge binaries are all installed in /usr/local/bin. There are systemd configuration files to start up CPCd, zigbeed and socat for Zigbee, OTBR for OpenThread, and cpc-hci-bridge and hciattach for Bluetooth. The definition files for those are in /etc/systemd/system. Use systemd commands to start the services from within the Docker container shell as follows. Note that the otbr service takes an iid argument.
systemctl start zigbeed
systemctl start otbr
systemctl start hciattachFrom outside of the container, as follows:
docker exec -it multiprotocol systemctl start zigbeed
docker exec -it multiprotocol systemctl start otbr
docker exec -it multiprotocol systemctl start hciattachFor Bluetooth, to avoid interference with Bluetooth running in the container, first disable Bluetooth on the native Raspi host using the following commands:
sudo systemctl stop bluetooth
sudo systemctl mask bluetooth.serviceAfter starting the container and opening a shell, issue the command:
service hciattach startThis uses the systemd utility to start the necessary processes for the BlueZ stack to connect to the RCP via CPCd.
To interact with the Bluetooth network, issue the command:
bluetoothctlOnce at the bluetoothctl prompt, use the bluetoothctl commands such as list, advertise, connect, and scan to exercise the host Bluetooth stack and RCP. Additional documentation for bluetoothctl and BlueZ is available online.
Note that the zigbeed service automatically starts the zigbeed-socat service, and the hciattach service automatically starts the cpc-hcibridge service.
For convenience, the run.sh script has arguments to start each of these services after the container is running:
-Z starts zigbeed and launches a terminal with zigbee_z3_gateway
-T starts OTBR and opens a terminal with ot-ctl
-L starts Bluetooth and opens a terminal with bluetoothctl
-C launches a terminal with zigbee_z3_gateway_cpc (for use with the Zigbee NCP/OpenThread RCP)You can see the processes by running ps aux inside the Docker container. Alternatively, use systemd commands to see the state of the various services as follows:
systemctl status zigbeedTo stop the docker container issue:
run.sh -s. Zigbee Host Applications in Docker#
For convenience, a precompiled zigbee_z3_gateway host sample application is included in the Docker container. To run it with Zigbeed, issue the following commands from inside the Docker container shell (or on the host, depending on your installation):
Systemctl start zigbeed
/usr/local/bin/zigbee_z3_gateway -p ttyZigbeeNCPThe ttyZigbeeNCP refers to the file /dev/ttyZigbeeNCP. The zigbee_z3_gateway application automatically prepends /dev to a relative path in the -p argument. The run.sh -Z is a script that will run these commands on an already running container. Any Zigbee host application built with EZSP/ASH for communicating with a Zigbee NCP over a UART can also be used with Zigbeed by passing it the PTY device name. This is because to the host application, the PTY device appears exactly like a normal serial device. If theZigbee host application was built for EZSP/SPI, it will have to rebuild for EZSP/ASH to work with Zigbeed.
Some EZSP commands that are not supported with zigbeed:
• Set/Get Manufacturing Tokens
• EZSP_SET_MFG_TOKEN
• EZSP_GET_MFG_TOKEN
• Secure EZSP Commands
• EZSP_SET_SECURITY_KEY
• EZSP_SET_SECURITY_PARAMETERS
• EZSP_RESET_TO_FACTORY_DEFAULTS
• EZSP_GET_SECURITY_KEY_STATUS
• Bootloader Commands
• EZSP_LAUNCH_STANDALONE_BOOTLOADER
• EZSP_SEND_BOOTLOADER_MESSAGE
• EZSP_GET_STANDALONE_BOOTLOADER_VERSION_PLAT_MICRO_PHY
• EZSP_INCOMING_BOOTLOAD_MESSAGE_HANDLER
• EZSP_BOOTLOAD_TRANSMIT_COMPLETE_HANDLER
• EZSP_AES_ENCRYPTIf using the Zigbee NCP/OpenThread RCP, do not run Zigbeed on the host. Instead use a host app that has been built with the zigbee_ezsp_cpc component. For convenience, a precompiled zigbee_z3_gateway_cpc host sample application has been included in the Docker container. No arguments are required to run it, as it connects directly to CPCd. An optional -c argument can be supplied to specify the CPC daemon instance name to connect to. The default instance connected to is cpcd_0.
OT CLI Application in Docker#
A precompiled OpenThread ot-cli sample application with multi-PAN and CPCd support is also included in the Docker container and SDK. ot-cli is a stand-alone sample host application that includes the OpenThread stack and exposes the standard OpenThread CLI. You can run by issuing this command:
/usr/local/bin/ot-cli 'spinel+cpc://cpcd_0?iid=2&iid-list=0'The RCP uses the interface id parameter of the radio-url argument (iid=2) to distinguish between the OpenThread and Zigbeed applications. By default, the /usr/local/etc/zigbeed.conf file uses a radio-url argument with iid=1. The iid-list argument in radiourl is to allow spinel frames other than the host interface id. RCP uses the interface id zero to broadcast a spinel frame to all the hosts. The string ‘cpcd_0’ in the radio-url is the default CPCd instance name, which is defined in the /usr/local/etc/cpcd.conf file. To enable otcli debugging output, use the command line argument -d <level> to enable logging at the desired level 1-5. By default, log messages are printed to syslog. Add the argument -v as well to echo log messages to stdout as well. The run.sh -O command can be used as a shortcut to start this application on a running container and open a shell to it.
OpenThread Border Router (OTBR) Application in Docker#
The Multiprotocol Docker container is based on the OpenThread Border Router Docker container. It has all the necessary dependencies to run OTBR over CPC. To run OTBR with iid 2, issue the following commands from inside the Multiprotocol Docker container shell (or on the host, depending on your installation):
systemctl start otbr
ot-ctlFor convenience, this can be run with run.sh -T on a running container and open a shell to it. Note that OTBR uses ot-ctl instead of ot-cli. These two utilities offer similar CLI to the OpenThread network. But ot-ctl is a utility that connects to otbr-agent, which is the process that runs the OpenThread stack for OTBR. TODO POINT TO WHERE WE DISCUSS CHANING OTBR RADIO URL
To use OTBR with Zigbee NCP/OpenThread RCP application, OTBR must set iid value to zero in the radio-url. Otherwise, OpenThread RCP will reject the spinel frames for all non-zero iid values. To run OTBR with iid 0, issue the following command from inside the Multiprotocol Docker container:
systemctl start otbr
ot-ctlFor convenience, this can be run with run.sh -T 0 on an already running container to run OTBR with iid value zero.
Bluetooth Host Applications on Docker#
The multiprotocol solution uses the standard Linux BlueZ Bluetooth stack on the host. BlueZ and associated utilities are documented extensively online. Once Bluetooth is running as described in section 8: Bluetooth Host Setup, you can use standard Bluetooth tools such as bluetoothctl for a CLI utility and btmon to view the traffic going through the Bluetooth device.