Multicast DNS#

This module includes APIs for Multicast DNS (mDNS).

The mDNS APIs are available when the mDNS support OPENTHREAD_CONFIG_MULTICAST_DNS_ENABLE is enabled and the OPENTHREAD_CONFIG_MULTICAST_DNS_PUBLIC_API_ENABLE is also enabled.

Modules#

otMdnsLocalHostAddress

otMdnsCacheInfo

Enumerations#

enum
OT_MDNS_ENTRY_STATE_PROBING
OT_MDNS_ENTRY_STATE_REGISTERED
OT_MDNS_ENTRY_STATE_CONFLICT
OT_MDNS_ENTRY_STATE_REMOVING
}

Represents a host/service/key entry state.

Typedefs#

Represents a request ID (uint32_t value) for registering a host, a service, or a key service.

Represents the callback function to report the outcome of a host, service, or key registration request.

typedef void(*
otMdnsConflictCallback)(otInstance *aInstance, const char *aName, const char *aServiceType)

Represents the callback function to report a detected name conflict after successful registration of an entry.

Represents an mDNS host.

Represents an mDNS service.

Represents an mDNS key record.

typedef struct otMdnsIterator

Represents an mDNS entry iterator.

typedef enum otMdnsEntryState

Represents a host/service/key entry state.

typedef struct otMdnsLocalHostAddress

Represents a local host IPv4 or IPv6 address entry.

Represents a service browser.

Represents the callback function pointer type used to report a browse result.

Represents a browse result.

Represents an SRV service resolver.

Represents the callback function pointer type used to report an SRV resolve result.

Represents an SRV resolver result.

Represents a TXT service resolver.

Represents the callback function pointer type used to report a TXT resolve result.

Represents a TXT resolver result.

Represents an address resolver.

Represents the callback function pointer type use to report an IPv6/IPv4 address resolve result.

Represents a discovered host address and its TTL.

Represents address resolver result.

Represents a record query result.

Represents the callback function used to report a record querier result.

Represents a record querier.

typedef struct otMdnsCacheInfo

Represents additional information about a browser/resolver and its cached results.

Functions#

otMdnsSetEnabled(otInstance *aInstance, bool aEnable, uint32_t aInfraIfIndex)

Enables or disables the mDNS module.

bool
otMdnsIsEnabled(otInstance *aInstance)

Indicates whether the mDNS module is enabled.

void
otMdnsSetQuestionUnicastAllowed(otInstance *aInstance, bool aAllow)

Sets whether the mDNS module is allowed to send questions requesting unicast responses referred to as "QU" questions.

bool
otMdnsIsQuestionUnicastAllowed(otInstance *aInstance)

Indicates whether mDNS module is allowed to send "QU" questions requesting unicast response.

void
otMdnsSetConflictCallback(otInstance *aInstance, otMdnsConflictCallback aCallback)

Sets the post-registration conflict callback.

const char *
otMdnsGetLocalHostName(otInstance *aInstance)

Gets the local host name.

otMdnsSetLocalHostName(otInstance *aInstance, const char *aName)

Sets the local host name.

otMdnsRegisterHost(otInstance *aInstance, const otMdnsHost *aHost, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a host on mDNS.

otMdnsUnregisterHost(otInstance *aInstance, const otMdnsHost *aHost)

Unregisters a host on mDNS.

otMdnsRegisterService(otInstance *aInstance, const otMdnsService *aService, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a service on mDNS.

otMdnsUnregisterService(otInstance *aInstance, const otMdnsService *aService)

Unregisters a service on mDNS module.

otMdnsRegisterKey(otInstance *aInstance, const otMdnsKey *aKey, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a key record on mDNS module.

otMdnsUnregisterKey(otInstance *aInstance, const otMdnsKey *aKey)

Unregisters a key record on mDNS.

otMdnsAllocateIterator(otInstance *aInstance)

Allocates a new iterator.

void
otMdnsFreeIterator(otInstance *aInstance, otMdnsIterator *aIterator)

Frees a previously allocated iterator.

otMdnsGetNextHost(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsHost *aHost, otMdnsEntryState *aState)

Iterates over registered host entries.

otMdnsGetNextService(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsService *aService, otMdnsEntryState *aState)

Iterates over registered service entries.

otMdnsGetNextKey(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsKey *aKey, otMdnsEntryState *aState)

Iterates over registered key entries.

otMdnsGetNextLocalHostAddress(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsLocalHostAddress *aAddress)

Iterates over the local host IPv6 and IPv4 addresses tracked by OpenThread mDNS module.

otMdnsStartBrowser(otInstance *aInstance, const otMdnsBrowser *aBrowser)

Starts a service browser.

otMdnsStopBrowser(otInstance *aInstance, const otMdnsBrowser *aBroswer)

Stops a service browser.

otMdnsStartSrvResolver(otInstance *aInstance, const otMdnsSrvResolver *aResolver)

Starts an SRV record resolver.

otMdnsStopSrvResolver(otInstance *aInstance, const otMdnsSrvResolver *aResolver)

Stops an SRV record resolver.

otMdnsStartTxtResolver(otInstance *aInstance, const otMdnsTxtResolver *aResolver)

Starts a TXT record resolver.

otMdnsStopTxtResolver(otInstance *aInstance, const otMdnsTxtResolver *aResolver)

Stops a TXT record resolver.

otMdnsStartIp6AddressResolver(otInstance *aInstance, const otMdnsAddressResolver *aResolver)

Starts an IPv6 address resolver.

otMdnsStopIp6AddressResolver(otInstance *aInstance, const otMdnsAddressResolver *aResolver)

Stops an IPv6 address resolver.

otMdnsStartIp4AddressResolver(otInstance *aInstance, const otMdnsAddressResolver *aResolver)

Starts an IPv4 address resolver.

otMdnsStopIp4AddressResolver(otInstance *aInstance, const otMdnsAddressResolver *aResolver)

Stops an IPv4 address resolver.

otMdnsStartRecordQuerier(otInstance *aInstance, const otMdnsRecordQuerier *aQuerier)

Starts a record querier.

otMdnsStopRecordQuerier(otInstance *aInstance, const otMdnsRecordQuerier *aQuerier)

Stops a record querier.

otMdnsGetNextBrowser(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsBrowser *aBrowser, otMdnsCacheInfo *aInfo)

Iterates over browsers.

otMdnsGetNextSrvResolver(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsSrvResolver *aResolver, otMdnsCacheInfo *aInfo)

Iterates over SRV resolvers.

otMdnsGetNextTxtResolver(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsTxtResolver *aResolver, otMdnsCacheInfo *aInfo)

Iterates over TXT resolvers.

otMdnsGetNextIp6AddressResolver(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsAddressResolver *aResolver, otMdnsCacheInfo *aInfo)

Iterates over IPv6 address resolvers.

otMdnsGetNextIp4AddressResolver(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsAddressResolver *aResolver, otMdnsCacheInfo *aInfo)

Iterates over IPv4 address resolvers.

otMdnsGetNextRecordQuerier(otInstance *aInstance, otMdnsIterator *aIterator, otMdnsRecordQuerier *aQuerier, otMdnsCacheInfo *aInfo)

Iterates over record querier entries.

Enumeration Documentation#

otMdnsEntryState#

otMdnsEntryState

Represents a host/service/key entry state.

Enumerator
OT_MDNS_ENTRY_STATE_PROBING

Probing to claim the name.

OT_MDNS_ENTRY_STATE_REGISTERED

Entry is successfully registered.

OT_MDNS_ENTRY_STATE_CONFLICT

Name conflict was detected.

OT_MDNS_ENTRY_STATE_REMOVING

Entry is being removed (sending "goodbye" announcements).


Typedef Documentation#

otMdnsRequestId#

typedef otPlatDnssdRequestId otMdnsRequestId

Represents a request ID (uint32_t value) for registering a host, a service, or a key service.


otMdnsRegisterCallback#

typedef otPlatDnssdRegisterCallback otMdnsRegisterCallback

Represents the callback function to report the outcome of a host, service, or key registration request.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

The OpenThread instance.

[in]aRequestId

The request ID.

[in]aError

Error indicating the outcome of request.

The outcome of a registration request is reported back by invoking this callback with one of the following aError inputs:

  • OT_ERROR_NONE indicates registration was successful.

  • OT_ERROR_DUPLICATED indicates a name conflict while probing, i.e., name is claimed by another mDNS responder.

See otMdnsRegisterHost(), otMdnsRegisterService(), and otMdnsRegisterKey() for more details about when the callback will be invoked.


otMdnsConflictCallback#

typedef void(* otMdnsConflictCallback) (otInstance *aInstance, const char *aName, const char *aServiceType) )(otInstance *aInstance, const char *aName, const char *aServiceType)

Represents the callback function to report a detected name conflict after successful registration of an entry.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

The OpenThread instance.

[in]aName

The host name or the service instance label.

[in]aServiceType

The service type (e.g., _tst._udp).

If a conflict is detected while registering an entry, it is reported through the provided otMdnsRegisterCallback. The otMdnsConflictCallback is used only when a name conflict is detected after an entry has been successfully registered.

A non-NULL aServiceType indicates that conflict is for a service entry. In this case aName specifies the service instance label (treated as as a single DNS label and can potentially include dot . character).

A NULL aServiceType indicates that conflict is for a host entry. In this case Name specifies the host name. It does not include the domain name.


otMdnsHost#

typedef otPlatDnssdHost otMdnsHost

Represents an mDNS host.

This type is used to register or unregister a host (otMdnsRegisterHost() and otMdnsUnregisterHost()).

See the description of each function for more details on how different fields are used in each case.


otMdnsService#

typedef otPlatDnssdService otMdnsService

Represents an mDNS service.

This type is used to register or unregister a service (otMdnsRegisterService() and otMdnsUnregisterService()).

See the description of each function for more details on how different fields are used in each case.


otMdnsKey#

typedef otPlatDnssdKey otMdnsKey

Represents an mDNS key record.

See otMdnsRegisterKey(), otMdnsUnregisterKey() for more details about fields in each case.


otMdnsIterator#

typedef struct otMdnsIterator otMdnsIterator

Represents an mDNS entry iterator.


otMdnsEntryState#

typedef enum otMdnsEntryState otMdnsEntryState

Represents a host/service/key entry state.


otMdnsLocalHostAddress#

typedef struct otMdnsLocalHostAddress otMdnsLocalHostAddress

Represents a local host IPv4 or IPv6 address entry.


otMdnsBrowser#

typedef otPlatDnssdBrowser otMdnsBrowser

Represents a service browser.

Refer to otPlatDnssdBrowser for documentation of member fields and otMdnsStartBrowser() for how they are used.


otMdnsBrowseCallback#

typedef otPlatDnssdBrowseCallback otMdnsBrowseCallback

Represents the callback function pointer type used to report a browse result.


otMdnsBrowseResult#

typedef otPlatDnssdBrowseResult otMdnsBrowseResult

Represents a browse result.


otMdnsSrvResolver#

typedef otPlatDnssdSrvResolver otMdnsSrvResolver

Represents an SRV service resolver.

Refer to otPlatDnssdSrvResolver for documentation of member fields and otMdnsStartSrvResolver() for how they are used.


otMdnsSrvCallback#

typedef otPlatDnssdSrvCallback otMdnsSrvCallback

Represents the callback function pointer type used to report an SRV resolve result.


otMdnsSrvResult#

typedef otPlatDnssdSrvResult otMdnsSrvResult

Represents an SRV resolver result.


otMdnsTxtResolver#

typedef otPlatDnssdTxtResolver otMdnsTxtResolver

Represents a TXT service resolver.

Refer to otPlatDnssdTxtResolver for documentation of member fields and otMdnsStartTxtResolver() for how they are used.


otMdnsTxtCallback#

typedef otPlatDnssdTxtCallback otMdnsTxtCallback

Represents the callback function pointer type used to report a TXT resolve result.


otMdnsTxtResult#

typedef otPlatDnssdTxtResult otMdnsTxtResult

Represents a TXT resolver result.


otMdnsAddressResolver#

typedef otPlatDnssdAddressResolver otMdnsAddressResolver

Represents an address resolver.

Refer to otPlatDnssdAddressResolver for documentation of member fields and otMdnsStartIp6AddressResolver() or otMdnsStartIp4AddressResolver() for how they are used.


otMdnsAddressCallback#

typedef otPlatDnssdAddressCallback otMdnsAddressCallback

Represents the callback function pointer type use to report an IPv6/IPv4 address resolve result.


otMdnsAddressAndTtl#

typedef otPlatDnssdAddressAndTtl otMdnsAddressAndTtl

Represents a discovered host address and its TTL.


otMdnsAddressResult#

typedef otPlatDnssdAddressResult otMdnsAddressResult

Represents address resolver result.


otMdnsRecordResult#

typedef otPlatDnssdRecordResult otMdnsRecordResult

Represents a record query result.


otMdnsRecordCallback#

typedef otPlatDnssdRecordCallback otMdnsRecordCallback

Represents the callback function used to report a record querier result.


otMdnsRecordQuerier#

typedef otPlatDnssdRecordQuerier otMdnsRecordQuerier

Represents a record querier.


otMdnsCacheInfo#

typedef struct otMdnsCacheInfo otMdnsCacheInfo

Represents additional information about a browser/resolver and its cached results.


Function Documentation#

otMdnsSetEnabled#

otError otMdnsSetEnabled (otInstance * aInstance, bool aEnable, uint32_t aInfraIfIndex)

Enables or disables the mDNS module.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

bool[in]aEnable

Boolean to indicate whether to enable (on TRUE) or disable (on FALSE).

uint32_t[in]aInfraIfIndex

The network interface index for mDNS operation. Value is ignored when disabling

The mDNS module should be enabled before registration any host, service, or key entries. Disabling mDNS will immediately stop all operations and any communication (multicast or unicast tx) and remove any previously registered entries without sending any "goodbye" announcements or invoking their callback. Once disabled, all currently active browsers and resolvers are stopped.


otMdnsIsEnabled#

bool otMdnsIsEnabled (otInstance * aInstance)

Indicates whether the mDNS module is enabled.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.


otMdnsSetQuestionUnicastAllowed#

void otMdnsSetQuestionUnicastAllowed (otInstance * aInstance, bool aAllow)

Sets whether the mDNS module is allowed to send questions requesting unicast responses referred to as "QU" questions.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

bool[in]aAllow

Indicates whether or not to allow "QU" questions.

The "QU" questions request unicast responses, in contrast to "QM" questions which request multicast responses.

When allowed, the first probe will be sent as a "QU" question. This API can be used to address platform limitation where platform socket cannot accept unicast response received on mDNS port (due to it being already bound).


otMdnsIsQuestionUnicastAllowed#

bool otMdnsIsQuestionUnicastAllowed (otInstance * aInstance)

Indicates whether mDNS module is allowed to send "QU" questions requesting unicast response.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

otMdnsSetConflictCallback#

void otMdnsSetConflictCallback (otInstance * aInstance, otMdnsConflictCallback aCallback)

Sets the post-registration conflict callback.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsConflictCallback[in]aCallback

The conflict callback.

If a conflict is detected while registering an entry, it is reported through the provided otMdnsRegisterCallback. The otMdnsConflictCallback is used only when a name conflict is detected after an entry has been successfully registered.

aCallback can be set to NULL if not needed. Subsequent calls will replace any previously set callback.


otMdnsGetLocalHostName#

const char * otMdnsGetLocalHostName (otInstance * aInstance)

Gets the local host name.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

Returns

  • The local host name.


otMdnsSetLocalHostName#

otError otMdnsSetLocalHostName (otInstance * aInstance, const char * aName)

Sets the local host name.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const char *[in]aName

The local host name to use, can be to NULL to allow the mDNS module to choose the name.

The local host name can be set only when the mDNS module is disabled. If not set the mDNS module itself will auto-generate the local host name.


otMdnsRegisterHost#

otError otMdnsRegisterHost (otInstance * aInstance, const otMdnsHost * aHost, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a host on mDNS.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsHost *[in]aHost

Information about the host to register.

otMdnsRequestId[in]aRequestId

The ID associated with this request.

otMdnsRegisterCallback[in]aCallback

The callback function pointer to report the outcome (can be NULL if not needed).

The fields in aHost follow these rules:

  • The mHostName field specifies the host name to register (e.g., "myhost"). MUST NOT contain the domain name.

  • The mAddresses is array of IPv6 addresses to register with the host. mAddressesLength provides the number of entries in mAddresses array.

  • The mAddresses array can be empty with zero mAddressesLength. In this case, mDNS will treat it as if host is unregistered and stops advertising any addresses for this the host name.

  • The mTtl specifies the TTL if non-zero. If zero, the mDNS core will choose the default TTL of 120 seconds.

  • Other fields in aHost structure are ignored in an otMdnsRegisterHost() call.

This function can be called again for the same mHostName to update a previously registered host entry, for example, to change the list of addresses of the host. In this case, the mDNS module will send "goodbye" announcements for any previously registered and now removed addresses and announce any newly added addresses.

The outcome of the registration request is reported back by invoking the provided aCallback with aRequestId as its input and one of the following aError inputs:

  • OT_ERROR_NONE indicates registration was successful.

  • OT_ERROR_DULICATED indicates a name conflict while probing, i.e., name is claimed by another mDNS responder.

For caller convenience, the OpenThread mDNS module guarantees that the callback will be invoked after this function returns, even in cases of immediate registration success. The aCallback can be NULL if caller does not want to be notified of the outcome.


otMdnsUnregisterHost#

otError otMdnsUnregisterHost (otInstance * aInstance, const otMdnsHost * aHost)

Unregisters a host on mDNS.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsHost *[in]aHost

Information about the host to unregister.

The fields in aHost follow these rules:

  • The mHostName field specifies the host name to unregister (e.g., "myhost"). MUST NOT contain the domain name.

  • Other fields in aHost structure are ignored in an otMdnsUnregisterHost() call.

If there is no previously registered host with the same name, no action is performed.

If there is a previously registered host with the same name, the mDNS module will send "goodbye" announcement for all previously advertised address records.


otMdnsRegisterService#

otError otMdnsRegisterService (otInstance * aInstance, const otMdnsService * aService, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a service on mDNS.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsService *[in]aService

Information about the service to register.

otMdnsRequestId[in]aRequestId

The ID associated with this request.

otMdnsRegisterCallback[in]aCallback

The callback function pointer to report the outcome (can be NULL if not needed).

The fields in aService follow these rules:

  • The mServiceInstance specifies the service instance label. It is treated as a single DNS name label. It may contain dot . character which is allowed in a service instance label.

  • The mServiceType specifies the service type (e.g., "_tst._udp"). It is treated as multiple dot . separated labels. It MUST NOT contain the domain name.

  • The mHostName field specifies the host name of the service if it is not NULL. Otherwise, if it is NULL, it indicates that this service is for the local host (this device itself).

  • The mSubTypeLabels is an array of strings representing sub-types associated with the service. Each array entry is a sub-type label. The mSubTypeLabels can be NULL if there is no sub-type. Otherwise, the array length is specified bymSubTypeLabelsLength.

  • ThemTxtDataandmTxtDataLengthspecify the encoded TXT data. ThemTxtDatacan be NULL ormTxtDataLength can be zero to specify an empty TXT data. In this case mDNS module will use a single zero byte[ 0 ]` as the TXT data.

  • The mPort, mWeight, and mPriority specify the service's parameters as specified in DNS SRV record.

  • The mTtl specifies the TTL if non-zero. If zero, the mDNS module will use the default TTL of 120 seconds.

  • Other fields in aService structure are ignored in an otMdnsRegisterService() call.

This function can be called again for the same mServiceInstance and mServiceType to update a previously registered service entry, for example, to change the sub-types list, or update any parameter such as port, weight, priority, TTL, or host name. The mDNS module will send announcements for any changed info, e.g., will send "goodbye" announcements for any removed sub-types and announce any newly added sub-types.

Regarding the invocation of the aCallback, this function behaves in the same way as described in otMdnsRegisterHost().


otMdnsUnregisterService#

otError otMdnsUnregisterService (otInstance * aInstance, const otMdnsService * aService)

Unregisters a service on mDNS module.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsService *[in]aService

Information about the service to unregister.

The fields in aService follow these rules:

  • The mServiceInstance specifies the service instance label. It is treated as a single DNS name label. It may contain dot . character which is allowed in a service instance label.

  • The mServiceType specifies the service type (e.g., "_tst._udp"). It is treated as multiple dot . separated labels. It MUST NOT contain the domain name.

  • Other fields in aService structure are ignored in an otMdnsUnregisterService() call.

If there is no previously registered service with the same name, no action is performed.

If there is a previously registered service with the same name, the mDNS module will send "goodbye" announcements for all related records.


otMdnsRegisterKey#

otError otMdnsRegisterKey (otInstance * aInstance, const otMdnsKey * aKey, otMdnsRequestId aRequestId, otMdnsRegisterCallback aCallback)

Registers or updates a key record on mDNS module.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsKey *[in]aKey

Information about the key record to register.

otMdnsRequestId[in]aRequestId

The ID associated with this request.

otMdnsRegisterCallback[in]aCallback

The callback function pointer to report the outcome (can be NULL if not needed).

The fields in aKey follow these rules:

  • If the key is associated with a host entry, the mName field specifies the host name and the mServiceType MUST be NULL.

  • If the key is associated with a service entry, the mName filed specifies the service instance label (always treated as a single label) and the mServiceType filed specifies the service type (e.g., "_tst._udp"). In this case the DNS name for key record is <mName>.<mServiceTye>.

  • The mKeyData field contains the key record's data with mKeyDataLength as its length in byes.

  • The mTtl specifies the TTL if non-zero. If zero, the mDNS module will use the default TTL of 120 seconds.

  • Other fields in aKey structure are ignored in an otMdnsRegisterKey() call.

This function can be called again for the same name to updated a previously registered key entry, for example, to change the key data or TTL.

Regarding the invocation of the aCallback, this function behaves in the same way as described in otMdnsRegisterHost().


otMdnsUnregisterKey#

otError otMdnsUnregisterKey (otInstance * aInstance, const otMdnsKey * aKey)

Unregisters a key record on mDNS.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsKey *[in]aKey

Information about the key to unregister.

The fields in aKey follow these rules:

  • If the key is associated with a host entry, the mName field specifies the host name and the mServiceType MUST be NULL.

  • If the key is associated with a service entry, the mName filed specifies the service instance label (always treated as a single label) and the mServiceType filed specifies the service type (e.g., "_tst._udp"). In this case the DNS name for key record is <mName>.<mServiceTye>.

  • Other fields in aKey structure are ignored in an otMdnsUnregisterKey() call.

If there is no previously registered key with the same name, no action is performed.

If there is a previously registered key with the same name, the mDNS module will send "goodbye" announcements for the key record.


otMdnsAllocateIterator#

otMdnsIterator * otMdnsAllocateIterator (otInstance * aInstance)

Allocates a new iterator.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

An allocated iterator must be freed by the caller using otMdnsFreeIterator().

Returns

  • A pointer to the allocated iterator, or NULL if it fails to allocate.


otMdnsFreeIterator#

void otMdnsFreeIterator (otInstance * aInstance, otMdnsIterator * aIterator)

Frees a previously allocated iterator.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

The iterator to free.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.


otMdnsGetNextHost#

otError otMdnsGetNextHost (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsHost * aHost, otMdnsEntryState * aState)

Iterates over registered host entries.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsHost *[out]aHost

Pointer to an otMdnsHost to return the information about the next host entry.

otMdnsEntryState *[out]aState

Pointer to an otMdnsEntryState to return the entry state.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aHost is populated with information about the next host. Pointers within the otMdnsHost structure (like mName) remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextService#

otError otMdnsGetNextService (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsService * aService, otMdnsEntryState * aState)

Iterates over registered service entries.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator to use.

otMdnsService *[out]aService

Pointer to an otMdnsService to return the information about the next service entry.

otMdnsEntryState *[out]aState

Pointer to an otMdnsEntryState to return the entry state.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aService is populated with information about the next service . Pointers within the otMdnsService structure (like mServiceType, mSubTypeLabels) remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextKey#

otError otMdnsGetNextKey (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsKey * aKey, otMdnsEntryState * aState)

Iterates over registered key entries.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator to use.

otMdnsKey *[out]aKey

Pointer to an otMdnsKey to return the information about the next key entry.

otMdnsEntryState *[out]aState

Pointer to an otMdnsEntryState to return the entry state.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aKey is populated with information about the next key. Pointers within the otMdnsKey structure (like mName) remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextLocalHostAddress#

otError otMdnsGetNextLocalHostAddress (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsLocalHostAddress * aAddress)

Iterates over the local host IPv6 and IPv4 addresses tracked by OpenThread mDNS module.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[out]aIterator

Pointer to the iterator to use.

otMdnsLocalHostAddress *[out]aAddress

Pointer to an otMdnsLocalHostAddress to output the next address entry.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

The platform layer is responsible for monitoring and reporting all host IPv4 and IPv6 addresses to the OpenThread mDNS module, which then tracks the full address list (see otPlatMdnsHandleHostAddressEvent()). This function allows iteration through this tracked list, primarily intended for information and debugging purposes.


otMdnsStartBrowser#

otError otMdnsStartBrowser (otInstance * aInstance, const otMdnsBrowser * aBrowser)

Starts a service browser.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsBrowser *[in]aBrowser

The browser to be started.

Initiates a continuous search for the specified mServiceType in aBrowser. For sub-type services, use mSubTypeLabel to define the sub-type, for base services, set mSubTypeLabel to NULL.

Discovered services are reported through the mCallback function in aBrowser. Services that have been removed are reported with a TTL value of zero. The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached results are used, the reported TTL value will reflect the original TTL from the last received response.

Multiple browsers can be started for the same service, provided they use different callback functions.


otMdnsStopBrowser#

otError otMdnsStopBrowser (otInstance * aInstance, const otMdnsBrowser * aBroswer)

Stops a service browser.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsBrowser *[in]aBroswer

The browser to stop.

No action is performed if no matching browser with the same service and callback is currently active.


otMdnsStartSrvResolver#

otError otMdnsStartSrvResolver (otInstance * aInstance, const otMdnsSrvResolver * aResolver)

Starts an SRV record resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsSrvResolver *[in]aResolver

The resolver to be started.

Initiates a continuous SRV record resolver for the specified service in aResolver.

Discovered information is reported through the mCallback function in aResolver. When the service is removed it is reported with a TTL value of zero. In this case, mHostName may be NULL and other result fields (such as mPort) should be ignored.

The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached result is used, the reported TTL value will reflect the original TTL from the last received response.

Multiple resolvers can be started for the same service, provided they use different callback functions.


otMdnsStopSrvResolver#

otError otMdnsStopSrvResolver (otInstance * aInstance, const otMdnsSrvResolver * aResolver)

Stops an SRV record resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsSrvResolver *[in]aResolver

The resolver to stop.

No action is performed if no matching resolver with the same service and callback is currently active.


otMdnsStartTxtResolver#

otError otMdnsStartTxtResolver (otInstance * aInstance, const otMdnsTxtResolver * aResolver)

Starts a TXT record resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsTxtResolver *[in]aResolver

The resolver to be started.

Initiates a continuous TXT record resolver for the specified service in aResolver.

Discovered information is reported through the mCallback function in aResolver. When the TXT record is removed it is reported with a TTL value of zero. In this case, mTxtData may be NULL, and other result fields (such as mTxtDataLength) should be ignored.

The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached result is used, the reported TTL value will reflect the original TTL from the last received response.

Multiple resolvers can be started for the same service, provided they use different callback functions.


otMdnsStopTxtResolver#

otError otMdnsStopTxtResolver (otInstance * aInstance, const otMdnsTxtResolver * aResolver)

Stops a TXT record resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsTxtResolver *[in]aResolver

The resolver to stop.

No action is performed if no matching resolver with the same service and callback is currently active.


otMdnsStartIp6AddressResolver#

otError otMdnsStartIp6AddressResolver (otInstance * aInstance, const otMdnsAddressResolver * aResolver)

Starts an IPv6 address resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsAddressResolver *[in]aResolver

The resolver to be started.

Initiates a continuous IPv6 address resolver for the specified host name in aResolver.

Discovered addresses are reported through the mCallback function in aResolver. The callback is invoked whenever addresses are added or removed, providing an updated list. If all addresses are removed, the callback is invoked with an empty list (mAddresses will be NULL, and mAddressesLength will be zero).

The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached result is used, the reported TTL values will reflect the original TTL from the last received response.

Multiple resolvers can be started for the same host name, provided they use different callback functions.


otMdnsStopIp6AddressResolver#

otError otMdnsStopIp6AddressResolver (otInstance * aInstance, const otMdnsAddressResolver * aResolver)

Stops an IPv6 address resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsAddressResolver *[in]aResolver

The resolver to stop.

No action is performed if no matching resolver with the same host name and callback is currently active.


otMdnsStartIp4AddressResolver#

otError otMdnsStartIp4AddressResolver (otInstance * aInstance, const otMdnsAddressResolver * aResolver)

Starts an IPv4 address resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsAddressResolver *[in]aResolver

The resolver to be started.

Initiates a continuous IPv4 address resolver for the specified host name in aResolver.

Discovered addresses are reported through the mCallback function in aResolver. The IPv4 addresses are represented using the IPv4-mapped IPv6 address format in mAddresses array. The callback is invoked whenever addresses are added or removed, providing an updated list. If all addresses are removed, the callback is invoked with an empty list (mAddresses will be NULL, and mAddressesLength will be zero).

The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached result is used, the reported TTL values will reflect the original TTL from the last received response.

Multiple resolvers can be started for the same host name, provided they use different callback functions.


otMdnsStopIp4AddressResolver#

otError otMdnsStopIp4AddressResolver (otInstance * aInstance, const otMdnsAddressResolver * aResolver)

Stops an IPv4 address resolver.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsAddressResolver *[in]aResolver

The resolver to stop.

No action is performed if no matching resolver with the same host name and callback is currently active.


otMdnsStartRecordQuerier#

otError otMdnsStartRecordQuerier (otInstance * aInstance, const otMdnsRecordQuerier * aQuerier)

Starts a record querier.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsRecordQuerier *[in]aQuerier

The record querier to be started.

Initiates a continuous query for a given mRecordType as specified in aQuerier. The queried name is specified by the combination of mFirstLabel and mNextLabels (optional rest of the labels) in aQuerier. The mFirstLabel MUST be non-NULL but mNextLabels can be NULL if there are no other labels. The mNextLabels MUST NOT include the domain name. The reason for a separate first label is to allow it to include a dot . character (as allowed for service instance labels).

Discovered results are reported through the mCallback function in aQuerier, providing the record data bytes (RDATA). For NS, CNAME, SOA, PTR, MX, RP, AFSDB, RT, PX, SRV, KX, DNAME, and NSEC record types, the RDATA format contains one or more DNS names (which may use DNS name compression). For the above list, the reported record data bytes via mCallback will be decompressed to contain the full DNS name(s). For all other record types, the record data bytes are provided exactly as they appear in the received mDNS response. This aligns the implementation with RFC 6762 (section 18.14) regarding the use of name compression.

A removed record data is indicated with a TTL value of zero. The callback may be invoked immediately with cached information (if available) and potentially before this function returns. When cached results are used, the reported TTL value will reflect the original TTL from the last received response.

Multiple querier instances can be started for the same name, provided they use different callback functions.

The record querier MUST not be used for record types PTR, SRV, TXT, A, and AAAA. Otherwise, OT_ERROR_INVALID_ARGS will be returned. For these, browsers/resolvers can be used. This design is intentional to enable the implementation of an "opportunistic cache mechanism", where, depending on currently active service browsers/resolvers, the mDNS implementation will also monitor and cache related records (e.g., when a service is resolved, the address records associated with its host name are cached even if there is no active address resolver for this hostname).

The aQuerier and all its contained information (strings) are only valid during this call. The platform MUST save a copy of the information if it wants to retain the information after returning from this function.


otMdnsStopRecordQuerier#

otError otMdnsStopRecordQuerier (otInstance * aInstance, const otMdnsRecordQuerier * aQuerier)

Stops a record querier.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const otMdnsRecordQuerier *[in]aQuerier

The record querier to be stopped.

No action is performed if no matching querier with the same name and callback is currently active.

The aQuerier and all its contained information (strings) are only valid during this call. The platform MUST save a copy of the information if it wants to retain the information after returning from this function.


otMdnsGetNextBrowser#

otError otMdnsGetNextBrowser (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsBrowser * aBrowser, otMdnsCacheInfo * aInfo)

Iterates over browsers.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsBrowser *[out]aBrowser

Pointer to an otMdnsBrowser to return the information about the next browser.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aBrowser is populated with information about the next browser. The mCallback field is always set to NULL as there may be multiple active browsers with different callbacks. Other pointers within the otMdnsBrowser structure remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextSrvResolver#

otError otMdnsGetNextSrvResolver (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsSrvResolver * aResolver, otMdnsCacheInfo * aInfo)

Iterates over SRV resolvers.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsSrvResolver *[out]aResolver

Pointer to an otMdnsSrvResolver to return the information about the next resolver.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aResolver is populated with information about the next resolver. The mCallback field is always set to NULL as there may be multiple active resolvers with different callbacks. Other pointers within the otMdnsSrvResolver structure remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextTxtResolver#

otError otMdnsGetNextTxtResolver (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsTxtResolver * aResolver, otMdnsCacheInfo * aInfo)

Iterates over TXT resolvers.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsTxtResolver *[out]aResolver

Pointer to an otMdnsTxtResolver to return the information about the next resolver.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aResolver is populated with information about the next resolver. The mCallback field is always set to NULL as there may be multiple active resolvers with different callbacks. Other pointers within the otMdnsTxtResolver structure remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextIp6AddressResolver#

otError otMdnsGetNextIp6AddressResolver (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsAddressResolver * aResolver, otMdnsCacheInfo * aInfo)

Iterates over IPv6 address resolvers.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsAddressResolver *[out]aResolver

Pointer to an otMdnsAddressResolver to return the information about the next resolver.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aResolver is populated with information about the next resolver. The mCallback field is always set to NULL as there may be multiple active resolvers with different callbacks. Other pointers within the otMdnsAddressResolver structure remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextIp4AddressResolver#

otError otMdnsGetNextIp4AddressResolver (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsAddressResolver * aResolver, otMdnsCacheInfo * aInfo)

Iterates over IPv4 address resolvers.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsAddressResolver *[out]aResolver

Pointer to an otMdnsAddressResolver to return the information about the next resolver.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aResolver is populated with information about the next resolver. The mCallback field is always set to NULL as there may be multiple active resolvers with different callbacks. Other pointers within the otMdnsAddressResolver structure remain valid until the next call to any OpenThread stack's public or platform API/callback.


otMdnsGetNextRecordQuerier#

otError otMdnsGetNextRecordQuerier (otInstance * aInstance, otMdnsIterator * aIterator, otMdnsRecordQuerier * aQuerier, otMdnsCacheInfo * aInfo)

Iterates over record querier entries.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otMdnsIterator *[in]aIterator

Pointer to the iterator.

otMdnsRecordQuerier *[out]aQuerier

Pointer to an otMdnsRecordQuerier to return the information about the next one.

otMdnsCacheInfo *[out]aInfo

Pointer to an otMdnsCacheInfo to return additional information.

Requires OPENTHREAD_CONFIG_MULTICAST_DNS_ENTRY_ITERATION_API_ENABLE.

On success, aQuerier is populated with information about the next querier . The mCallback field is always set to NULL as there may be multiple active querier with different callbacks. Other pointers within the otMdnsRecordQuerier structure remain valid until the next call to any OpenThread stack's public or platform API/callback.