Tasklets#
This module includes functions that control the Thread stack's execution.
Functions#
void
otTaskletsProcess(otInstance *aInstance)
Run all queued OpenThread tasklets at the time this is called.
bool
otTaskletsArePending(otInstance *aInstance)
Indicates whether or not OpenThread has tasklets pending.
void
otTaskletsSignalPending(otInstance *aInstance)
OpenThread calls this function when the tasklet queue transitions from empty to non-empty.
Function Documentation#
otTaskletsProcess#
void otTaskletsProcess (otInstance *aInstance)
Run all queued OpenThread tasklets at the time this is called.
Parameters
[in] | aInstance | A pointer to an OpenThread instance. |
Definition at line
60
of file include/openthread/tasklet.h
otTaskletsArePending#
bool otTaskletsArePending (otInstance *aInstance)
Indicates whether or not OpenThread has tasklets pending.
Parameters
[in] | aInstance | A pointer to an OpenThread instance. |
Definition at line
71
of file include/openthread/tasklet.h
otTaskletsSignalPending#
void otTaskletsSignalPending (otInstance *aInstance)
OpenThread calls this function when the tasklet queue transitions from empty to non-empty.
Parameters
[in] | aInstance | A pointer to an OpenThread instance. |
Definition at line
79
of file include/openthread/tasklet.h