Represents Backbone Router configuration.
Public Attributes#
uint16_t
Only used when get Primary Backbone Router information in the Thread Network.
uint16_t
Reregistration Delay (in seconds)
uint32_t
Multicast Listener Registration Timeout (in seconds)
uint8_t
Sequence Number.
Public Attribute Documentation#
mServer16#
uint16_t otBackboneRouterConfig::mServer16
Only used when get Primary Backbone Router information in the Thread Network.
Definition at line
60
of file include/openthread/backbone_router.h
mReregistrationDelay#
uint16_t otBackboneRouterConfig::mReregistrationDelay
Reregistration Delay (in seconds)
Definition at line
61
of file include/openthread/backbone_router.h
mMlrTimeout#
uint32_t otBackboneRouterConfig::mMlrTimeout
Multicast Listener Registration Timeout (in seconds)
Definition at line
62
of file include/openthread/backbone_router.h
mSequenceNumber#
uint8_t otBackboneRouterConfig::mSequenceNumber
Sequence Number.
Definition at line
63
of file include/openthread/backbone_router.h