Represents a socket address info.

Public Attributes#

IP address. IPv4-mapped IPv6 format should be used to represent IPv4 address.

uint16_t

Port number.

uint32_t

Interface index.

Public Attribute Documentation#

mAddress#

otIp6Address otPlatMdnsAddressInfo::mAddress

IP address. IPv4-mapped IPv6 format should be used to represent IPv4 address.


Definition at line 65 of file include/openthread/platform/mdns_socket.h

mPort#

uint16_t otPlatMdnsAddressInfo::mPort

Port number.


Definition at line 66 of file include/openthread/platform/mdns_socket.h

mInfraIfIndex#

uint32_t otPlatMdnsAddressInfo::mInfraIfIndex

Interface index.


Definition at line 67 of file include/openthread/platform/mdns_socket.h