Represents a Service configuration.
Public Attributes#
uint8_t
Service ID (when iterating over the Network Data).
uint32_t
IANA Enterprise Number.
uint8_t
Length of service data.
uint8_t
Service data bytes.
The Server configuration.
Public Attribute Documentation#
mServiceId#
uint8_t otServiceConfig::mServiceId
Service ID (when iterating over the Network Data).
Definition at line
133
of file include/openthread/netdata.h
mEnterpriseNumber#
uint32_t otServiceConfig::mEnterpriseNumber
IANA Enterprise Number.
Definition at line
134
of file include/openthread/netdata.h
mServiceDataLength#
uint8_t otServiceConfig::mServiceDataLength
Length of service data.
Definition at line
135
of file include/openthread/netdata.h
mServiceData#
uint8_t otServiceConfig::mServiceData[OT_SERVICE_DATA_MAX_SIZE]
Service data bytes.
Definition at line
136
of file include/openthread/netdata.h
mServerConfig#
otServerConfig otServiceConfig::mServerConfig
The Server configuration.
Definition at line
137
of file include/openthread/netdata.h