Radio Configuration#
This module includes the platform abstraction for radio configuration.
Functions#
Get the radio capabilities.
Get the radio version string.
Get the radio receive sensitivity value.
Gets the factory-assigned IEEE EUI-64 for this interface.
Set the PAN ID for address filtering.
Set the Extended Address for address filtering.
Set the Short Address for address filtering.
Get the radio's transmit power in dBm.
Set the radio's transmit power in dBm.
Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Gets the external FEM's Rx LNA gain in dBm.
Sets the external FEM's Rx LNA gain in dBm.
Get the status of promiscuous mode.
Enable or disable promiscuous mode.
Update MAC keys and key index.
Sets the current MAC frame counter value.
Sets the current MAC frame counter value only if the new given value is larger than the current value.
Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).
Get the bus speed in bits/second between the host and the radio chip.
Function Documentation#
otPlatRadioGetCaps#
otRadioCaps otPlatRadioGetCaps (otInstance *aInstance)
Get the radio capabilities.
[in] | aInstance | The OpenThread instance structure. |
Returns
The radio capability bit vector (see
OT_RADIO_CAP_*
definitions).
477
of file include/openthread/platform/radio.h
otPlatRadioGetVersionString#
const char * otPlatRadioGetVersionString (otInstance *aInstance)
Get the radio version string.
[in] | aInstance | The OpenThread instance structure. |
This is an optional radio driver platform function. If not provided by platform radio driver, OpenThread uses the OpenThread version instead (See Also
Returns
A pointer to the OpenThread radio version.
490
of file include/openthread/platform/radio.h
otPlatRadioGetReceiveSensitivity#
int8_t otPlatRadioGetReceiveSensitivity (otInstance *aInstance)
Get the radio receive sensitivity value.
[in] | aInstance | The OpenThread instance structure. |
Returns
The radio receive sensitivity value in dBm.
500
of file include/openthread/platform/radio.h
otPlatRadioGetIeeeEui64#
void otPlatRadioGetIeeeEui64 (otInstance *aInstance, uint8_t *aIeeeEui64)
Gets the factory-assigned IEEE EUI-64 for this interface.
[in] | aInstance | The OpenThread instance structure. |
[out] | aIeeeEui64 | A pointer to the factory-assigned IEEE EUI-64. |
509
of file include/openthread/platform/radio.h
otPlatRadioSetPanId#
void otPlatRadioSetPanId (otInstance *aInstance, otPanId aPanId)
Set the PAN ID for address filtering.
[in] | aInstance | The OpenThread instance structure. |
[in] | aPanId | The IEEE 802.15.4 PAN ID. |
518
of file include/openthread/platform/radio.h
otPlatRadioSetExtendedAddress#
void otPlatRadioSetExtendedAddress (otInstance *aInstance, const otExtAddress *aExtAddress)
Set the Extended Address for address filtering.
[in] | aInstance | The OpenThread instance structure. |
[in] | aExtAddress | A pointer to the IEEE 802.15.4 Extended Address stored in little-endian byte order. |
528
of file include/openthread/platform/radio.h
otPlatRadioSetShortAddress#
void otPlatRadioSetShortAddress (otInstance *aInstance, otShortAddress aShortAddress)
Set the Short Address for address filtering.
[in] | aInstance | The OpenThread instance structure. |
[in] | aShortAddress | The IEEE 802.15.4 Short Address. |
537
of file include/openthread/platform/radio.h
otPlatRadioGetTransmitPower#
otError otPlatRadioGetTransmitPower (otInstance *aInstance, int8_t *aPower)
Get the radio's transmit power in dBm.
[in] | aInstance | The OpenThread instance structure. |
[out] | aPower | The transmit power in dBm. |
Note
The transmit power returned will be no larger than the power specified in the max power table for the current channel.
553
of file include/openthread/platform/radio.h
otPlatRadioSetTransmitPower#
otError otPlatRadioSetTransmitPower (otInstance *aInstance, int8_t aPower)
Set the radio's transmit power in dBm.
[in] | aInstance | The OpenThread instance structure. |
[in] | aPower | The transmit power in dBm. |
Note
The real transmit power will be no larger than the power specified in the max power table for the current channel.
568
of file include/openthread/platform/radio.h
otPlatRadioGetCcaEnergyDetectThreshold#
otError otPlatRadioGetCcaEnergyDetectThreshold (otInstance *aInstance, int8_t *aThreshold)
Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
[in] | aInstance | The OpenThread instance structure. |
[out] | aThreshold | The CCA ED threshold in dBm. |
581
of file include/openthread/platform/radio.h
otPlatRadioSetCcaEnergyDetectThreshold#
otError otPlatRadioSetCcaEnergyDetectThreshold (otInstance *aInstance, int8_t aThreshold)
Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
[in] | aInstance | The OpenThread instance structure. |
[in] | aThreshold | The CCA ED threshold in dBm. |
594
of file include/openthread/platform/radio.h
otPlatRadioGetFemLnaGain#
otError otPlatRadioGetFemLnaGain (otInstance *aInstance, int8_t *aGain)
Gets the external FEM's Rx LNA gain in dBm.
[in] | aInstance | The OpenThread instance structure. |
[out] | aGain | The external FEM's Rx LNA gain in dBm. |
607
of file include/openthread/platform/radio.h
otPlatRadioSetFemLnaGain#
otError otPlatRadioSetFemLnaGain (otInstance *aInstance, int8_t aGain)
Sets the external FEM's Rx LNA gain in dBm.
[in] | aInstance | The OpenThread instance structure. |
[in] | aGain | The external FEM's Rx LNA gain in dBm. |
619
of file include/openthread/platform/radio.h
otPlatRadioGetPromiscuous#
bool otPlatRadioGetPromiscuous (otInstance *aInstance)
Get the status of promiscuous mode.
[in] | aInstance | The OpenThread instance structure. |
630
of file include/openthread/platform/radio.h
otPlatRadioSetPromiscuous#
void otPlatRadioSetPromiscuous (otInstance *aInstance, bool aEnable)
Enable or disable promiscuous mode.
[in] | aInstance | The OpenThread instance structure. |
[in] | aEnable | TRUE to enable or FALSE to disable promiscuous mode. |
639
of file include/openthread/platform/radio.h
otPlatRadioSetMacKey#
void otPlatRadioSetMacKey (otInstance *aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKeyMaterial *aPrevKey, const otMacKeyMaterial *aCurrKey, const otMacKeyMaterial *aNextKey, otRadioKeyType aKeyType)
Update MAC keys and key index.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aKeyIdMode | The key ID mode. |
[in] | aKeyId | Current MAC key index. |
[in] | aPrevKey | A pointer to the previous MAC key. |
[in] | aCurrKey | A pointer to the current MAC key. |
[in] | aNextKey | A pointer to the next MAC key. |
[in] | aKeyType | Key Type used. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC capability.
655
of file include/openthread/platform/radio.h
otPlatRadioSetMacFrameCounter#
void otPlatRadioSetMacFrameCounter (otInstance *aInstance, uint32_t aMacFrameCounter)
Sets the current MAC frame counter value.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aMacFrameCounter | The MAC frame counter value. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC
capability.
672
of file include/openthread/platform/radio.h
otPlatRadioSetMacFrameCounterIfLarger#
void otPlatRadioSetMacFrameCounterIfLarger (otInstance *aInstance, uint32_t aMacFrameCounter)
Sets the current MAC frame counter value only if the new given value is larger than the current value.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aMacFrameCounter | The MAC frame counter value. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC
capability.
683
of file include/openthread/platform/radio.h
otPlatRadioGetNow#
uint64_t otPlatRadioGetNow (otInstance *aInstance)
Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).
[in] | aInstance | A pointer to an OpenThread instance. |
The radio clock SHALL NOT wrap during the device's uptime. Implementations SHALL therefore identify and compensate for internal counter overflows. The clock does not have a defined epoch and it SHALL NOT introduce any continuous or discontinuous adjustments (e.g. leap seconds). Implementations SHALL compensate for any sleep times of the device.
Implementations MAY choose to discipline the radio clock and compensate for sleep times by any means (e.g. by combining a high precision/low power RTC with a high resolution counter) as long as the exposed combined clock provides continuous monotonic microsecond resolution ticks within the accuracy limits announced by otPlatRadioGetCslAccuracy.
Returns
The current time in microseconds. UINT64_MAX when platform does not support or radio time is not ready.
707
of file include/openthread/platform/radio.h
otPlatRadioGetBusSpeed#
uint32_t otPlatRadioGetBusSpeed (otInstance *aInstance)
Get the bus speed in bits/second between the host and the radio chip.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The bus speed in bits/second between the host and the radio chip. Return 0 when the MAC and above layer and Radio layer resides on the same chip.
718
of file include/openthread/platform/radio.h