Introduction and Setup#

This guide describes how to get started with the Simplicity Power Estimator, including installation, access options, and configuration for supported devices and applications.

System Requirements#

To use the Simplicity Power Estimator, ensure the following requirements are met:

Requirement

Description

Simplicity Studio 6

Required when using the estimator from within Simplicity Studio.

Internet Access

Required when accessing the estimator through a web browser.

Access the Simplicity Power Estimator#

The Simplicity Power Estimator is available through Simplicity Studio 6 or directly through a web browser.

Access from Simplicity Studio 6#

  1. Open the SLT Installer.

  2. Go to the Package Manager.

  3. Search for Simplicity Power Estimator.

  4. Select Install.

Access from a Web Browser#

Open the Simplicity Power Estimator at:

https://power-estimator.silabs.net/