CDC ACM CALLBACKS.

CDC ACM Callbacks

Public Attributes#

void(*

Callback for enable event.

void(*

Callback for disable event.

void(*

Callback for line control changed event.

bool(*

Callback for line coding change event.

Public Attribute Documentation#

enable#

void(* sl_usbd_cdc_acm_callbacks_t::enable) (uint8_t subclass_nbr)

Callback for enable event.


Definition at line 122 of file protocol/usb/inc/sl_usbd_class_cdc_acm.h

disable#

void(* sl_usbd_cdc_acm_callbacks_t::disable) (uint8_t subclass_nbr)

Callback for disable event.


Definition at line 124 of file protocol/usb/inc/sl_usbd_class_cdc_acm.h

line_control_changed#

void(* sl_usbd_cdc_acm_callbacks_t::line_control_changed) (uint8_t subclass_nbr, uint8_t event, uint8_t event_chngd)

Callback for line control changed event.


Definition at line 126 of file protocol/usb/inc/sl_usbd_class_cdc_acm.h

line_coding_changed#

bool(* sl_usbd_cdc_acm_callbacks_t::line_coding_changed) (uint8_t subclass_nbr, sl_usbd_cdc_acm_line_coding_t *p_line_coding)

Callback for line coding change event.


Definition at line 130 of file protocol/usb/inc/sl_usbd_class_cdc_acm.h