MODULE.

INCLUDE FILES DATA TYPES Vendor callbacks

Public Attributes#

void(*

Callback for enable event.

void(*

Callback for disable event.

void(*

Callback for setup req event.

Public Attribute Documentation#

enable#

void(* sl_usbd_vendor_callbacks_t::enable) (uint8_t class_nbr)

Callback for enable event.


Definition at line 54 of file protocol/usb/inc/sl_usbd_class_vendor.h

disable#

void(* sl_usbd_vendor_callbacks_t::disable) (uint8_t class_nbr)

Callback for disable event.


Definition at line 56 of file protocol/usb/inc/sl_usbd_class_vendor.h

setup_req#

void(* sl_usbd_vendor_callbacks_t::setup_req) (uint8_t class_nbr, const sl_usbd_setup_req_t *p_setup_req)

Callback for setup req event.


Definition at line 58 of file protocol/usb/inc/sl_usbd_class_vendor.h