You are viewing documentation for version:
PDFUSB DEVICE MICROSOFT XTENDED PROPERTIES DATA TYPE.
USB SETUP REQUEST
Public Attributes#
uint8_t
Characteristics of request.
uint16_t
Varies according to request.
uint16_t
Varies according to request; typically used as index.
uint16_t
Transfer length if data stage present.
Public Attribute Documentation#
bmRequestType#
uint8_t sl_usbd_setup_req_t::bmRequestType
Characteristics of request.
bRequest#
uint8_t sl_usbd_setup_req_t::bRequest
Specific request.
wValue#
uint16_t sl_usbd_setup_req_t::wValue
Varies according to request.
wIndex#
uint16_t sl_usbd_setup_req_t::wIndex
Varies according to request; typically used as index.
wLength#
uint16_t sl_usbd_setup_req_t::wLength
Transfer length if data stage present.