Modules#

RAIL Changelist

RAILtest Changelist

API Changes

Release Notes#

RAIL Library 2.14.2 GA#

March 8, 2023

Release Highlights#

  • Bugfixes and minor improvements.

Release Details#

RAIL Library 2.14.1 GA#

February 1, 2023

Release Highlights#

  • Added support for the EFR32xG25 series of parts.

  • Bugfixes and minor improvements.

Release Details#

RAIL Library 2.14.0 GA#

December 14, 2022

Release Highlights#

  • Added support for IEEE 802.15.4 fast RX channel switching to enable detecting packets on two different IEEE 802.15.4 channels at the same time on supported platforms. See the RAIL_IEEE802154_ConfigRxChannelSwitching for more details.

  • Added support for the BGM240SB22VNA, MGM240SB22VNA, MGM240SD22VNA, BGM220SC23HNA, MGM240SA22VNA, BGM240SA22VNA, and BGM241SD22VNA modules.

  • Added support for HFXO compensation on select platforms. See RAIL_ConfigHFXOCompensation for more details.

  • Added support for Thermal Protection on select platforms to restrict transmit over a certain temperature.

  • Added initial support for 40MHz crystals when using the EFR32xG24 part.

  • Fixed a critical issue on the EFR32xG24 that could corrupt a SYNTH calibration value in specific circumstances. For Silicon Labs BLE stack users this would happen when using EM2 sleep and receiving a packet with an error right before sleep. For other Silicon Labs stacks this condition was not exposed.

  • Bugfixes and minor improvements.

Release Details#