Power Amplifier (PA)#
APIs for interacting with one of the on chip PAs.
These APIs let you configure the on-chip PA to get the appropriate output power.
These are the function types: 1) Configuration functions: These functions set and get configuration for the PA. In this case, "configuration" refers to a) indicating which PA to use, b) the voltage supplied by your board to the PA, and c) the ramp time over which to ramp the PA up to its full power. 2) Power-setting functions: These functions consume the actual values written to the PA registers and write them appropriately. These values are referred to as "(raw) power levels". The range of acceptable values for these functions depends on which PA is currently active. The higher the power level set, the higher the dBm power output by the chip. However, the mapping between dBm and these power levels can vary greatly between modules/boards. 3) Conversion functions: These functions convert between the "power levels" discussed previously and the dBm values output by the chip. Continue reading for more information about unit conversion.
The accuracy of the chip output power is application-specific. For some protocols or channels, the protocol itself or legal limitations require applications to know exactly what power they're transmitting at, in dBm. Other applications do not have these restrictions, and users determine power level(s) that fit their criteria for the trade-off between radio range and power savings, regardless of what dBm power that maps to.
RAIL_ConvertRawToDbm and RAIL_ConvertDbmToRaw, which convert between the dBm power and the raw power levels, provide a solution that fits all these applications. The levels of customization are outlined below: 1) No customization needed: for a given dBm value, the result of RAIL_ConvertDbmToRaw provides an appropriate raw power level that, when written to the registers via RAIL_SetPowerLevel, causes the chip to output at that dBm power. In this case, no action is needed by the user, the WEAK versions of the conversion functions can be used and the default include paths in pa_conversions_efr32.h can be used. 2) The mapping of power level to dBm is not ideal, but the level of precision is sufficient: In pa_conversions_efr32.c, the WEAK versions of the conversion functions work by using 8-segment piecewise linear curves to convert between dBm and power levels for PA's with hundreds of power levels and simple mapping tables for use with PA's with only a few levels. If this method is sufficiently precise, but the mapping between power levels and dBm is incorrect, copy pa_curves_efr32.h into a new file, updating the segments to form a better fit (_DCDC_CURVES or _VBAT_CURVES defines) and then add the RAIL_PA_CURVES define to your build with the path to the new file. 3) A different level of precision is needed and the fit is bad: If the piecewise-linear line segment fit is not appropriate for your solution, the functions in pa_conversions_efr32.c can be totally rewritten, as long as RAIL_ConvertDbmToRaw and RAIL_ConvertRawToDbm have the same signatures. It is completely acceptable to re-write these in a way that makes the pa_curves_efr32.h and pa_curve_types_efr32.h files referenced in pa_conversions_efr32.h unnecessary. Those files are needed solely for the provided conversion methods. 4) dBm values are not necessary: If the application does not require dBm values at all, overwrite RAIL_ConvertDbmToRaw and RAIL_ConvertRawToDbm with smaller functions (i.e., return 0 or whatever was input). These functions are called from within the RAIL library, so they can never be deadstripped, but making them as small as possible is the best way to reduce code size. From there, call RAIL_SetTxPower, without converting from a dBm value. To stop the library from coercing the power based on channels, overwrite RAIL_ConvertRawToDbm to always return 0 and overwrite RAIL_ConvertDbmToRaw to always return 255.
The following is example code that shows how to initialize your PA
#include "pa_conversions_efr32.h"
// A helper macro to declare all the curve structures used by the provided
// conversion functions.
RAIL_DECLARE_TX_POWER_VBAT_CURVES(piecewiseSegments, curvesSg, curves24Hp, curves24Lp);
// Puts the variables declared above into the appropriate structure.
RAIL_TxPowerCurvesConfig_t txPowerCurvesConfig = { curves24Hp, curvesSg, curves24Lp, piecewiseSegments };
// Saves those curves
// to be referenced when the conversion functions are called.
RAIL_InitTxPowerCurves(&txPowerCurvesConfig);
// Declares the structure used to configure the PA.
RAIL_TxPowerConfig_t txPowerConfig = { RAIL_TX_POWER_MODE_2P4_HP, 3300, 10 };
// Initializes the PA. Here, it is assumed that 'railHandle' is a valid RAIL_Handle_t
// that has already been initialized.
RAIL_ConfigTxPower(railHandle, &txPowerConfig);
// Picks a dBm power to use: 100 deci-dBm = 10 dBm. See docs on RAIL_TxPower_t.
RAIL_TxPower_t power = 100;
// Gets the config written by RAIL_ConfigTxPower to confirm what was actually set.
RAIL_GetTxPowerConfig(railHandle, &txPowerConfig);
// RAIL_ConvertDbmToRaw is the default weak version,
// or the customer version, if overwritten.
RAIL_TxPowerLevel_t powerLevel = RAIL_ConvertDbmToRaw(railHandle,
txPowerConfig.mode,
power);
// Writes the result of the conversion to the PA power registers in terms
// of raw power levels.
RAIL_SetTxPower(railHandle, powerLevel);
Note
All lines following "RAIL_TxPower_t power = 100;" can be replaced with the provided utility function, RAIL_SetTxPowerDbm. However, the full example here was provided for clarity. See the documentation on RAIL_SetTxPowerDbm for more details.
Modules#
Enumerations#
An enumeration of the EFR32 power modes.
Enum used to specify the band for a PA.
Typedefs#
The transmit power in deci-dBm units (e.g., 4.5 dBm -> 45 deci-dBm).
Raw power levels used directly by the RAIL_Get/SetTxPower API where a higher numerical value corresponds to a higher output power.
PA power setting used directly by the RAIL_GetPaPowerSetting() and RAIL_SetPaPowerSetting() APIs which is decoded to the actual hardware register value(s).
Variables#
The actual PA auto mode configuration structure used by the auto mode plugin to control output power.
Functions#
Initialize TX power settings.
Get the TX power settings currently used in the amplifier.
Set the TX power in units of raw units (see rail_chip_specific.h for value ranges).
Return the current power setting of the PA.
Convert raw values written to registers to decibel value (in units of deci-dBm).
Convert the desired decibel value (in units of deci-dBm) to raw integer values used by the TX amplifier registers.
Verify the TX Power Curves on modules.
Set the TX power in terms of deci-dBm instead of raw power level.
Get the TX power in terms of deci-dBm instead of raw power level.
Get the TX PA power setting table and related values.
Set the TX PA power setting used to configure the PA hardware for the PA output power determined by RAIL_SetTxPowerDbm().
Get the TX PA power setting, which is used to configure power configurations when the dBm to paPowerSetting mapping table mode is used.
Enable automatic switching between PAs internally to the RAIL library.
Query status of PA Auto Mode.
Callback that decides which PA and power level should be used while in PA auto mode.
Configure the PA auto mode entries.
Macros#
The maximum valid value for a RAIL_TxPower_t.
The minimum valid value for a RAIL_TxPower_t.
The maximum power in deci-dBm the curve supports.
The increment step in deci-dBm for calculating power level.
mV are used for all TX power voltage values.
deci-dBm are used for all TX power dBm values.
Invalid RAIL_TxPowerLevel_t value returned when an error occurs with RAIL_GetTxPower.
Sentinel value that can be passed to RAIL_SetTxPower to set the highest power level available on the current PA, regardless of which one is selected.
Returned by RAIL_GetPaPowerSetting when the device does not support the dBm to power setting mapping table.
The names of the TX power modes.
Convenience macro for any EFF power mode.
Convenience macro for any OFDM mapping table mode.
Convenience macro for any Sub-GHz mapping table mode.
Convenience macro for any mapping table mode.
Convenience macro for any OFDM mode.
Enumeration Documentation#
RAIL_TxPowerMode_t#
RAIL_TxPowerMode_t
An enumeration of the EFR32 power modes.
The power modes on the EFR32 correspond to the different on-chip PAs that are available. For more information about the power and performance characteristics of a given amplifier, see the data sheet.
| Enumerator | |
|---|---|
| RAIL_TX_POWER_MODE_2P4GIG_HP | High-power 2.4 GHz amplifier EFR32xG1X: up to 20 dBm, raw values: 0-252 EFR32xG21: up to 20 dBm, raw values: 1-180 EFR32xG22: up to 6 dBm, raw values: 1-128 EFR32xG24: up to 20 dBm, raw values: 0-180, or up to 10 dBm, raw values: 0-90 EFR32xG26: same as EFR32xG24 EFR32xG27: up to 6 dBm, raw values: 1-128 EFR32xG28: up to 10 dBm, raw values: 0-240 Not supported on other platforms. |
| RAIL_TX_POWER_MODE_2P4_HP | DeprecatedPlease use RAIL_TX_POWER_MODE_2P4GIG_HP instead. |
| RAIL_TX_POWER_MODE_2P4GIG_MP | Mid-power 2.4 GHz amplifier EFR32xG21: up to 10 dBm, raw values: 1-90 Not supported on other platforms. |
| RAIL_TX_POWER_MODE_2P4_MP | DeprecatedPlease use RAIL_TX_POWER_MODE_2P4GIG_MP instead. |
| RAIL_TX_POWER_MODE_2P4GIG_LP | Low-power 2.4 GHz amplifier EFR32xG1x: up to 0 dBm, raw values: 1-7 EFR32xG21: up to 0 dBm, raw values: 1-64 EFR32xG22: up to 0 dBm, raw values: 1-16 EFR32xG24: up to 0 dBm, raw values: 1-16 EFR32xG26: same as EFR32xG24 EFR32xG27: up to 0 dBm, raw values: 1-16 Not supported on other platforms. |
| RAIL_TX_POWER_MODE_2P4_LP | DeprecatedPlease use RAIL_TX_POWER_MODE_2P4GIG_LP instead. |
| RAIL_TX_POWER_MODE_2P4GIG_LLP | Low-Low-power 2.4 GHz amplifier Not currently supported on any EFR32 platform. |
| RAIL_TX_POWER_MODE_2P4GIG_HIGHEST | Select the highest 2.4 GHz power PA available on the current chip. |
| RAIL_TX_POWER_MODE_2P4_HIGHEST | DeprecatedPlease use RAIL_TX_POWER_MODE_2P4GIG_HIGHEST instead. |
| RAIL_TX_POWER_MODE_SUBGIG_POWERSETTING_TABLE | PA for all Sub-GHz dBm values in range, using RAIL_PaPowerSetting_t table. |
| RAIL_TX_POWER_MODE_SUBGIG_HP | High-power Sub-GHz amplifier (Class D mode) EFR32xG1x: up to 20 dBm, raw values: 0-248 Also supported on FR32xG23 and EFR32xG28. |
| RAIL_TX_POWER_MODE_SUBGIG | DeprecatedPlease use RAIL_TX_POWER_MODE_SUBGIG_HP instead. |
| RAIL_TX_POWER_MODE_SUBGIG_MP | Mid-power Sub-GHz amplifier Supported only on EFR32xG23 and EFR32xG28. |
| RAIL_TX_POWER_MODE_SUBGIG_LP | Low-power Sub-GHz amplifier Supported only on EFR32xG23 and EFR32xG28. |
| RAIL_TX_POWER_MODE_SUBGIG_LLP | Low-Low-power Sub-GHz amplifier Supported only on EFR32xG23 and EFR32xG28. |
| RAIL_TX_POWER_MODE_SUBGIG_HIGHEST | Select the highest Sub-GHz power PA available on the current chip. |
| RAIL_TX_POWER_MODE_OFDM_PA_POWERSETTING_TABLE | PA for all OFDM Sub-GHz dBm values in range, using RAIL_PaPowerSetting_t table. |
| RAIL_TX_POWER_MODE_OFDM_PA | DeprecatedPlease use RAIL_TX_POWER_MODE_OFDM_PA_POWERSETTING_TABLE instead. |
| RAIL_TX_POWER_MODE_NONE | Invalid amplifier Selection. |
RAIL_PaBand_t#
RAIL_PaBand_t
Enum used to specify the band for a PA.
| Enumerator | |
|---|---|
| RAIL_PA_BAND_2P4GIG | Indicates a 2.4GHz band PA. |
| RAIL_PA_BAND_SUBGIG | Indicates a Sub-GHz band PA. |
| RAIL_PA_BAND_COUNT | A count of the choices in this enumeration. |
Typedef Documentation#
RAIL_TxPower_t#
typedef int16_t RAIL_TxPower_t
The transmit power in deci-dBm units (e.g., 4.5 dBm -> 45 deci-dBm).
These values are used by the conversion functions to convert a RAIL_TxPowerLevel_t to deci-dBm for the application consumption. On EFR32, they can range from RAIL_TX_POWER_MIN to RAIL_TX_POWER_MAX.
RAIL_TxPowerLevel_t#
typedef uint8_t RAIL_TxPowerLevel_t
Raw power levels used directly by the RAIL_Get/SetTxPower API where a higher numerical value corresponds to a higher output power.
These are referred to as 'raw (values/units)'. On EFR32, they can range from one of RAIL_TX_POWER_LEVEL_2P4_LP_MIN, RAIL_TX_POWER_LEVEL_2P4_HP_MIN, or RAIL_TX_POWER_LEVEL_SUBGIG_HP_MIN to one of RAIL_TX_POWER_LEVEL_2P4_LP_MAX, RAIL_TX_POWER_LEVEL_2P4_HP_MAX, and RAIL_TX_POWER_LEVEL_SUBGIG_HP_MAX, respectively, depending on the selected RAIL_TxPowerMode_t.
RAIL_PaPowerSetting_t#
typedef uint32_t RAIL_PaPowerSetting_t
PA power setting used directly by the RAIL_GetPaPowerSetting() and RAIL_SetPaPowerSetting() APIs which is decoded to the actual hardware register value(s).
Variable Documentation#
RAIL_PaAutoModeConfig#
const RAIL_PaAutoModeConfigEntry_t* RAIL_PaAutoModeConfig
The actual PA auto mode configuration structure used by the auto mode plugin to control output power.
Function Documentation#
RAIL_ConfigTxPower#
RAIL_Status_t RAIL_ConfigTxPower (RAIL_Handle_t railHandle, const RAIL_TxPowerConfig_t * config)
Initialize TX power settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_TxPowerConfig_t * | [in] | config | An instance which contains desired initial settings for the TX amplifier. |
Returns
RAIL_Status_t indicating success or an error.
These settings include the selection between the multiple TX amplifiers, voltage supplied to the TX power amplifier, and ramp times. This must be called before any transmit occurs or RAIL_SetTxPower is called. While this function should always be called during initialization, it can also be called any time if these settings need to change to adapt to a different application/protocol. This API also resets TX power to RAIL_TX_POWER_LEVEL_INVALID, so RAIL_SetTxPower must be called afterwards.
At times, certain combinations of configurations cannot be achieved. This API attempts to get as close as possible to the requested settings. The following "RAIL_Get..." API can be used to determine what values were set. A change in RAIL_TxPowerConfig_t::rampTime may affect the minimum timings that can be achieved in RAIL_StateTiming_t::idleToTx and RAIL_StateTiming_t::rxToTx. Call RAIL_SetStateTiming() again to check whether these times have changed.
RAIL_GetTxPowerConfig#
RAIL_Status_t RAIL_GetTxPowerConfig (RAIL_Handle_t railHandle, RAIL_TxPowerConfig_t * config)
Get the TX power settings currently used in the amplifier.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPowerConfig_t * | [out] | config | A pointer to memory allocated to hold the current TxPower configuration structure. A NULL configuration will produce undefined behavior. |
Returns
RAIL status variable indicating whether or not the get was successful.
Note that this API does not return the current TX power, which is separately managed by the RAIL_GetTxPower / RAIL_SetTxPower APIs. Use this API to determine which values were set as a result of RAIL_ConfigTxPower.
RAIL_SetTxPower#
RAIL_Status_t RAIL_SetTxPower (RAIL_Handle_t railHandle, RAIL_TxPowerLevel_t powerLevel)
Set the TX power in units of raw units (see rail_chip_specific.h for value ranges).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPowerLevel_t | [in] | powerLevel | Power in chip-specific RAIL_TxPowerLevel_t units. |
Returns
RAIL_Status_t indicating success or an error.
To convert between decibels and the integer values that the registers take, call RAIL_ConvertDbmToRaw. A weak version of this function, which works well with our boards is provided. However, customers using a custom board need to characterize chip operation on that board and override the function to convert appropriately from the desired dB values to raw integer values.
Depending on the configuration used in RAIL_ConfigTxPower, not all power levels are achievable. This API will get as close as possible to the desired power without exceeding it, and calling RAIL_GetTxPower is the only way to know the exact value written.
Calling this function before configuring the PA (i.e., before a successful call to RAIL_ConfigTxPower) will return an error.
RAIL_GetTxPower#
RAIL_TxPowerLevel_t RAIL_GetTxPower (RAIL_Handle_t railHandle)
Return the current power setting of the PA.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
The chip-specific RAIL_TxPowerLevel_t value of the current transmit power.
This API returns the raw value that was set by RAIL_SetTxPower. A weak version of RAIL_ConvertRawToDbm that works with our boards to convert the raw values into actual output dBm values is provided. However, customers using a custom board need to re-characterize the relationship between raw and decibel values and rewrite the provided function.
Calling this function before configuring the PA (i.e., before a successful call to RAIL_ConfigTxPower) will return an error (RAIL_TX_POWER_LEVEL_INVALID).
RAIL_ConvertRawToDbm#
RAIL_TxPower_t RAIL_ConvertRawToDbm (RAIL_Handle_t railHandle, RAIL_TxPowerMode_t mode, RAIL_TxPowerLevel_t powerLevel)
Convert raw values written to registers to decibel value (in units of deci-dBm).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPowerMode_t | [in] | mode | PA mode for which to convert. |
| RAIL_TxPowerLevel_t | [in] | powerLevel | A raw amplifier register value to be converted to deci-dBm. |
Returns
raw amplifier values converted to units of deci-dBm.
A weak version of this function is provided that is tuned to provide accurate values for our boards. For a custom board, the relationship between what is written to the TX amplifier and the actual output power should be re-characterized and implemented in an overriding version of RAIL_ConvertRawToDbm. For minimum code size and best speed, use only raw values with the TxPower API and override this function with a smaller function. In the weak version provided with the RAIL library, railHandle is only used to indicate to the user from where the function was called, so it is OK to use either a real protocol handle, or one of the chip-specific ones, such as RAIL_EFR32_HANDLE.
Although the definitions of this function may change, the signature must be as declared here.
RAIL_ConvertDbmToRaw#
RAIL_TxPowerLevel_t RAIL_ConvertDbmToRaw (RAIL_Handle_t railHandle, RAIL_TxPowerMode_t mode, RAIL_TxPower_t power)
Convert the desired decibel value (in units of deci-dBm) to raw integer values used by the TX amplifier registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPowerMode_t | [in] | mode | PA mode for which to do the conversion. |
| RAIL_TxPower_t | [in] | power | Desired dBm values in units of deci-dBm. |
Returns
deci-dBm value converted to a raw integer value that can be used directly with RAIL_SetTxPower.
A weak version of this function is provided that is tuned to provide accurate values for our boards. For a custom board, the relationship between what is written to the TX amplifier and the actual output power should be characterized and implemented in an overriding version of RAIL_ConvertDbmToRaw. For minimum code size and best speed use only raw values with the TxPower API and override this function with a smaller function. In the weak version provided with the RAIL library, railHandle is only used to indicate to the user from where the function was called, so it is OK to use either a real protocol handle, or one of the chip-specific ones, such as RAIL_EFR32_HANDLE.
Although the definitions of this function may change, the signature must be as declared here.
Note
This function is called from within the RAIL library for comparison between channel limitations and current power. It will throw an assert if you haven't called RAIL_InitTxPowerCurves which initializes the mappings between raw power levels and actual dBm powers. To avoid the assert, ensure that the maxPower of all channel configuration entries is RAIL_TX_POWER_MAX or above, or override this function to always return 255.
RAIL_VerifyTxPowerCurves#
void RAIL_VerifyTxPowerCurves (const struct RAIL_TxPowerCurvesConfigAlt * config)
Verify the TX Power Curves on modules.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const struct RAIL_TxPowerCurvesConfigAlt * | [in] | config | TX Power Curves to use on this module. |
This function only needs to be called when using a module and has no effect otherwise. Transmit will not work before this function is called.
RAIL_SetTxPowerDbm#
RAIL_Status_t RAIL_SetTxPowerDbm (RAIL_Handle_t railHandle, RAIL_TxPower_t power)
Set the TX power in terms of deci-dBm instead of raw power level.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPower_t | [in] | power | A desired deci-dBm power to be set. |
Returns
RAIL Status variable indicate whether setting the power was successful.
This is a utility function for user convenience. Normally, to set TX power in dBm, do the following:
RAIL_TxPower_t power = 100; // 100 deci-dBm, 10 dBm
RAIL_TxPowerConfig_t txPowerConfig;
RAIL_GetTxPowerConfig(railHandle, &txPowerConfig);
// RAIL_ConvertDbmToRaw will be the weak version provided by Silicon Labs
// by default, or the customer version, if overwritten.
RAIL_TxPowerLevel_t powerLevel = RAIL_ConvertDbmToRaw(railHandle,
txPowerConfig.mode,
power);
RAIL_SetTxPower(railHandle, powerLevel);
This function wraps all those calls in a single function with power passed in as a parameter.
RAIL_GetTxPowerDbm#
RAIL_TxPower_t RAIL_GetTxPowerDbm (RAIL_Handle_t railHandle)
Get the TX power in terms of deci-dBm instead of raw power level.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
The current output power in deci-dBm.
This is a utility function for user convenience. Normally, to get TX power in dBm, do the following:
RAIL_TxPowerLevel_t powerLevel = RAIL_GetTxPower(railHandle);
RAIL_TxPowerConfig_t txPowerConfig;
RAIL_GetTxPowerConfig(railHandle, &txPowerConfig);
// RAIL_ConvertRawToDbm will be the weak version provided by Silicon Labs
// by default, or the customer version, if overwritten.
RAIL_TxPower_t power = RAIL_ConvertRawToDbm(railHandle,
txPowerConfig.mode,
powerLevel);
return power;
This function wraps all those calls in a single function with power returned as the result.
RAIL_GetPowerSettingTable#
const RAIL_PaPowerSetting_t * RAIL_GetPowerSettingTable (RAIL_Handle_t railHandle, RAIL_TxPowerMode_t mode, RAIL_TxPower_t * minPower, RAIL_TxPower_t * maxPower, RAIL_TxPowerLevel_t * step)
Get the TX PA power setting table and related values.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPowerMode_t | [in] | mode | PA mode for which to get the powersetting table |
| RAIL_TxPower_t * | [out] | minPower | A pointer to a RAIL_TxPower_t |
| RAIL_TxPower_t * | [out] | maxPower | A pointer to a RAIL_TxPower_t |
| RAIL_TxPowerLevel_t * | [out] | step | In deci-dBm increments. A pointer to a RAIL_TxPowerLevel_t |
Returns
Power setting table start address. When NULL is returned all out params above won't be set.
The number of entries in the table can be calculated based on the minPower, maxPower, and step parameters. For example, for minPower = 115 (11.5 dBm), maxPower = 300 (30 dBm), and step = 1, the number of entries in table would be 186
RAIL_SetPaPowerSetting#
RAIL_Status_t RAIL_SetPaPowerSetting (RAIL_Handle_t railHandle, RAIL_PaPowerSetting_t paPowerSetting, RAIL_TxPower_t minPowerDbm, RAIL_TxPower_t maxPowerDbm, RAIL_TxPower_t currentPowerDbm)
Set the TX PA power setting used to configure the PA hardware for the PA output power determined by RAIL_SetTxPowerDbm().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_PaPowerSetting_t | [in] | paPowerSetting | The desired PA power setting. |
| RAIL_TxPower_t | [in] | minPowerDbm | The minimum power in dBm that the PA can output. |
| RAIL_TxPower_t | [in] | maxPowerDbm | The maximum power in dBm that the PA can output. |
| RAIL_TxPower_t | [in] | currentPowerDbm | The corresponding output power in dBm for this power setting. |
Returns
RAIL Status variable indicate whether setting the PA power setting was successful.
RAIL_GetPaPowerSetting#
RAIL_PaPowerSetting_t RAIL_GetPaPowerSetting (RAIL_Handle_t railHandle)
Get the TX PA power setting, which is used to configure power configurations when the dBm to paPowerSetting mapping table mode is used.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
The current PA power setting.
RAIL_EnablePaAutoMode#
RAIL_Status_t RAIL_EnablePaAutoMode (RAIL_Handle_t railHandle, bool enable)
Enable automatic switching between PAs internally to the RAIL library.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A real (not generic) RAIL instance handle. |
| bool | [in] | enable | Enable or disable PA Auto Mode. |
While PA Automode is enabled, the PA will be chosen and set automatically whenever RAIL_SetTxPowerDbm is called or whenever powers are coerced automatically, internally to the RAIL library during a channel change. While PA Auto Mode is enabled, users cannot call RAIL_ConfigTxPower or RAIL_SetTxPower. When entering auto mode, RAIL_SetTxPowerDbm must be called to specify the desired power. When leaving auto mode, RAIL_ConfigTxPower as well as one of RAIL_SetTxPower or RAIL_SetTxPowerDbm must be called to re-specify the desired PA and power level combination.
Note
: Power conversion curves must be initialized before calling this function. That is, RAIL_ConvertDbmToRaw and RAIL_ConvertRawToDbm most both be able to operate properly to ensure that PA Auto Mode functions correctly. See the PA Conversions plugin or AN1127 for more details.
Returns
Status parameter indicating success of function call.
RAIL_IsPaAutoModeEnabled#
bool RAIL_IsPaAutoModeEnabled (RAIL_Handle_t railHandle)
Query status of PA Auto Mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A real (not generic) RAIL instance handle on which to query PA Auto Mode status. |
Returns
Indicator of whether Auto Mode is enabled (true) or not (false).
RAILCb_PaAutoModeDecision#
RAIL_Status_t RAILCb_PaAutoModeDecision (RAIL_Handle_t railHandle, RAIL_TxPower_t * power, RAIL_TxPowerMode_t * mode, const RAIL_ChannelConfigEntry_t * chCfgEntry)
Callback that decides which PA and power level should be used while in PA auto mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_TxPower_t * | [inout] | power | Pointer to the dBm output power (in deci-dBm, 10*dBm) being requested. The value this points to when the function returns will be applied to the radio. |
| RAIL_TxPowerMode_t * | [out] | mode | Pointer to the RAIL_TxPowerMode_t to be used to achieve the requested power. The value this points to when the function returns will be applied to the radio. |
| const RAIL_ChannelConfigEntry_t * | [in] | chCfgEntry | Pointer to a RAIL_ChannelConfigEntry_t. While switching channels, it will be the entry RAIL is switch to, during a call to RAIL_SetTxPowerDbm, it will be the entry RAIL is already on. Can be NULL if a channel configuration was not set or no valid channels are present. |
Returns
Return status indicating result of function call. If this is anything except RAIL_STATUS_NO_ERROR, neither PA's nor their powers will be configured automatically.
Whatever values mode and powerLevel point to when this function return will be applied to the PA hardware and used for transmits. Note
The mode and power level provided by this function depends on the RAIL_PaAutoModeConfig provided for the chip. The RAIL_PaAutoModeConfig definition for a chip should tend to all the bands supported by the chip and cover the full range of power to find a valid entry for requested power for a specific band.
RAIL_ConfigPaAutoEntry#
RAIL_Status_t RAIL_ConfigPaAutoEntry (RAIL_Handle_t railHandle, const RAIL_PaAutoModeConfigEntry_t * paAutoModeEntry)
Configure the PA auto mode entries.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_PaAutoModeConfigEntry_t * | [in] | paAutoModeEntry | Entries used to configure PA auto mode decision points. |
Returns
Status parameter indicating success of function call.
Macro Definition Documentation#
RAIL_TX_POWER_MAX#
#define RAIL_TX_POWER_MAXValue:
((RAIL_TxPower_t)0x7FFF)
The maximum valid value for a RAIL_TxPower_t.
RAIL_TX_POWER_MIN#
#define RAIL_TX_POWER_MINValue:
((RAIL_TxPower_t)0x8000)
The minimum valid value for a RAIL_TxPower_t.
RAIL_TX_POWER_CURVE_DEFAULT_MAX#
#define RAIL_TX_POWER_CURVE_DEFAULT_MAXValue:
((RAIL_TxPower_t)200)
The maximum power in deci-dBm the curve supports.
RAIL_TX_POWER_CURVE_DEFAULT_INCREMENT#
#define RAIL_TX_POWER_CURVE_DEFAULT_INCREMENTValue:
((RAIL_TxPower_t)40)
The increment step in deci-dBm for calculating power level.
RAIL_TX_POWER_VOLTAGE_SCALING_FACTOR#
#define RAIL_TX_POWER_VOLTAGE_SCALING_FACTORValue:
1000
mV are used for all TX power voltage values.
TX power voltages take and return voltages multiplied by this factor.
RAIL_TX_POWER_DBM_SCALING_FACTOR#
#define RAIL_TX_POWER_DBM_SCALING_FACTORValue:
10
deci-dBm are used for all TX power dBm values.
All dBm inputs to TX power functions take dBm power times this factor.
RAIL_TX_POWER_LEVEL_INVALID#
#define RAIL_TX_POWER_LEVEL_INVALIDValue:
(255U)
Invalid RAIL_TxPowerLevel_t value returned when an error occurs with RAIL_GetTxPower.
RAIL_TX_POWER_LEVEL_MAX#
#define RAIL_TX_POWER_LEVEL_MAXValue:
(254U)
Sentinel value that can be passed to RAIL_SetTxPower to set the highest power level available on the current PA, regardless of which one is selected.
RAIL_TX_PA_POWER_SETTING_UNSUPPORTED#
#define RAIL_TX_PA_POWER_SETTING_UNSUPPORTEDValue:
(0U)
Returned by RAIL_GetPaPowerSetting when the device does not support the dBm to power setting mapping table.
RAIL_TX_POWER_MODE_NAMES#
#define RAIL_TX_POWER_MODE_NAMESValue:
The names of the TX power modes.
A list of the names for the TX power modes on EFR32 parts. This macro is useful for test applications and debugging output.
RAIL_POWER_MODE_IS_ANY_EFF#
#define RAIL_POWER_MODE_IS_ANY_EFFValue:
Convenience macro for any EFF power mode.
RAIL_POWER_MODE_IS_DBM_POWERSETTING_MAPPING_TABLE_OFDM#
#define RAIL_POWER_MODE_IS_DBM_POWERSETTING_MAPPING_TABLE_OFDMValue:
Convenience macro for any OFDM mapping table mode.
RAIL_POWER_MODE_IS_DBM_POWERSETTING_MAPPING_TABLE_SUBGIG#
#define RAIL_POWER_MODE_IS_DBM_POWERSETTING_MAPPING_TABLE_SUBGIGValue:
Convenience macro for any Sub-GHz mapping table mode.
RAIL_POWER_MODE_IS_ANY_DBM_POWERSETTING_MAPPING_TABLE#
#define RAIL_POWER_MODE_IS_ANY_DBM_POWERSETTING_MAPPING_TABLEValue:
Convenience macro for any mapping table mode.
RAIL_POWER_MODE_IS_ANY_OFDM#
#define RAIL_POWER_MODE_IS_ANY_OFDMValue:
(x)
Convenience macro for any OFDM mode.