A configuration for PTI.

Public Attributes#

Packet Trace mode (UART or SPI).

uint32_t

Output baudrate for PTI in Hz.

uint8_t

Data output (DOUT) location for doutPort/Pin.

uint8_t

Data output (DOUT) GPIO port.

uint8_t

Data output (DOUT) GPIO pin.

uint8_t

Data clock (DCLK) location for dclkPort/Pin.

uint8_t

Data clock (DCLK) GPIO port.

uint8_t

Data clock (DCLK) GPIO pin.

uint8_t

Data frame (DFRAME) location for dframePort/Pin.

uint8_t

Data frame (DFRAME) GPIO port.

uint8_t

Data frame (DFRAME) GPIO pin.

Public Attribute Documentation#

mode#

RAIL_PtiMode_t RAIL_PtiConfig_t::mode

Packet Trace mode (UART or SPI).


Definition at line 2396 of file common/rail_types.h

baud#

uint32_t RAIL_PtiConfig_t::baud

Output baudrate for PTI in Hz.


Definition at line 2398 of file common/rail_types.h

doutLoc#

uint8_t RAIL_PtiConfig_t::doutLoc

Data output (DOUT) location for doutPort/Pin.

Only needed on EFR32 Series 1; ignored on other platforms.


Definition at line 2401 of file common/rail_types.h

doutPort#

uint8_t RAIL_PtiConfig_t::doutPort

Data output (DOUT) GPIO port.


Definition at line 2403 of file common/rail_types.h

doutPin#

uint8_t RAIL_PtiConfig_t::doutPin

Data output (DOUT) GPIO pin.


Definition at line 2405 of file common/rail_types.h

dclkLoc#

uint8_t RAIL_PtiConfig_t::dclkLoc

Data clock (DCLK) location for dclkPort/Pin.

Only used in SPI mode. Only needed on EFR32 Series 1; ignored on other platforms.


Definition at line 2408 of file common/rail_types.h

dclkPort#

uint8_t RAIL_PtiConfig_t::dclkPort

Data clock (DCLK) GPIO port.

Only used in SPI mode.


Definition at line 2410 of file common/rail_types.h

dclkPin#

uint8_t RAIL_PtiConfig_t::dclkPin

Data clock (DCLK) GPIO pin.

Only used in SPI mode.


Definition at line 2412 of file common/rail_types.h

dframeLoc#

uint8_t RAIL_PtiConfig_t::dframeLoc

Data frame (DFRAME) location for dframePort/Pin.

Only needed on EFR32 Series 1; ignored on other platforms.


Definition at line 2415 of file common/rail_types.h

dframePort#

uint8_t RAIL_PtiConfig_t::dframePort

Data frame (DFRAME) GPIO port.


Definition at line 2417 of file common/rail_types.h

dframePin#

uint8_t RAIL_PtiConfig_t::dframePin

Data frame (DFRAME) GPIO pin.


Definition at line 2419 of file common/rail_types.h