Calibration#

APIs for calibrating the radio.

IEEE802154 protocol-specific APIs for calibrating the radio.

Bluetooth protocol-specific APIs for calibrating the radio.

The EFR32 supports the Image Rejection (IR) calibration and a temperature-dependent calibration.

These APIs calibrate the radio. The RAIL library determines which calibrations are necessary. Calibrations can be enabled/disabled with the RAIL_CalMask_t parameter.

Some calibrations produce values that can be saved and reapplied to avoid repeating the calibration process.

Calibrations can either be run with RAIL_Calibrate, or with the individual chip-specific calibration routines. An example for running code with RAIL_Calibrate looks like the following:

static RAIL_CalValues_t calValues = RAIL_CALVALUES_UNINIT;

void RAILCb_Event(RAIL_Handle_t railHandle, RAIL_Events_t events) {
  // Omitting other event handlers
  if (events & RAIL_EVENT_CAL_NEEDED) {
    // Run all pending calibrations, and save the results
    RAIL_Calibrate(railHandle, &calValues, RAIL_CAL_ALL_PENDING);
  }
}

Alternatively, if the image rejection calibration for your chip can be determined ahead of time, such as by running the calibration on a separate firmware image on each chip, the following calibration process will result in smaller code.

static uint32_t imageRejection = IRCAL_VALUE;

void RAILCb_Event(RAIL_Handle_t railHandle, RAIL_Events_t events) {
  // Omitting other event handlers
  if (events & RAIL_EVENT_CAL_NEEDED) {
    RAIL_CalMask_t pendingCals = RAIL_GetPendingCal(railHandle);
    // Disable the radio if we have to do an offline calibration
    if (pendingCals & RAIL_CAL_TEMP_VC0) {
      RAIL_CalibrateTemp(railHandle);
    }
    if (pendingCals & RAIL_CAL_ONETIME_IRCAL) {
      RAIL_ApplyIrCalibration(railHandle, imageRejection);
    }
  }
}

The IR calibration can be computed once and stored off or computed each time at startup. Because it is PHY-specific and provides sensitivity improvements, it is highly recommended. The IR calibration should only be run when the radio is IDLE.

The temperature-dependent calibrations are used to recalibrate the synth if the temperature crosses 0C or the temperature delta since the last calibration exceeds 70C while in receive. RAIL will run the VCO calibration automatically upon entering receive or transmit states, so the application can omit this calibration if the stack re-enters receive or transmit with enough frequency to avoid reaching the temperature delta. If the application does not calibrate for temperature, it's possible to miss receive packets due to a drift in the carrier frequency.

Modules#

RAIL_TxIrCalValues_t

RAIL_IrCalValues_t

EFR32

Typedefs#

typedef uint32_t

A calibration mask type.

typedef uint32_t

RAIL_RxIrCalValues_t.

A calibration value structure.

Functions#

RAIL_ConfigCal(RAIL_Handle_t railHandle, RAIL_CalMask_t calEnable)

Initialize RAIL calibration.

RAIL_Calibrate(RAIL_Handle_t railHandle, RAIL_CalValues_t *calValues, RAIL_CalMask_t calForce)

Start the calibration process.

RAIL_GetPendingCal(RAIL_Handle_t railHandle)

Return the current set of pending calibrations.

RAIL_ApplyIrCalibration(RAIL_Handle_t railHandle, uint32_t imageRejection)

Apply a given image rejection calibration value.

RAIL_ApplyIrCalibrationAlt(RAIL_Handle_t railHandle, RAIL_IrCalValues_t *imageRejection, RAIL_AntennaSel_t rfPath)

Apply a given image rejection calibration value.

RAIL_CalibrateIr(RAIL_Handle_t railHandle, uint32_t *imageRejection)

Run the image rejection calibration.

RAIL_CalibrateIrAlt(RAIL_Handle_t railHandle, RAIL_IrCalValues_t *imageRejection, RAIL_AntennaSel_t rfPath)

Run the image rejection calibration.

RAIL_CalibrateTemp(RAIL_Handle_t railHandle)

Run the temperature calibration.

RAIL_CalibrateHFXO(RAIL_Handle_t railHandle, int8_t *crystalPPMError)

Performs HFXO compensation.

void
RAIL_EnablePaCal(bool enable)

Enable/disable the PA calibration.

RAIL_BLE_CalibrateIr(RAIL_Handle_t railHandle, uint32_t *imageRejection)

Calibrate image rejection for Bluetooth Low Energy.

RAIL_IEEE802154_CalibrateIr2p4Ghz(RAIL_Handle_t railHandle, uint32_t *imageRejection)

Calibrate image rejection for IEEE 802.15.4 2.4 GHz.

RAIL_IEEE802154_CalibrateIrSubGhz(RAIL_Handle_t railHandle, uint32_t *imageRejection)

Calibrate image rejection for IEEE 802.15.4 915 MHz and 868 MHz.

Macros#

#define
RAIL_CAL_TEMP_VCO (0x00000001U)

EFR32-specific temperature calibration bit.

#define
RAIL_CAL_TEMP_HFXO (0x00000002U)

EFR32-specific HFXO temperature check bit.

#define
RAIL_CAL_COMPENSATE_HFXO (0x00000004U)

EFR32-specific HFXO compensation bit.

#define
RAIL_CAL_RX_IRCAL (0x00010000U)

EFR32-specific IR calibration bit.

#define
RAIL_CAL_OFDM_TX_IRCAL (0x00100000U)

EFR32-specific Tx IR calibration bit.

#define
RAIL_CAL_ONETIME_IRCAL (RAIL_CAL_RX_IRCAL | RAIL_CAL_OFDM_TX_IRCAL)

A mask to run EFR32-specific IR calibrations.

#define
RAIL_CAL_TEMP (RAIL_CAL_TEMP_VCO | RAIL_CAL_TEMP_HFXO | RAIL_CAL_COMPENSATE_HFXO)

A mask to run temperature-dependent calibrations.

#define
RAIL_CAL_ONETIME (RAIL_CAL_ONETIME_IRCAL)

A mask to run one-time calibrations.

#define
RAIL_CAL_PERF (0)

A mask to run optional performance calibrations.

#define
RAIL_CAL_OFFLINE (RAIL_CAL_ONETIME_IRCAL)

A mask for calibrations that require the radio to be off.

#define
RAIL_CAL_ALL (RAIL_CAL_TEMP | RAIL_CAL_ONETIME)

A mask to run all possible calibrations for this chip.

#define
RAIL_CAL_ALL_PENDING (0x00000000U)

A mask to run all pending calibrations.

#define
RAIL_CAL_INVALID_VALUE (0xFFFFFFFFU)

An invalid calibration value.

#define
RAIL_MAX_RF_PATHS 2

Indicates the maximum number of RF Paths supported across all platforms.

#define
RAIL_IRCALVALUES_RX_UNINIT undefined

A define to set all RAIL_RxIrCalValues_t values to uninitialized.

#define
RAIL_IRCALVALUES_TX_UNINIT undefined

A define to set all RAIL_TxIrCalValues_t values to uninitialized.

#define
RAIL_IRCALVALUES_UNINIT undefined

A define to set all RAIL_IrCalValues_t values to uninitialized.

#define
RAIL_IRCALVAL (irCalStruct, rfPath)

A define allowing Rx calibration value access compatibility between non-OFDM and OFDM platforms.

#define
RAIL_CALVALUES_UNINIT RAIL_IRCALVALUES_UNINIT

A define to set all RAIL_CalValues_t values to uninitialized.

#define
RAIL_PACTUNE_IGNORE (255U)

Use this value with either TX or RX values in RAIL_SetPaCTune to use whatever value is already set and do no update.

Typedef Documentation#

RAIL_CalMask_t#

RAIL_CalMask_t

A calibration mask type.

This type is a bitmask of different RAIL calibration values. The exact meaning of these bits depends on what a particular chip supports.


RAIL_RxIrCalValues_t#

typedef uint32_t RAIL_RxIrCalValues_t[2] [2]

RAIL_RxIrCalValues_t.

RX IR calibration values.

Platforms with fewer RAIL_RF_PATHS than RAIL_MAX_RF_PATHS will only respect and update RAIL_RF_PATHS indices and ignore the rest.


RAIL_CalValues_t#

RAIL_CalValues_t

A calibration value structure.

This structure contains the set of persistent calibration values for EFR32. You can set these beforehand and apply them at startup to save the time required to compute them. Any of these values may be set to RAIL_CAL_INVALID_VALUE to force the code to compute that calibration value.


Function Documentation#

RAIL_ConfigCal#

RAIL_Status_t RAIL_ConfigCal (RAIL_Handle_t railHandle, RAIL_CalMask_t calEnable)

Initialize RAIL calibration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_CalMask_t[in]calEnable

A bitmask that indicates which calibrations to enable for a callback notification. The exact meaning of these bits is chip-specific.

Returns

  • Status code indicating success of the function call.

Calibration initialization provides the calibration settings that correspond to the current radio configuration.


RAIL_Calibrate#

RAIL_Status_t RAIL_Calibrate (RAIL_Handle_t railHandle, RAIL_CalValues_t * calValues, RAIL_CalMask_t calForce)

Start the calibration process.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_CalValues_t *[inout]calValues

A structure of calibration values to apply. If a valid calibration structure is provided and the structure contains valid calibration values, those values will be applied to the hardware and the RAIL library will cache those values for use again later. If a valid calibration structure is provided and the structure contains a calibration value of RAIL_CAL_INVALID_VALUE for the desired calibration, the desired calibration will run, the calibration values structure will be updated with a valid calibration value, and the RAIL library will cache that value for use again later. If a NULL pointer is provided, the desired calibration will run and the RAIL library will cache that value for use again later. However, the valid calibration value will not be returned to the application.

RAIL_CalMask_t[in]calForce

A mask to force specific calibration(s) to execute. To run all pending calibrations, use the value RAIL_CAL_ALL_PENDING. Only the calibrations specified will run, even if not enabled during initialization.

Returns

  • Status code indicating success of the function call.

If calibrations were performed previously and the application saves the calibration values (i.e., call this function with a calibration values structure containing calibration values of RAIL_CAL_INVALID_VALUE before a reset), the application can later bypass the time it would normally take to recalibrate hardware by reusing previous calibration values (i.e., call this function with a calibration values structure containing valid calibration values after a reset).

If multiple protocols are used, this function will make the given railHandle active, if not already, and perform calibration. If called during a protocol switch, to perform an IR calibration for the first time, it will return RAIL_STATUS_INVALID_STATE, in which case the application must defer calibration until after the protocol switch is complete. Silicon Labs recommends calling this function from the application main loop.

Note

  • Instead of this function, consider using the individual chip-specific functions. Using the individual functions will allow for better dead-stripping if not all calibrations are run.

  • Some calibrations should only be executed when the radio is IDLE. See chip-specific documentation for more details.


RAIL_GetPendingCal#

RAIL_CalMask_t RAIL_GetPendingCal (RAIL_Handle_t railHandle)

Return the current set of pending calibrations.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • A mask of all pending calibrations that the user has been asked to perform.

This function returns a full set of pending calibrations. The only way to clear pending calibrations is to perform them using the RAIL_Calibrate() API with the appropriate list of calibrations.


RAIL_ApplyIrCalibration#

RAIL_Status_t RAIL_ApplyIrCalibration (RAIL_Handle_t railHandle, uint32_t imageRejection)

Apply a given image rejection calibration value.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint32_t[in]imageRejection

The image rejection value to apply.

Returns

  • A status code indicating success of the function call.

Take an image rejection calibration value and apply it. This value should be determined from a previous run of RAIL_CalibrateIr on the same physical device with the same radio configuration. The imageRejection value will also be stored to the RAIL_ChannelConfigEntry_t::attr, if possible.

If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. In that case, the caller must attempt to re-call this function later.

DeprecatedPlease use RAIL_ApplyIrCalibrationAlt instead.


RAIL_ApplyIrCalibrationAlt#

RAIL_Status_t RAIL_ApplyIrCalibrationAlt (RAIL_Handle_t railHandle, RAIL_IrCalValues_t * imageRejection, RAIL_AntennaSel_t rfPath)

Apply a given image rejection calibration value.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_IrCalValues_t *[in]imageRejection

Pointer to the image rejection value to apply.

RAIL_AntennaSel_t[in]rfPath

RF path to calibrate.

Returns

  • A status code indicating success of the function call.

Take an image rejection calibration value and apply it. This value should be determined from a previous run of RAIL_CalibrateIrAlt on the same physical device with the same radio configuration. The imageRejection value will also be stored to the RAIL_ChannelConfigEntry_t::attr, if possible. Note

  • : To make sure the imageRejection value is stored/configured correctly, RAIL_ConfigAntenna should be called before calling this API.

If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. In that case, the caller must attempt to re-call this function later.


RAIL_CalibrateIr#

RAIL_Status_t RAIL_CalibrateIr (RAIL_Handle_t railHandle, uint32_t * imageRejection)

Run the image rejection calibration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint32_t *[out]imageRejection

The result of the image rejection calibration.

Returns

  • A status code indicating success of the function call.

Run the image rejection calibration and apply the resulting value. If the imageRejection parameter is not NULL, store the value at that location. The imageRejection value will also be stored to the RAIL_ChannelConfigEntry_t::attr, if possible. This is a long-running calibration that adds significant code space when run and can be run with a separate firmware image on each device to save code space in the final image.

If multiple protocols are used, this function will make the given railHandle active, if not already, and perform calibration. If called during a protocol switch, it will return RAIL_STATUS_INVALID_STATE. In this case, RAIL_ApplyIrCalibration may be called to apply a previously determined IR calibration value, or the app must defer calibration until the protocol switch is complete. Silicon Labs recommends calling this function from the application main loop.

DeprecatedPlease use RAIL_CalibrateIrAlt instead.


RAIL_CalibrateIrAlt#

RAIL_Status_t RAIL_CalibrateIrAlt (RAIL_Handle_t railHandle, RAIL_IrCalValues_t * imageRejection, RAIL_AntennaSel_t rfPath)

Run the image rejection calibration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_IrCalValues_t *[out]imageRejection

Pointer to the image rejection result.

RAIL_AntennaSel_t[in]rfPath

RF path to calibrate.

Returns

  • A status code indicating success of the function call.

Run the image rejection calibration and apply the resulting value. If the imageRejection parameter is not NULL, store the value at that location. The imageRejection value will also be stored to the RAIL_ChannelConfigEntry_t::attr, if possible. This is a long-running calibration that adds significant code space when run and can be run with a separate firmware image on each device to save code space in the final image. Note

  • : To make sure the imageRejection value is stored/configured correctly, RAIL_ConfigAntenna should be called before calling this API.

If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. In that case, the caller must attempt to re-call this function later.


RAIL_CalibrateTemp#

RAIL_Status_t RAIL_CalibrateTemp (RAIL_Handle_t railHandle)

Run the temperature calibration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • A status code indicating success of the function call.

Run the temperature calibration, which needs to recalibrate the synth if the temperature crosses 0C or the temperature delta since the last calibration exceeds 70C while in receive. RAIL will run the VCO calibration automatically upon entering receive or transmit states, so the application can omit this calibration if the stack re-enters receive or transmit with enough frequency to avoid reaching the temperature delta. If the application does not calibrate for temperature, it's possible to miss receive packets due to a drift in the carrier frequency.

If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. In that case, the calibration will be automatically performed next time the radio enters receive.


RAIL_CalibrateHFXO#

RAIL_Status_t RAIL_CalibrateHFXO (RAIL_Handle_t railHandle, int8_t * crystalPPMError)

Performs HFXO compensation.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

int8_t *[out]crystalPPMError

Current deviation that has been corrected, measured in PPM. May be NULL.

Returns

  • A status code indicating the result of the function call.

Compute the PPM correction using the thermistor value available when RAIL_EVENT_THERMISTOR_DONE occurs, after RAIL_StartThermistorMeasurement() call. Then correct the RF frequency as well as TX and RX sampling.

This function calls the following RAIL functions in sequence saving having to call them individually:

Note

  • This function makes the radio idle.


RAIL_EnablePaCal#

void RAIL_EnablePaCal (bool enable)

Enable/disable the PA calibration.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

Enables/disables the PA calibration.

Enabling will ensure that the PA power remains constant chip-to-chip. By default, this feature is disabled after reset.

Note


RAIL_BLE_CalibrateIr#

RAIL_Status_t RAIL_BLE_CalibrateIr (RAIL_Handle_t railHandle, uint32_t * imageRejection)

Calibrate image rejection for Bluetooth Low Energy.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint32_t *[out]imageRejection

The result of the image rejection calibration.

Returns

  • A status code indicating success of the function call.

Some chips have protocol-specific image rejection calibrations programmed into their flash. This function will either get the value from flash and apply it, or run the image rejection algorithm to find the value.


RAIL_IEEE802154_CalibrateIr2p4Ghz#

RAIL_Status_t RAIL_IEEE802154_CalibrateIr2p4Ghz (RAIL_Handle_t railHandle, uint32_t * imageRejection)

Calibrate image rejection for IEEE 802.15.4 2.4 GHz.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint32_t *[out]imageRejection

The result of the image rejection calibration.

Returns

  • A status code indicating success of the function call.

Some chips have protocol-specific image rejection calibrations programmed into their flash. This function will either get the value from flash and apply it, or run the image rejection algorithm to find the value.


RAIL_IEEE802154_CalibrateIrSubGhz#

RAIL_Status_t RAIL_IEEE802154_CalibrateIrSubGhz (RAIL_Handle_t railHandle, uint32_t * imageRejection)

Calibrate image rejection for IEEE 802.15.4 915 MHz and 868 MHz.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint32_t *[out]imageRejection

The result of the image rejection calibration.

Returns

  • A status code indicating success of the function call.

Some chips have protocol-specific image rejection calibrations programmed into their flash. This function will either get the value from flash and apply it, or run the image rejection algorithm to find the value.

DeprecatedPlease use RAIL_CalibrateIrAlt instead.