Allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().
Public Attributes#
bool
Enable synchronous RX DOUT using DCLK vs.
bool
Enable synchronous TX DIN using DCLK vs.
uint8_t
RX Data output (DOUT) GPIO port.
uint8_t
RX Data output (DOUT) GPIO pin.
uint8_t
Data clock (DCLK) GPIO port.
uint8_t
Data clock (DCLK) GPIO pin.
uint8_t
TX Data input (DIN) GPIO port.
uint8_t
TX Data input (DIN) GPIO pin.
uint8_t
uint8_t
uint8_t
Public Attribute Documentation#
syncRx#
bool RAIL_DirectModeConfig_t::syncRx
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
syncTx#
bool RAIL_DirectModeConfig_t::syncTx
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
dclkPort#
uint8_t RAIL_DirectModeConfig_t::dclkPort
Data clock (DCLK) GPIO port.
Only used in synchronous mode.
dclkPin#
uint8_t RAIL_DirectModeConfig_t::dclkPin
Data clock (DCLK) GPIO pin.
Only used in synchronous mode.