Allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().
Public Attributes#
Enable synchronous RX DOUT using DCLK vs.
Enable synchronous TX DIN using DCLK vs.
RX Data output (DOUT) GPIO port.
RX Data output (DOUT) GPIO pin.
Data clock (DCLK) GPIO port.
Data clock (DCLK) GPIO pin.
TX Data input (DIN) GPIO port.
TX Data input (DIN) GPIO pin.
Public Attribute Documentation#
syncRx#
bool RAIL_DirectModeConfig_t::syncRx
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
5486
of file common/rail_types.h
syncTx#
bool RAIL_DirectModeConfig_t::syncTx
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
5488
of file common/rail_types.h
doutPort#
uint8_t RAIL_DirectModeConfig_t::doutPort
RX Data output (DOUT) GPIO port.
5491
of file common/rail_types.h
doutPin#
uint8_t RAIL_DirectModeConfig_t::doutPin
RX Data output (DOUT) GPIO pin.
5493
of file common/rail_types.h
dclkPort#
uint8_t RAIL_DirectModeConfig_t::dclkPort
Data clock (DCLK) GPIO port.
Only used in synchronous mode.
5496
of file common/rail_types.h
dclkPin#
uint8_t RAIL_DirectModeConfig_t::dclkPin
Data clock (DCLK) GPIO pin.
Only used in synchronous mode.
5498
of file common/rail_types.h
dinPort#
uint8_t RAIL_DirectModeConfig_t::dinPort
TX Data input (DIN) GPIO port.
5501
of file common/rail_types.h
dinPin#
uint8_t RAIL_DirectModeConfig_t::dinPin
TX Data input (DIN) GPIO pin.
5503
of file common/rail_types.h
doutLoc#
uint8_t RAIL_DirectModeConfig_t::doutLoc
DeprecatedNo longer used (ignored).
5506
of file common/rail_types.h
dclkLoc#
uint8_t RAIL_DirectModeConfig_t::dclkLoc
DeprecatedNo longer used (ignored).
5508
of file common/rail_types.h
dinLoc#
uint8_t RAIL_DirectModeConfig_t::dinLoc
DeprecatedNo longer used (ignored).
5510
of file common/rail_types.h