You are viewing documentation for version:
Contains RAIL Library Version Information.
It is filled in by RAIL_GetVersion().
Public Attributes#
bool
Boolean to indicate whether this is a multiprotocol library or not.
Public Attribute Documentation#
hash#
uint32_t RAIL_Version_t::hash
Git hash.
Definition at line 85
of file common/rail_types.h
major#
uint8_t RAIL_Version_t::major
Major number.
Definition at line 87
of file common/rail_types.h
minor#
uint8_t RAIL_Version_t::minor
Minor number.
Definition at line 89
of file common/rail_types.h
rev#
uint8_t RAIL_Version_t::rev
Revision number.
Definition at line 91
of file common/rail_types.h
build#
uint8_t RAIL_Version_t::build
Build number.
Definition at line 93
of file common/rail_types.h
flags#
uint8_t RAIL_Version_t::flags
Build flags.
Definition at line 95
of file common/rail_types.h
multiprotocol#
bool RAIL_Version_t::multiprotocol
Boolean to indicate whether this is a multiprotocol library or not.
Definition at line 97
of file common/rail_types.h