Data link layer header (first block)
Public Attributes#
uint8_t
Length field.
uint8_t
Control field raw mode.
Control field function code.
bool
Control field fcv/dcf.
bool
Control field fcb/acd.
bool
Control field, primary station bit.
struct sl_rail_sdk_wmbus_dll_header_t::@0::@2
Control field detailed mode.
union sl_rail_sdk_wmbus_dll_header_t::@0
Control field.
uint16_t
Address, manufacturer ID.
uint32_t
Address, device ID.
uint8_t
Address, version.
uint8_t
Address, device type.
struct sl_rail_sdk_wmbus_dll_header_t::@1::@3
Address field detailed mode.
union sl_rail_sdk_wmbus_dll_header_t::@1
Address field.
Public Attribute Documentation#
lField#
uint8_t sl_rail_sdk_wmbus_dll_header_t::lField
Length field.
Definition at line
189
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
raw#
uint8_t sl_rail_sdk_wmbus_dll_header_t::raw[8]
Control field raw mode.
Address field raw mode.
Definition at line
191
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
function_code#
sl_rail_sdk_wmbus_function_code_t sl_rail_sdk_wmbus_dll_header_t::function_code
Control field function code.
Definition at line
193
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
fcv_dcf#
bool sl_rail_sdk_wmbus_dll_header_t::fcv_dcf
Control field fcv/dcf.
Definition at line
194
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
fcb_acd#
bool sl_rail_sdk_wmbus_dll_header_t::fcb_acd
Control field fcb/acd.
Definition at line
195
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
primary#
bool sl_rail_sdk_wmbus_dll_header_t::primary
Control field, primary station bit.
Definition at line
196
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
detailed#
struct sl_rail_sdk_wmbus_dll_header_t::@0::@2 sl_rail_sdk_wmbus_dll_header_t::detailed
Control field detailed mode.
Definition at line
197
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
c_field#
union sl_rail_sdk_wmbus_dll_header_t::@0 sl_rail_sdk_wmbus_dll_header_t::c_field
Control field.
Definition at line
198
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
manufacturer#
uint16_t sl_rail_sdk_wmbus_dll_header_t::manufacturer
Address, manufacturer ID.
Definition at line
202
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
id#
uint32_t sl_rail_sdk_wmbus_dll_header_t::id
Address, device ID.
Definition at line
203
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
version#
uint8_t sl_rail_sdk_wmbus_dll_header_t::version
Address, version.
Definition at line
204
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
device_type#
uint8_t sl_rail_sdk_wmbus_dll_header_t::device_type
Address, device type.
Definition at line
205
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
detailed#
struct sl_rail_sdk_wmbus_dll_header_t::@1::@3 sl_rail_sdk_wmbus_dll_header_t::detailed
Address field detailed mode.
Definition at line
206
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h
address#
union sl_rail_sdk_wmbus_dll_header_t::@1 sl_rail_sdk_wmbus_dll_header_t::address
Address field.
Definition at line
207
of file /mnt/raid/workspaces/ws.jprnpkXRl/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h