Wireless M-Bus Support#
The Wireless M-Bus Support component adds minimalist support for coding and decoding Wireless M-Bus packets. This component is essential for applications that need to communicate using the Wireless M-Bus protocol, providing the necessary tools to handle packet formatting and interpretation.
Key Features:
Packet Coding and Decoding: Functions to encode and decode Wireless M-Bus packets, ensuring correct data formatting for transmission and reception.
Function Codes: Defines a set of function codes used in the first block's C-field, such as WMBUS_FUNCTION_SND_NKE, WMBUS_FUNCTION_SND_UD, and WMBUS_FUNCTION_SND_NR.
Device Types: Supports various device types used in address fields, including oil meters, electricity meters, gas meters, and more.
Manufacturer ID: Functions to retrieve the manufacturer ID (M-field) for M-Bus addressing.
Encryption and Decryption: Includes functions for encrypting and decrypting Wireless M-Bus frames using the Crypto5 algorithm.
Modules#
Functions#
Runs the required software based phy processes on the buffer, depending on the mode.
Get the current Wireless M-Bus accessibility settings.
Set the current Wireless M-Bus accessibility settings.
Initializes the MBUS and its mode.
Sets the MBUS mode to use.
Gets the selected Wireless M-Bus mode.
Returns the delay after TX when RX should start in limited accessibility sl_rail_sdk_wmbus_set_mode should be called before using this function.
Returns the delay after TX when RX should stop in limited accessibility sl_rail_sdk_wmbus_set_mode should be called before using this function.
Helper function for building the payload of a Wireless M-Bus frame.
Helper function for building the payload of a Wireless M-Bus frame.
Helper function for building the payload of a Wireless M-Bus frame.
Helper function for building the payload of a Wireless M-Bus frame.
Helper function for converting uppercase ASCII letters to 2B manufacturer ID.
Helper function for converting 2B manufacturer ID to 3 uppercase ASCII letter.
Initializes crypto engine.
Sets key for mode5 encryption/decryption (AES-CBC)
Returns key for mode5 encryption/decryption (AES-CBC)
Encrypts blocks using mode5 (AES-CBC) encryption.
Decrypts blocks using mode5 (AES-CBC) encryption.
Sets up a Wireless M-Bus frame.
Function Documentation#
sl_rail_sdk_wmbus_phy_software#
uint16_t sl_rail_sdk_wmbus_phy_software (uint8_t * buffer, uint8_t length, uint16_t buffer_length)
Runs the required software based phy processes on the buffer, depending on the mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [inout] | buffer | The buffer that holds the data, and what will hold the processed data |
| uint8_t | [in] | length | Length of the input buffer |
| uint16_t | [in] | buffer_length | Size of the buffer, to prevent writing outside of the buffer |
The buffer must be big enough to hold the processed data. Currently, only T mode's Meter to Other requires software based crc and 3of6 encoding. For that, the buffer should be at 436B long for the longest packet. All other modes passes through this call without modifications sl_rail_sdk_wmbus_set_mode should be called before using this function.
Returns
The length of the processed packet, that can be passed to the hardware, or 0 on error
sl_rail_sdk_wmbus_get_accessibility#
sl_rail_sdk_wmbus_accessibility_t sl_rail_sdk_wmbus_get_accessibility (void )
Get the current Wireless M-Bus accessibility settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
the current value
sl_rail_sdk_wmbus_set_accessibility#
void sl_rail_sdk_wmbus_set_accessibility (sl_rail_sdk_wmbus_accessibility_t new_wmbus_accessibility)
Set the current Wireless M-Bus accessibility settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_sdk_wmbus_accessibility_t | [in] | new_wmbus_accessibility | to be applied |
sl_rail_sdk_wmbus_init#
void sl_rail_sdk_wmbus_init (void )
Initializes the MBUS and its mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_rail_sdk_wmbus_set_mode#
void sl_rail_sdk_wmbus_set_mode (sl_rail_sdk_wmbus_mode_t mode)
Sets the MBUS mode to use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_sdk_wmbus_mode_t | [in] | mode | is the desired mode of the Wireless M-Bus |
Currently only used to init and enable GPCRC for T mode Tx, and it also changes the time returned by sl_rail_sdk_wmbus_get_meter_limited_acc_rx_start().
sl_rail_sdk_wmbus_get_selected_mode#
sl_rail_sdk_wmbus_mode_t sl_rail_sdk_wmbus_get_selected_mode (void )
Gets the selected Wireless M-Bus mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The selected mode of the Wireless M-Bus
sl_rail_sdk_wmbus_get_meter_limited_acc_rx_start#
uint32_t sl_rail_sdk_wmbus_get_meter_limited_acc_rx_start (bool slowMode)
Returns the delay after TX when RX should start in limited accessibility sl_rail_sdk_wmbus_set_mode should be called before using this function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | slowMode | True in case of slow mode. Only used in mode C and F |
Returns
The delay in microseconds
sl_rail_sdk_wmbus_get_meter_limited_acc_rx_stop#
uint32_t sl_rail_sdk_wmbus_get_meter_limited_acc_rx_stop (bool slowMode)
Returns the delay after TX when RX should stop in limited accessibility sl_rail_sdk_wmbus_set_mode should be called before using this function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | slowMode | True in case of slow mode. Only used in mode C and F |
Returns
The delay in microseconds
sl_rail_sdk_wmbus_frame_add_payload_int8#
uint8_t sl_rail_sdk_wmbus_frame_add_payload_int8 (uint8_t * buffer, sl_rail_sdk_wmbus_frame_dib_function_t dibFunction, uint8_t vib, int8_t value)
Helper function for building the payload of a Wireless M-Bus frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | buffer | The buffer to write into. Should point at the first free byte |
| sl_rail_sdk_wmbus_frame_dib_function_t | [in] | dibFunction | Function field in the DIB (Data Information Block) |
| uint8_t | [in] | vib | Value information block containing the VIF (Value Information Field) |
| int8_t | [in] | value | The value of the data block. |
Adds an 8 bit integer (binary) data block to a buffer. Returns
the number of bytes written into buffer
sl_rail_sdk_wmbus_frame_add_payload_int16#
uint8_t sl_rail_sdk_wmbus_frame_add_payload_int16 (uint8_t * buffer, sl_rail_sdk_wmbus_frame_dib_function_t dibFunction, uint8_t vib, int16_t value)
Helper function for building the payload of a Wireless M-Bus frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | buffer | The buffer to write into. Should point at the first free byte |
| sl_rail_sdk_wmbus_frame_dib_function_t | [in] | dibFunction | Function field in the DIB (Data Information Block) |
| uint8_t | [in] | vib | Value information block containing the VIF (Value Information Field) |
| int16_t | [in] | value | The value of the data block. |
Adds a 16 bit integer (binary) data block to a buffer. Returns
the number of bytes written into buffer
sl_rail_sdk_wmbus_frame_add_payload_int32#
uint8_t sl_rail_sdk_wmbus_frame_add_payload_int32 (uint8_t * buffer, sl_rail_sdk_wmbus_frame_dib_function_t dibFunction, uint8_t vib, int32_t value)
Helper function for building the payload of a Wireless M-Bus frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | buffer | The buffer to write into. Should point at the first free byte |
| sl_rail_sdk_wmbus_frame_dib_function_t | [in] | dibFunction | Function field in the DIB (Data Information Block) |
| uint8_t | [in] | vib | Value information block containing the VIF (Value Information Field) |
| int32_t | [in] | value | The value of the data block. |
Adds a 32 bit integer (binary) data block to a buffer. Returns
the number of bytes written into buffer
sl_rail_sdk_wmbus_frame_add_idle_filler#
uint16_t sl_rail_sdk_wmbus_frame_add_idle_filler (uint8_t * buffer, uint16_t fillerLength)
Helper function for building the payload of a Wireless M-Bus frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | buffer | The buffer to write into. Should point at the first free byte |
| uint16_t | [in] | fillerLength | Number of bytes to fill. |
Adds filler bytes required before encryption Returns
the number of bytes written into buffer
sl_rail_sdk_wmbus_frame_chars_to_mfield#
uint16_t sl_rail_sdk_wmbus_frame_chars_to_mfield (const char * manuf)
Helper function for converting uppercase ASCII letters to 2B manufacturer ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | [in] | manuf | Pointer to a 3 element char array, containing the uppercase letters of the manufacturer assigned by also known as DLMS FLAG ID |
Returns
the manufacturer id (or M-field) for M-Bus addressing
sl_rail_sdk_wmbus_frame_mfield_to_chars#
void sl_rail_sdk_wmbus_frame_mfield_to_chars (const uint16_t mfield, char * manuf)
Helper function for converting 2B manufacturer ID to 3 uppercase ASCII letter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint16_t | [in] | mfield | mfield value |
| char * | [out] | manuf | pointer to a 3 element char array to write the 3 letters |
sl_rail_sdk_wmbus_frame_crypto5_init#
void sl_rail_sdk_wmbus_frame_crypto5_init (void )
Initializes crypto engine.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_rail_sdk_wmbus_frame_crypto5_set_key#
void sl_rail_sdk_wmbus_frame_crypto5_set_key (const uint8_t * newKey)
Sets key for mode5 encryption/decryption (AES-CBC)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | newKey | 16B array containing the new key |
sl_rail_sdk_wmbus_frame_crypto5_get_key#
void sl_rail_sdk_wmbus_frame_crypto5_get_key (uint8_t * key)
Returns key for mode5 encryption/decryption (AES-CBC)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | key | Copy of the current key |
sl_rail_sdk_wmbus_frame_crypto5_encrypt#
uint8_t sl_rail_sdk_wmbus_frame_crypto5_encrypt (uint8_t * input, uint8_t * output, uint8_t * iv, uint16_t length, uint8_t encryptedBlocks)
Encrypts blocks using mode5 (AES-CBC) encryption.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | input | Input data. Should be at least 16B*encryptedBlocks long. |
| uint8_t * | [out] | output | Output data. Should be at least 16B*encryptedBlocks long. Can be the same as input. |
| uint8_t * | [inout] | iv | Initialization vector, 16B long |
| uint16_t | [in] | length | Length of the input data |
| uint8_t | [in] | encryptedBlocks | Number of blocks to encode. If 0, all data will be encoded based on length |
Also adds padding if needed, but the payload should include the 2B AES check (0x2f2f) in the beginning of the payload
Returns
the number of blocks encoded. Output length is 16 times this value.
sl_rail_sdk_wmbus_frame_crypto5_decrypt#
void sl_rail_sdk_wmbus_frame_crypto5_decrypt (uint8_t * input, uint8_t * output, uint8_t * iv, uint16_t length)
Decrypts blocks using mode5 (AES-CBC) encryption.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | input | Input data. Should be at least length long. |
| uint8_t * | [out] | output | Output data. Should be at least length long. Can be the same as input. |
| uint8_t * | [inout] | iv | Initialization vector, 16B long |
| uint16_t | [in] | length | Length of the input data. Should be divisible by 16 |
sl_rail_sdk_wmbus_setup_frame#
uint16_t sl_rail_sdk_wmbus_setup_frame (uint8_t * buffer, uint8_t access_number, sl_rail_sdk_wmbus_accessibility_t accessibility, sl_rail_sdk_wmbus_device_type_t new_device_type, sl_rail_sdk_wmbus_sensor_data_t * sensors_data, bool periodic, bool encrypt)
Sets up a Wireless M-Bus frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | buffer | The buffer to store the Wireless M-Bus frame. |
| uint8_t | [in] | access_number | The access number of the frame. |
| sl_rail_sdk_wmbus_accessibility_t | [in] | accessibility | The accessibility of the frame. |
| sl_rail_sdk_wmbus_device_type_t | [in] | new_device_type | The device type of the frame. |
| sl_rail_sdk_wmbus_sensor_data_t * | [in] | sensors_data | An array of data to be included in the frame. |
| bool | [in] | periodic | Indicates whether the frame is periodic or not. |
| bool | [in] | encrypt | Indicates whether the frame should be encrypted or not. |
Sets up a Wireless M-Bus frame by populating the provided buffer with the necessary information.
Returns
The length of the assembled frame.