Type definitions#
Modules#
sl_rail_sdk_wmbus_dll_header_t
sl_rail_sdk_wmbus_stl_header_t
sl_rail_sdk_wmbus_ltl_header_t
sl_rail_sdk_wmbus_sensor_data_t
Enumerations#
Function code to use in the first block's C-field.
Device type to be used in the address field(s)
CI field codes.
Application errors coded into the status field.
Accessibility settings in the config word.
Values for function field in DIB.
MBUS modes.
Enumeration Documentation#
sl_rail_sdk_wmbus_function_code_t#
sl_rail_sdk_wmbus_function_code_t
Function code to use in the first block's C-field.
| Enumerator | |
|---|---|
| WMBUS_FUNCTION_SND_NKE | SND-NKE. | 
| WMBUS_FUNCTION_SND_UD | SND-UD/SND-UD2. | 
| WMBUS_FUNCTION_SND_NR | SND-NR. | 
| WMBUS_FUNCTION_SND_IR | SND-IR. | 
| WMBUS_FUNCTION_ACC_NR | ACC-NR. | 
| WMBUS_FUNCTION_ACC_DMD | ACC-DMD. | 
| WMBUS_FUNCTION_REQ_UD1 | REQ-UD1. | 
| WMBUS_FUNCTION_REQ_UD2 | REQ-UD2. | 
sl_rail_sdk_wmbus_device_type_t#
sl_rail_sdk_wmbus_device_type_t
Device type to be used in the address field(s)
| Enumerator | |
|---|---|
| WMBUS_DEVICE_OTHER | Other. | 
| WMBUS_DEVICE_OIL_METER | Oil meter. | 
| WMBUS_DEVICE_ELECTRICITY_METER | Electricity meter. | 
| WMBUS_DEVICE_GAS_METER | Gas meter. | 
| WMBUS_DEVICE_HEAT_METER | Heat meter. | 
| WMBUS_DEVICE_STEAM_METER | Steam meter. | 
| WMBUS_DEVICE_WARM_WATER_METER | Warm water meter (30-90C) | 
| WMBUS_DEVICE_WATER_METER | Water meter. | 
| WMBUS_DEVICE_HEAT_COST_ALLOCATOR | Heat cost allocator. | 
| WMBUS_DEVICE_COMPRESSED_AIR | Compressed air. | 
| WMBUS_DEVICE_COOLING_METER_OUTLET | Cooling meter (volume measured at return temperature: outlet) | 
| WMBUS_DEVICE_COOLING_METER_INLET | Cooling meter (volume measured at flow temperature: inlet) | 
| WMBUS_DEVICE_HEAT_METER_INLET | Heat meter (volume measured at flow temperature: inlet) | 
| WMBUS_DEVICE_COMBINED_HEAT_COOLING_METER | Combined heat/cooling meter. | 
| WMBUS_DEVICE_BUS_SYSTEM_COMPONENT | Bus/system component. | 
| WMBUS_DEVICE_CALORIFIC_VALUE | Calorific value. | 
| WMBUS_DEVICE_HOT_WATER_METER | Hot water meter (>90C) | 
| WMBUS_DEVICE_COLD_WATER_METER | Cold water meter. | 
| WMBUS_DEVICE_DUAL_WATER_METER | Dual register (hot/cold) water meter. | 
| WMBUS_DEVICE_PRESSURE_METER | Pressure meter. | 
| WMBUS_DEVICE_AD_CONVERTER | A/D converter. | 
| WMBUS_DEVICE_SMOKE_DETECTOR | Smoke detector. | 
| WMBUS_DEVICE_ROOM_SENSOR | Room sensor (e.g. | 
| WMBUS_DEVICE_GAS_DETECTOR | Gas detector. | 
| WMBUS_DEVICE_BREAKER | Breaker (electricity) | 
| WMBUS_DEVICE_VALVE | Valve (gas or water) | 
| WMBUS_DEVICE_CUSTOMER_UNIT | Customer unit (display device) | 
| WMBUS_DEVICE_WASTE_WATER_METER | Waste water meter. | 
| WMBUS_DEVICE_GARBAGE | Garbage. | 
| WMBUS_DEVICE_CARBON_DIOXIDE | Reserved for carbon dioxide. | 
| WMBUS_DEVICE_COMMUNICATION_CONTROLLER | Communication controller (Gateway) | 
| WMBUS_DEVICE_UNIDIRECTIONAL_REPEATER | Unidirectional repeater. | 
| WMBUS_DEVICE_BIDIRECTIONAL_REPEATER | Bidirectional repeater. | 
| WMBUS_DEVICE_RADIO_CONVERTER_SYSTEM | Radio converter (system side) | 
| WMBUS_DEVICE_RADIO_CONVERTER_METER | Radio converter (meter side) | 
sl_rail_sdk_wmbus_ci_field_t#
sl_rail_sdk_wmbus_ci_field_t
CI field codes.
| Enumerator | |
|---|---|
| WMBUS_CI_DATA_TO_METER_NONE | Data sent by readout device to the Meter without transport layer. | 
| WMBUS_CI_MBUS_DATA_TO_METER_SHORT | MBUS data sent by readout device to the Meter with short transport layer. | 
| WMBUS_CI_MBUS_DATA_TO_METER_LONG | MBUS data sent by readout device to the Meter with long transport layer. | 
| WMBUS_CI_COSEM_DATA_TO_METER_LONG | COSEM data sent by readout device to the Meter with long transport layer. | 
| WMBUS_CI_COSEM_DATA_TO_METER_SHORT | COSEM data sent by readout device to the Meter with short transport layer. | 
| WMBUS_CI_OBIS_DATA_TO_METER_LONG | OBIS based data sent by readout device to the Meter with long transport layer. | 
| WMBUS_CI_OBIS_DATA_TO_METER_SHORT | OBIS based data sent by readout device to the Meter with short transport layer. | 
| WMBUS_CI_EN13757_3_DATA_TO_METER_NONE | EN13757-3 application layer with Format frame and no transport layer. | 
| WMBUS_CI_EN13757_3_DATA_TO_METER_SHORT | EN13757-3 application layer with Format frame and short transport layer. | 
| WMBUS_CI_EN13757_3_DATA_TO_METER_LONG | EN13757-3 application layer with Format frame and long transport layer. | 
| WMBUS_CI_CLOCK_SYNC_ABSOLUTE | Clock synchronisation (absolute) | 
| WMBUS_CI_CLOCK_SYNC_RELATIVE | Clock synchronisation (relative) | 
| WMBUS_CI_APPLICATION_ERROR_SHORT | Application error from Meter with short transport layer. | 
| WMBUS_CI_APPLICATION_ERROR_LONG | Application error from Meter with long transport layer. | 
| WMBUS_CI_APPLICATION_ERROR_NONE | Application error from Meter with no transport layer. | 
| WMBUS_CI_ALARM_NONE | Alarm from Meter without transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_LONG | EN13757-3 application layer with long transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_CF_LONG | EN13757-3 application layer with compact frame and long transport layer. | 
| WMBUS_CI_ALARM_SHORT | Alarm from Meter with short transport layer. | 
| WMBUS_CI_ALARM_LONG | Alarm from Meter with long transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_NONE | EN13757-3 application layer with no transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_CF_NONE | EN13757-3 application layer with compact frame and no transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_SHORT | EN13757-3 application layer with short transport layer. | 
| WMBUS_CI_EN13757_3_APPLICATION_CF_SHORT | EN13757-3 application layer with compact frame and short transport layer. | 
| WMBUS_CI_COSEM_APPLICATION_LONG | COSEM application layer with long transport layer. | 
| WMBUS_CI_COSEM_APPLICATION_SHORT | COSEM application layer with short transport layer. | 
| WMBUS_CI_OBIS_APPLICATION_LONG | OBIS based application layer with long transport layer. | 
| WMBUS_CI_OBIS_APPLICATION_SHORT | OBIS based application layer with short transport layer. | 
| WMBUS_CI_EN13757_3_TRANSPORT_TO_METER_LONG | EN13757-3 Transport layer (long) from readout device to the meter. | 
| WMBUS_CI_NETWORK_LAYER_DATA | Network layer data. | 
| WMBUS_CI_FOR_FUTURE_USE | For future use. | 
| WMBUS_CI_NETWORK_MANAGEMENT_APPLICATION | Network management application. | 
| WMBUS_CI_TRANSPORT_TO_METER_MBUS_COMPACT | Transport layer to Meter (M Bus-Compact frame expected) | 
| WMBUS_CI_NETWORK_MANAGEMENT_DATA | Reserved for Network management data (EN 13757-5) | 
| WMBUS_CI_EN13757_3_TRANSPORT_FROM_METER_SHORT | EN13757-3 Transport layer (short) from the meter to the readout device. | 
| WMBUS_CI_EN13757_3_TRANSPORT_FROM_METER_LONG | EN13757-3 Transport layer (long) from the meter to the readout device. | 
| WMBUS_CI_EXTENDED_LINK_LAYER1 | Extended Link Layer I (2B) | 
| WMBUS_CI_EXTENDED_LINK_LAYER2 | Extended Link Layer II (8B) | 
| WMBUS_CI_EXTENDED_LINK_LAYER3 | Extended Link Layer III (10B) | 
| WMBUS_CI_EXTENDED_LINK_LAYER4 | Extended Link Layer IV (16B) | 
sl_rail_sdk_wmbus_status_t#
sl_rail_sdk_wmbus_status_t
Application errors coded into the status field.
| Enumerator | |
|---|---|
| WMBUS_STATUS_APPLICATION_BUSY | Application busy. | 
| WMBUS_STATUS_APPLICATION_ERROR | Any application error. | 
| WMBUS_STATUS_ABNORMAL_CONDITION | Abnormal condition/alarm. | 
| WMBUS_STATUS_POWER_LOW | Power low. | 
| WMBUS_STATUS_PERMANENT_ERROR | Permanent error. | 
| WMBUS_STATUS_TEMPORARY_ERROR | Temporary error. | 
sl_rail_sdk_wmbus_accessibility_t#
sl_rail_sdk_wmbus_accessibility_t
Accessibility settings in the config word.
| Enumerator | |
|---|---|
| WMBUS_ACCESSIBILITY_NO_ACCESS | No access (unidirectional) | 
| WMBUS_ACCESSIBILITY_TEMPORARY_NO_ACCESS | Bidirectional, temporary no access. | 
| WMBUS_ACCESSIBILITY_LIMITED_ACCESS | Bidirectional, limited access (short time after TX) | 
| WMBUS_ACCESSIBILITY_UNLIMITED_ACCESS | Bidirectional, unlimited access. | 
sl_rail_sdk_wmbus_frame_dib_function_t#
sl_rail_sdk_wmbus_frame_dib_function_t
Values for function field in DIB.
| Enumerator | |
|---|---|
| WMBUS_DIB_FUNCTION_INSTANTANEOUS | Instantaneous value. | 
| WMBUS_DIB_FUNCTION_MINIMUM | Minimum value. | 
| WMBUS_DIB_FUNCTION_MAXIMUM | Maximum value. | 
| WMBUS_DIB_FUNCTION_ERROR | Value during error state. | 
sl_rail_sdk_wmbus_mode_t#
sl_rail_sdk_wmbus_mode_t
MBUS modes.
| Enumerator | |
|---|---|
| WMBUS_MODE_S | S mode. | 
| WMBUS_MODE_T_METER | T mode, Meter to Other. | 
| WMBUS_MODE_T_COLLECTOR | T mode, Other to Meter. | 
| WMBUS_MODE_C | C mode. | 
| WMBUS_MODE_F | F mode. | 
| WMBUS_MODE_R2 | R2 mode. | 
| WMBUS_MODE_N_24 | N mode, 2.4kbps (channel 2a and 2b) | 
| WMBUS_MODE_N_48 | N mode, 4.8kbps (channel 1a, 1b, 3a and 3b) | 
| WMBUS_MODE_N_192 | N mode, 19.2kbps (channel 0) |