Data link layer header (first block)
Public Attributes#
uint8_t
Length field.
uint8_t
Control field raw mode.
Control field function code.
bool
Control field fcv/dcf.
bool
Control field fcb/acd.
bool
Control field, primary station bit.
struct sl_rail_sdk_wmbus_dll_header_t::@0::@2
Control field detailed mode.
union sl_rail_sdk_wmbus_dll_header_t::@0
Control field.
uint16_t
Address, manufacturer ID.
uint32_t
Address, device ID.
uint8_t
Address, version.
uint8_t
Address, device type.
struct sl_rail_sdk_wmbus_dll_header_t::@1::@3
Address field detailed mode.
union sl_rail_sdk_wmbus_dll_header_t::@1
Address field.
Public Attribute Documentation#
function_code#
sl_rail_sdk_wmbus_function_code_t sl_rail_sdk_wmbus_dll_header_t::function_code
Control field function code.
detailed#
struct sl_rail_sdk_wmbus_dll_header_t::@0::@2 sl_rail_sdk_wmbus_dll_header_t::detailed
Control field detailed mode.
c_field#
union sl_rail_sdk_wmbus_dll_header_t::@0 sl_rail_sdk_wmbus_dll_header_t::c_field
Control field.
detailed#
struct sl_rail_sdk_wmbus_dll_header_t::@1::@3 sl_rail_sdk_wmbus_dll_header_t::detailed
Address field detailed mode.
address#
union sl_rail_sdk_wmbus_dll_header_t::@1 sl_rail_sdk_wmbus_dll_header_t::address
Address field.