Information for calculating and representing a packet time stamp.
DeprecatedRAIL 2.x synonym of sl_rail_packet_time_stamp_t.
Public Attributes#
Time stamp of the packet in the RAIL timebase.
A value specifying the total length in bytes of the packet used when calculating the packetTime requested by the timePosition field.
A RAIL_PacketTimePosition_t value specifying the packet position to return in the packetTime field.
In RX for all platforms (except EFR32xG21): A value specifying the on-air duration of the data packet, starting with the first bit of the PHR (i.e., end of sync word); preamble and sync word duration are hence excluded.
Public Attribute Documentation#
packetTime#
RAIL_Time_t RAIL_PacketTimeStamp_t::packetTime
Time stamp of the packet in the RAIL timebase.
DeprecatedRAIL 2.x synonym of sl_rail_packet_time_stamp_t::packet_time.
totalPacketBytes#
uint16_t RAIL_PacketTimeStamp_t::totalPacketBytes
A value specifying the total length in bytes of the packet used when calculating the packetTime requested by the timePosition field.
This should account for all bytes sent over the air after the Preamble and Sync word(s) including CRC bytes.
DeprecatedRAIL 2.x synonym of sl_rail_packet_time_stamp_t::total_packet_bytes.
timePosition#
RAIL_PacketTimePosition_t RAIL_PacketTimeStamp_t::timePosition
A RAIL_PacketTimePosition_t value specifying the packet position to return in the packetTime field.
If this is RAIL_PACKET_TIME_DEFAULT, this field will be updated with the actual position corresponding to the packetTime value filled in by a call using this structure.
DeprecatedRAIL 2.x synonym of sl_rail_packet_time_stamp_t::time_position.
packetDurationUs#
RAIL_Time_t RAIL_PacketTimeStamp_t::packetDurationUs
In RX for all platforms (except EFR32xG21): A value specifying the on-air duration of the data packet, starting with the first bit of the PHR (i.e., end of sync word); preamble and sync word duration are hence excluded.
It is not available with BLE. When not available it will be 0.
In Tx for all platforms: A value specifying the on-air duration of the data packet, starting at the preamble (i.e. includes preamble, sync word, PHR, payload and FCS). This value can be used to compute duty cycles. Note
This field is currently valid only for normal transmits but not Auto-Ack transmits which set the field to zero.
DeprecatedRAIL 2.x synonym of sl_rail_packet_time_stamp_t::packet_duration_us.