Front End Module Voltage Detection (VDET) Utility#
RAIL VDET Utility#
This optional software component can be enabled to include default functionality related to VDET configuration. VDET allows customers to measure a voltage during specific timestamps of a transmit packet. This information is used to tune FEM output power measurements during manufacturing and allows compensation for variability in the output path.
Configuration Options#
VDET mode
VDET resolution
VDET sample delay
The following hardware pin must be enabled to use VDET and is fixed to specific GPIO pins on supported EFR32 devices that cannot be changed.
The RAC.AUXADC_IN8_SHIM_EN GPIO pin.