Power Manager Integration#

The Power Manager Integration component integrates RAIL with the Power Manager to enable efficient power management. This integration ensures that the RAIL and Power Manager work together in a synchronized mode, allowing the application to manage power consumption effectively. The component provides functions to initialize the power management integration, ensuring that the application can enter and exit low-power states as needed.

Key functions include:

Functions#

sl_rail_status_t

Initializes RAIL and Power Manager to work together in SYNC mode.

Function Documentation#

sl_rail_sdk_sleep_init#

sl_rail_status_t sl_rail_sdk_sleep_init (void )

Initializes RAIL and Power Manager to work together in SYNC mode.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function sets up the necessary configurations and prepares the RAIL SDK sleep module for operation. It should be called before using any other functions in the sleep module.

Returns

  • sl_rail_status_t

    • SL_RAIL_STATUS_NO_ERROR if initialization was successful.

    • An appropriate error code otherwise.