BT SPP Slave Tera Term Script#

This example demonstrates how to configure the RS9116W in Bluetooth SPP Slave mode to establish a SPP profile connection with a remote mobile device. Once connected, data can be exchanged between the two BT devices over SPP. This example uses an Android mobile device running a Bluetooth SPP Manager app. An example Bluetooth SPP Manager App is avalable from the Google Play store.

Before continuing, ensure the RS9116W is plugged into your computer and Tera Term is connected as described in Getting Started with PC using AT Commands.

STEP 1. Reset the RS9116W EVK.

STEP 2. In the Tera Term menu, select Control->Macro. Tera Term MacroTera Term Macro

STEP 3. Navigate to the folder <SDK>/examples/at_commands/teraterm/bt_spp_slave and select the file spp_slave.ttl. Tera Term Script to be selectedTera Term Script to be selected

At startup, the RS9116W is configured using the following commands:

  1. Opermode

  2. Set connectable mode

  3. Set discoverable mode

  4. Set profile mode

  5. Set local name

STEP 4. When complete, the RS9116W is discoverable by nearby bluetooth devices. Select OK to continue. RS9116W device in discoverable and connectable modeRS9116W device in discoverable and connectable mode

Connecting RS9116W with an Android mobile via Bluetooth#

There are two steps required to connect the RS9116W to a mobile device via Bluetooth using the SPP profile. Firstly, a Bluetooth connection is established, then a SPP connection over Bluetooth is established. These steps are explained in turn in the following sections.

Establishing a Bluetooth Connection#

STEP 1. On the mobile, find the settings page and enable Bluetooth.

STEP 2. Scan for nearby Bluetooth devices, the RS9116W appears as RS9116W_BT_SLAVE. Select the RS9116W_BT_SLAVE to establish a Bluetooth connection with the RS9116W.

Mobile device bluetooth scan resultsMobile device bluetooth scan results RS9116W device in discoverable and connectable modeRS9116W device in discoverable and connectable mode

STEP 3. When prompted, enter the PIN 1234 as shown in the following example.

Mobile device bluetooth connectionMobile device bluetooth connection

After entering the PIN, the RS9116W receives a AT+RSIBT_USRPINCODEREQ event as shown on the Tera Term console in the following example.

Bluetooth connectionBluetooth connection

STEP 4. When the RS9116W receives the AT+RSIBT_USRPINCODEREQ event, a Tera Term pop-up appears. Choose the 'Send User Pincode' response and select OK to establish a Bluetooth link between the RS9116W and the mobile.

Bluetooth connectionBluetooth connection connection establishment between the mobilephone and the moduleconnection establishment between the mobilephone and the module

Establishing a SPP Connection#

STEP 1. Open the Bluetooth SPP Manager mobile app and scan for nearby devices. Choose the RS9116W_BT_SLAVE and select 'Pair'. Device PairingDevice Pairing

STEP 2. On the pop-up, choose the appropriate response according to the notification received in the Tera Term console as follows.

Tera Term console event received

Pop-up Response

RSIBT_USRLINKKEYREQ

Send User Link Key

RSIBT_USRPINCODEREQ

Send User PIN Code

Device PairingDevice Pairing Device PairingDevice Pairing

After the pairing process completes, the RS9116W receives a link key save event and the SPP connection is automatically initiated from the mobile with the 'Bluetooth SPP Manager' app.

Device PairingDevice Pairing

The RS9116W sends a AT+RSI_SPPCONNECTED event to Tera Term to indicate the connection is established and data can be sent across the link.

SPP ConnectionSPP Connection Send MessageSend Message Receive MessageReceive Message

When the mobile disconnects the Bluetooth link, the RS9116W receives a disconnect event as AT+RSIBT_CLASSIC_DISCONNECTED. DisconnectionDisconnection

Transmit and Receive Event Sequence#

TX Events

RX Events

AT+RSIBT_USRLINKKEYREQ 34-1C-F0-70-D2-F8

at+rsibt_usrlinkkey=34-1C-F0-70-D2-F8,0,1234

AT+RSIBT_USRPINCODEREQ 34-1C-F0-70-D2-F8

at+rsibt_usrpincode=34-1C-F0-70-D2-F8,1,1234

AT+RSIBT_USRLINKKEYSAVE 34-1C-F0-70-D2-F8,52,25,EC,DB,9E,82,8A,89,5F,CA,FB,91,E3,B0,CE,A7

AT+RSIBT_AUTHENTICATION_STATUS 34-1C-F0-70-D2-F8,1

AT+RSIBT_SPPCONNECTED 34-1C-F0-70-D2-F8

at+rsibt_spptx=5,Hello

AT+RSIBT_SPPRX 18,Welcome to silabs