BLE Acceptlist#

1. Purpose / Scope#

This application is used to add a particular BD-Address to the Accept List. The device to connect is saved on the accept list located in the LL block of the controller.

This enumerates the remote devices that are allowed to communicate with the local device. The Accept List can restrict which device are allowed to connect to other device.

If it is not, it wont connect. Once the address was saved, the connection with that device is going to be an auto connection establishment procedure.

This means that the Controller autonomously establishes a connection with the device address that matches the address stored in the While List.

2. Prerequisites / Setup Requirements#

Before running the application, the user will need the following things to setup.

2.1 Hardware Requirements#

Setup Diagram For BLE Acceptlist Example Setup Diagram For BLE Acceptlist Example

2.2 Software Requirements#

  • WiSeConnect SDK

  • Embedded Development Environment

  • Download and install the Silicon Labs EFR Connect App in the android smart phones for testing BLE applications. Users can also use their choice of BLE apps available in Android/iOS smart phones.

3. Application Build Environment#

3.1 Platform#

The Application can be built and executed on below Host platforms

3.2 Host Interface#

  • By default, the application is configured to use the SPI bus for interfacing between Host platforms(STM32F411 Nucleo / EFR32MG21) and the RS9116W EVK.

  • This application is also configured to use the SDIO bus for interfacing between Host platforms(EFM32GG11) and the RS9116W EVK.

3.3 Project Configuration#

The Application is provided with the project folder containing Keil and Simplicity Studio project files.

  • Keil Project

    • The Keil project is used to evaluate the application on STM32.

    • Project path: <SDK>/examples/snippets/ble/ble_accept_list/projects/ble_accept_list-nucleo-f411re.uvprojx

  • Simplicity Studio

    • The Simplicity Studio project is used to evaluate the application on EFR32MG21.

    • Project path:

      • If the Radio Board is BRD4180A or BRD4181A, then access the path <SDK>/examples/snippets/ble/ble_accept_list/projects/ble_accept_list-brd4180a-mg21.slsproj

      • If the Radio Board is BRD4180B or BRD4181B, then access the path <SDK>/examples/snippets/ble/ble_accept_list/projects/ble_accept_list-brd4180b-mg21.slsproj

      • User can find the Radio Board version as given below

EFR Radio BoardsEFR Radio Boards

  • EFM32GG11 platform

    • The Simplicity Studio project is used to evaluate the application on EFM32GG11.

      • Project path:<SDK>/examples/snippets/ble/ble_accept_list/projects/ble_accept_list-brd2204a-gg11.slsproj

3.4 Bare Metal//RTOS Support#

This application supports bare metal and RTOS environment. By default, the application project files (Keil and Simplicity Studio) are provided with bare metal configuration.

4. Application Configuration Parameters#

The application can be configured to suit your requirements and development environment. Read through the following sections and make any changes needed.

4.1 Open rsi_ble_acceptlist.c file and update/modify following macros,

4.1.1 User must update the below parameters

RSI_BLE_DEV_ADDR_TYPE refers address type of the remote device to connect.

#define RSI_BLE_DEV_ADDR_TYPE                          LE_PUBLIC_ADDRESS

Based on address type of remote device, valid configurations are

LE_RANDOM_ADDRESS

LE_PUBLIC_ADDRESS

RSI_BLE_DEV_ADDR refers address of the remote device to connect.

#define RSI_BLE_DEV_ADDR                      "00:1A:7D:DA:71:48"

RSI_BLE_ACCEPTLIST_DEV_ADDR1_TYPE,RSI_BLE_ACCEPTLIST_DEV_ADDR1_TYPE refers address of the remote devices to be acceptlisted

#define RSI_BLE_ACCEPTLIST_DEV_ADDR1_TYPE              LE_PUBLIC_ADDRESS
#define RSI_BLE_ACCEPTLIST_DEV_ADDR2_TYPE              LE_PUBLIC_ADDRESS 

RSI_REMOTE_DEVICE_NAME refers the name of remote device to which Silicon Labs device has to connect

#define RSI_REMOTE_DEVICE_NAME                    "SILABS_DEV"

Note: user can configure either RSI_BLE_DEV_ADDR or RSI_REMOTE_DEVICE_NAME of the remote device.

Power save configuration

By default, the Application is configured without power save.

#define ENABLE_POWER_SAVE 0

If user wants to run the application in power save, modify the below configuration.

#define ENABLE_POWER_SAVE 1 

4.1.2 The desired parameters are provided below. User can also modify the parameters as per their needs and requirements.

Following are the event numbers for advertising, connection and Disconnection events,

#define RSI_APP_EVENT_ADV_REPORT                       0
#define RSI_APP_EVENT_CONNECTED                        1
#define RSI_APP_EVENT_DISCONNECTED                     2 

Following are the non-configurable macros in the application.

GLOBAL_BUFF_LEN refers Number of bytes required by the application and the driver

#define GLOBAL_BUFF_LEN                             15000

4.2 Open rsi_ble_config.h file and update/modify following macros,

#define RSI_BLE_PWR_INX                                30
#define RSI_BLE_PWR_SAVE_OPTIONS                       0
#define RSI_BLE_SCAN_FILTER_TYPE                       SCAN_FILTER_TYPE_ONLY_ACCEPT_LIST

Opermode command parameters

#define RSI_FEATURE_BIT_MAP                            FEAT_SECURITY_OPEN
#define RSI_TCP_IP_BYPASS                              RSI_DISABLE
#define RSI_TCP_IP_FEATURE_BIT_MAP                     TCP_IP_FEAT_DHCPV4_CLIENT
#define RSI_CUSTOM_FEATURE_BIT_MAP                     FEAT_CUSTOM_FEAT_EXTENTION_VALID
#define RSI_EXT_CUSTOM_FEATURE_BIT_MAP                 RAM_LEVEL_NWP_ALL_MCU_ZERO

Note! rsi_ble_config.h files are already set with desired configuration in respective example folders user need not change for each example. |


5. Testing the Application#

User has to follow the below steps for the successful execution of the application.

5.1 Loading the RS9116W Firmware#

Refer Getting started with PC to load the firmware into RS9116W EVK. The firmware binary is located in <SDK>/firmware/

5.2 Building the Application on the Host Platform#

5.2.1 Using STM32#

Refer EFx32 Getting Started

  • Open the project <SDK>/examples/snippets/ble/ble_accept_list/projects/ble_accept_list-nucleo-f411re.uvprojx in Keil IDE.

  • Build and Debug the project

  • Check for the RESET pin:

    • If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run.

    • If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run.

  • Free run the project

  • Then continue the common steps from Section 5.3

5.2.2 Using EFX32#

Refer EFx32 Getting Started, for settin-up EFR & EFM host platforms

  • Import the EFR32/EFM32 project from <SDK>/examples/snippets/ble/ble_accept_list/projects

    • Select the appropriate .slsproj as per Radio Board type mentioned in Section 3.3 for EFR32 board. (or)

    • Select the *.brd2204a-gg11.slsproj for EFM32GG11 board.

  • Compile and flash the project in to Host MCU

  • Debug the project

  • Check for the RESET pin:

    • If RESET pin is connected from EFX32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run

    • If RESET pin is not connected from EFX32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run

  • Free run the project

  • Then continue the common steps from Section 5.3

5.3 Common Steps#

  1. Configure the remote ble device in peripheral mode and put it in advertising mode.

  2. After the program gets executed, it adds the configured remote device addresses to the acceptlist, and Silicon Labs device tries to connect only with the acceptlisted remote device specified in RSI_BLE_DEV_ADDR or RSI_REMOTE_DEVICE_NAME macro and ble_acceptlist_addr1 array

  3. Observe that the connection is established between the desired device and Silicon Labs device.

  4. After successful program execution the print in teraterm looks as shown below.

Prints in TeratermPrints in Teraterm

 **Note:** Examples for ble peripherals: Blue tooth Dongle, mobile application, TA sensor tag

Compressed Debug Logging#

To enable the compressed debug logging feature please refer to Logging User Guide