SAPI Changelog#
This section describes details of changes and enhancements in the RS9116W SAPI library that are likely to impact backward compatibility. A novel compressed logging framework is added to provide debug information to developers. This framework is developed in June 2022 included in WiSeConnect 2.6 SDK release. A list of additional changes for previous releases is also provided.
SAPI Changelog#
Folder/Filename Changes for Release: 2.4#
The SAPI directory in the root folder of the SDK has been changed from sapis to sapi. The changes listed in the following table were made to files and sub-folders inside the sapi directory.
| Previous Name | New Name | Notes | 
|---|---|---|
| 
 | 
 | Renamed | 
| Moved  | ||
| Moved  | ||
| Removed various unsupported source files for profiles including hfp, hid, iap, sdp and l2cap | ||
| 
 | - | Removed | 
| 
 | 
 | No change | 
| Renamed  | ||
| Removed various unsupported source files from the package including  | ||
| 
 | - | Moved to the root directory of the SDK | 
| 
 | - | Moved into root level  | 
| 
 | 
 | Renamed | 
| Renamed  | ||
| Moved  | ||
| Moved  | ||
| 
 | 
 | Renamed | 
| Renamed  | ||
| Moved  | ||
| 
 | - | No longer included in the SDK | 
| 
 | - | No longer included in the SDK | 
Modifications for Release: 2.6#
| Wi-Fi APIs | Notes | Resolution for Backward Compatibility | 
|---|---|---|
| Added DFS channels and 4.9GHz channels | NA | |
| sl_fw_log_configure() | Sends the configurable parameters for firmware logging framework | NA | 
| sl_set_fw_component_log_levels() | Sets debug log levels for firmware components | NA | 
| sl_fw_log_init() | Initializes the firmware logging feature | NA | 
| sl_fw_queue_init() | Creates a queue for firmware log messages | NA | 
| sl_fw_log_enqueue() | Enqueues a log message node to the firmware log message queue | NA | 
| sl_fw_log_dequeue() | Dequeues a log message node from the firmware log message queue | NA | 
| sl_fw_log_pool_init() | Creates log pool from the provided buffer | NA | 
| sl_fw_log_node_alloc() | Allocates a log node from given log pool | NA | 
| sl_fw_log_node_free() | Frees the given log node | NA | 
| sl_fw_log_print() | Prints the log message from firmware | NA | 
Modifications for Release: 2.5#
| Wi-Fi APIs | Notes | Resolution for Backward Compatibility | 
|---|---|---|
| Need to call after the driver initialization | NA | |
| Configure XO Ctune value from host | NA | |
| Configure TA GPIOs using Command from host.This is a non-blocking API. | Added new parameter "gpio_type" | |
| Drive the Module GPIOs high or low using command from host. This is a non-blocking API. | Added new parameter "gpio_type" | |
| Read status of TA GPIOs using Command from host. This is a non-blocking API. | Added new parameter "gpio_type" | |
| Read status of TA GPIOs using Command from host. This is a non-blocking API. | NA | |
| Drive the TA GPIOs high or low using command from host. This is a non-blocking API. | NA | |
| is_power_of_two() | Checking input parameter is power of two or not. This is a non-blocking API. | NA | 
| Take the mutex from ISR context | NA | |
| Give the mutex from ISR context | NA | 
| Bluetooth APIs | Notes | Resolution for Backward Compatibility | 
|---|---|---|
| Indicate the local value to the remote device | NA | |
| Sent in reply to a received Exchange MTU Request | NA | |
| Update gain table offset/max power | NA | |
| rsi_ble_on_mtu_exchange_info_t | Callback function to indicate MTU size and who initated MTU Exchange Request | NA | 
Modifications for Release: 2.4#
Timeout Error Indication and Recovery Mechanism#
All SAPI command response-timeout errors return 0xFFFFFFE2 if the firmware takes more time than the configured timeout. If a timeout error occurs, the application must reset the device and driver state to recover from the error.
| Wi-Fi APIs | Notes | 
|---|---|
| Sort the Scan results in the order of RSSI. The application should call this API to get the scan result in sorted order. | 
| Bluetooth APIs | Notes | 
|---|---|
| Initialize A2DP profile with either user defined audio codec parameters or default stack audio codec params. This is a blocking API. | |
| Set the AVRCP profile mode and also enable the media player selection feature, if required. This is a blocking API | |
| Send Addressed player response from the Target to Controller. This is a blocking API | |
| Send Folder items response from Target to Controller. This is a Blocking API | |
| Send the response for the total number of items from the Target to Controller. This is a blocking API. | |
| The Authentication procedure usually starts from the stack itself after the PHY Level Connection completes, however if authentication is disabled after PHY Level Connection, and Authentication is needed, then firstly enable Authentication then call this API. This is a blocking API. | |
| Usually Encryption procedure will start from stack itself once PHY Level Connection and authentication is completed, however the user can decide whether to enable/disable encryption from the host. This is a blocking API. | |
| Keep the device in continuous wave mode. It is not necessary to call this API if  | |
| Issue vendor specific command for setting AutoRate in controller on given inputs. This is a blocking API. A received event  | |
| Issue vendor specific command for setting  | |
| rsi_bt_vendor_avdtp_stats_enabled() | Issue vendor specific command for setting avdtp stats enable in controller, to receive the stats. This is a blocking API. A received event  | 
| System APIs | Notes | 
|---|---|
| Application to provide feedback of frequency error in KHz. This is a blocking API. | |
| RF Calibration Process. This API commands the firmware to update the existing FLASH/EFuse calibration data. This is a blocking API. | |
| Select internal or external RF type and clock frequency to pass Feature enables dynamically. This is a blocking API. | |
| Register SAPI wait timeout handler. This is non-blocking API. | 
Modifications for Release: 2.3#
| Wi-Fi/Network APIs | Notes | Resolution for Backward Compatibility | 
|---|---|---|
| Description: Added support for Socket ID based return status for Socket APIs. | No changes required. By default, both rsi_wlan_get_status() and rsi_wlan_socket_get_status() return the actual status of Socket APIs. | |
| Purpose: To get socket ID based return status for socket APIs. This change is an enhancement. | ||
| 1.x.x: rsi_wlan_get_status() is used to get the return status of any SAPI command in case of a failure. The same API was used to get socket API status as well. | ||
| 2.x.x: rsi_wlan_socket_get_status() added to get return status for socket APIs based on socket ID input. Latest SAPI driver stores response for each socket id | ||
| Impact: In multi-threaded applications using rsi_wlan_get_status(), may not return exact Socket ID based status, as it may get over-written. Applications should use rsi_wlan_socket_get_status() instead of rsi_wlan_get_status() for getting actual return status for Socket APIs, especially in muti-threaded applications. | ||
| Enable 'socket wait close' configuration if using TCP Sockets in Application. | If TCP sockets is used in an application, enable  | See rsi_shutdown() for details. | 
| Bluetooth APIs | Notes | Resolution for Backward Compatibility | 
|---|---|---|
| 384kB memory requirement | It is mandatory to configure 384kB memory when using BT Classic, BLE and COEX. RS9116W firmware, from 2.X.X release supports only this mode. | In  | 
| - | - | - | 
| Support for HEX based input BD address in SAPI applications | Purpose: To avoid input BD address conversion from ASCII to HEX as RS9116W expect BD address in HEX format. This change is an enhancement. | Backward compatibility is achieved by  | 
| 1.1.x: RS9116W expects BD address in 6 bytes of HEX as input. But existing SAPI applications expect BD address input in ASCII and coverts it into HEX (internally in SAPI core) and then passes it to RS9116W | ||
| 2.x: Added support to take the input as a 6 bytes of HEX value which avoids ASCII to HEX conversion. | ||
| Impact: Existing designs which are developed with ASCII based BD address input will not work. | ||
| - | - | - | 
| BLE data flow mechanism to support flow control and multiple connections | Purpose: To maintain multiple BLE connections and serve them independently, RS9116W firmware and SAPI are enhanced with support for connection based buffer management and flow control between host (application) and RS9116W (firmware). This is an enhancement. | The app needs to use the APIs as described to check for buffer full response from RS9116W device. Device returns  | 
| 1.1.x: In earlier design, connection based buffer management was not supported. This effects data throughput, connectivity and simultaneous connections in different ways. In this design, when there is a data write request to remote BLE device from application, RS9116W provides response only after receiving the response from the remote device. There was no flow control mechanism in this case and one connection can consume all the buffers in RS9116W impacting other connection's control and data flows. | ||
| 2.x: In the new design, connection based buffer management is implemented (using dedicated buffers for each connected device ). If there are no buffers available in the RS9116W device, it returns an error to the host with that particular device address, stating that buffers are not available for that connection. Once the buffer are freed (device serves pending events), then the device will send an event (more data request) to the host requesting to send the data | ||
| New API/Event:  | ||
| Impact: All existing applications which use attribute write, long write or prepare write should be changed as per the new design, otherwise will not work. This impacts only BLE data flows. Not applicable for BT-Classic. |