Public Attributes#

uint32_t
uint16_t
uint8_t

Public Attribute Documentation#

id#

uint32_t id

Specifies the attribute/Value ID to be written


Definition at line 3226 of file include/rsi_bt_apis.h

char_set_id#

uint16_t char_set_id

Specifies the character set ID to be displayed on CT


Definition at line 3229 of file include/rsi_bt_apis.h

attr_text_len#

uint16_t attr_text_len

Length of the player application setting attribute/Value string


Definition at line 3232 of file include/rsi_bt_apis.h

att_text#

uint8_t att_text[31]

Specifies the player application setting attribute/Value string in specified character set.


Definition at line 3235 of file include/rsi_bt_apis.h