Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

att_id#

uint8_t att_id

Player application setting attribute ID for which the value is returned


Definition at line 1938 of file include/rsi_bt_apis.h

att_val#

uint8_t att_val

Currently set Player Application Setting value on the TG for the above PlayerApplicationSettingA ttributeID.


Definition at line 1942 of file include/rsi_bt_apis.h

reserved#

uint8_t reserved[2]

Reserved for Future Purpose


Definition at line 1945 of file include/rsi_bt_apis.h