Crypto APIs#
This section describes the Crypto APIs
Functions#
Compute the SHA digest. This is a blocking API.
Decide whether the SHA message can be sent once or requires multiple calls to send. This is a blocking API.
Hold computed digest from HMAC-SHA. This is a blocking API.
Decide whether the HMAC-SHA message can be sent once or requires multiple calls to send the message. This is a blocking API.
Decide whether the AES message can be sent once or requires multiple calls to send the message. This is a blocking API.
Calculate the DH key. This is a blocking API.
Compute the ECDH point multiplication vector. This is a blocking API.
Compute the ECDH point addition vector. This is a blocking API.
Compute the ECDH point subtraction vector. This is a blocking API.
Compute the ECDH point double vector. This is a blocking API.
Compute the ECDH point affinity vector. This is a blocking API.
Function Documentation#
rsi_sha_pen#
int32_t rsi_sha_pen (uint8_t sha_mode, uint8_t * msg, uint16_t msg_length, uint16_t chunk_len, uint8_t pending_flag, uint8_t * digest)
Compute the SHA digest. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | sha_mode | 1 – For SHA1 2 – For SHA256 3 – For SHA384 4 – For SHA512 |
| uint8_t * | [in] | msg | - Pointer to message |
| uint16_t | [in] | msg_length | - Total message length |
| uint16_t | [in] | chunk_len | - Current chunk length |
| uint8_t | [in] | pending_flag | - BIT(0) - 1st chunk BIT(1) - Middle chunk BIT(2) - Last chunk |
| uint8_t * | [out] | digest | - Output parameter to hold computed digest from SHA |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes.
rsi_sha#
int32_t rsi_sha (uint8_t sha_mode, uint8_t * msg, uint16_t msg_length, uint8_t * digest)
Decide whether the SHA message can be sent once or requires multiple calls to send. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | sha_mode | 1 – For SHA1 2 – For SHA256 3 – For SHA384 4 – For SHA512 |
| uint8_t * | [in] | msg | - Pointer to message |
| uint16_t | [in] | msg_length | - Total message length |
| uint8_t * | [out] | digest | - Output parameter to hold computed digest from SHA |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes.
rsi_hmac_sha_pen#
int32_t rsi_hmac_sha_pen (uint8_t hmac_sha_mode, uint8_t * data, uint16_t total_length, uint16_t chunk_length, uint32_t key_length, uint8_t pending_flag, uint8_t * digest)
Hold computed digest from HMAC-SHA. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | hmac_sha_mode | - 1 – For HMAC-SHA1 2 – For HMAC-SHA256 3 – For HMAC-SHA384 4 – For HMAC-SHA512 |
| uint8_t * | [in] | data | - Pointer to key along with message |
| uint16_t | [in] | total_length | - Total message length |
| uint16_t | [in] | chunk_length | - Current chunk length |
| uint32_t | [in] | key_length | - BIT(0) - 1st chunk BIT(1) - Middle chunk BIT(2) - Last chunk |
| uint8_t | [out] | pending_flag | - Output parameter to hold computed digest from HMAC-SHA |
| uint8_t * | N/A | digest |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes.
rsi_hmac_sha#
int32_t rsi_hmac_sha (uint8_t hmac_sha_mode, uint8_t * msg, uint32_t msg_length, uint8_t * key, uint32_t key_length, uint8_t * digest, uint8_t * hmac_buffer)
Decide whether the HMAC-SHA message can be sent once or requires multiple calls to send the message. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | hmac_sha_mode | - 1 – For HMAC-SHA1 2 – For HMAC-SHA256 3 – For HMAC-SHA384 4 – For HMAC-SHA512 |
| uint8_t * | [in] | msg | - Pointer to message |
| uint32_t | [in] | msg_length | - Total message length |
| uint8_t * | [in] | key | - Pointer to HMAC key |
| uint32_t | [in] | key_length | - HMAC key length in bytes |
| uint8_t * | [out] | digest | - Output parameter to hold computed digest from HMAC-SHA |
| uint8_t * | N/A | hmac_buffer |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_aes#
int32_t rsi_aes (uint16_t aes_mode, uint16_t enc_dec, uint8_t * msg, uint16_t msg_length, uint8_t * key, uint16_t key_length, uint8_t * iv, uint8_t * output)
Decide whether the AES message can be sent once or requires multiple calls to send the message. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | aes_mode | - 1 – For AES CBC mode 2 – For AES ECB mode 3 – For AES CTR mode |
| uint16_t | [in] | enc_dec | - 1 – For AES Encryption 2 – For AES Decryption |
| uint8_t * | [in] | msg | - Pointer to message |
| uint16_t | [in] | msg_length | - Total message length |
| uint8_t * | [in] | key | - Pointer to AES key |
| uint16_t | [in] | key_length | - AES key length in bytes |
| uint8_t * | [in] | iv | - Pointer to AES iv |
| uint8_t * | [out] | output | - Output parameter to hold encrypted/decrypted from AES |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_exponentiation#
int32_t rsi_exponentiation (uint8_t * prime, uint32_t prime_length, uint8_t * base, uint32_t base_length, uint8_t * exponent, uint32_t exponent_length, uint8_t * exp_result)
Calculate the DH key. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | prime | - Pointer to the prime |
| uint32_t | [in] | prime_length | - Length of the prime |
| uint8_t * | [in] | base | - Pointer to base |
| uint32_t | [in] | base_length | - Length of the base |
| uint8_t * | [in] | exponent | - Pointer to exponent |
| uint32_t | [in] | exponent_length | - Length of the exponent |
| uint8_t * | [out] | exp_result | - Output exponentiation result |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_ecdh_point_multiplication#
int32_t rsi_ecdh_point_multiplication (uint8_t ecdh_mode, uint8_t * d, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point multiplication vector. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | ecdh_mode | - 1 – For ECDH 192 2 – For ECDH 224 3 – For ECDH 256 |
| uint8_t * | [in] | d | - Pointer to scalar value that needs to be multiplied |
| uint8_t * | [in] | sx | - Pointers to x, y, z coordinates of the point to be multiplied with scalar ‘d’ |
| uint8_t * | [out] | sy | - Pointers to x, y, z coordinates of the result point |
| uint8_t * | N/A | sz | |
| uint8_t * | N/A | rx | |
| uint8_t * | N/A | ry | |
| uint8_t * | N/A | rz |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_ecdh_point_addition#
int32_t rsi_ecdh_point_addition (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * tx, uint8_t * ty, uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point addition vector. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | ecdh_mode | - 1 – For ECDH 192 2 – For ECDH 224 3 – For ECDH 256 |
| uint8_t * | [in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be added |
| uint8_t * | [in] | sy | - Pointers to x, y, z coordinates of the point2 that needs to be added |
| uint8_t * | [out] | sz | - Pointers to x, y, z coordinates of the result point |
| uint8_t * | N/A | tx | |
| uint8_t * | N/A | ty | |
| uint8_t * | N/A | tz | |
| uint8_t * | N/A | rx | |
| uint8_t * | N/A | ry | |
| uint8_t * | N/A | rz |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_ecdh_point_subtraction#
int32_t rsi_ecdh_point_subtraction (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * tx, uint8_t * ty, uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point subtraction vector. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | ecdh_mode | - 1 – For ECDH 192 2 – For ECDH 224 3 – For ECDH 256 |
| uint8_t * | [in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be subtracted |
| uint8_t * | [in] | sy | - Pointers to x, y, z coordinates of the point2 that needs to be subtracted |
| uint8_t * | [out] | sz | - Pointers to x, y, z coordinates of the result point |
| uint8_t * | N/A | tx | |
| uint8_t * | N/A | ty | |
| uint8_t * | N/A | tz | |
| uint8_t * | N/A | rx | |
| uint8_t * | N/A | ry | |
| uint8_t * | N/A | rz |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
rsi_ecdh_point_double#
int32_t rsi_ecdh_point_double (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point double vector. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | ecdh_mode | - 1 – For ECDH 192 2 – For ECDH 224 3 – For ECDH 256 |
| uint8_t * | [in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be doubled |
| uint8_t * | [out] | sy | - Pointers to x, y, z coordinates of the result point |
| uint8_t * | N/A | sz | |
| uint8_t * | N/A | rx | |
| uint8_t * | N/A | ry | |
| uint8_t * | N/A | rz |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.
rsi_ecdh_point_affine#
int32_t rsi_ecdh_point_affine (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point affinity vector. This is a blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | ecdh_mode | - 1 – For ECDH 192 2 – For ECDH 224 3 – For ECDH 256 |
| uint8_t * | [in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be affinified |
| uint8_t * | [out] | sy | - Pointers to x, y, z coordinates of the result point |
| uint8_t * | N/A | sz | |
| uint8_t * | N/A | rx | |
| uint8_t * | N/A | ry | |
| uint8_t * | N/A | rz |
Note
This API is not supported in current release.
Returns
0 - Success Non-Zero Value - If return value is lesser than 0 -2: Invalid parameters -3: Command given in wrong state -4: Buffer not available to serve the command If return value is greater than 0 0xFF15, 0xCC9C, 0xCC9B
Note
Refer Error Codes section for above error codes Error Codes.