Public Attributes#

uint8_t
uint8_t
int8_t

Public Attribute Documentation#

dev_addr_type#

uint8_t dev_addr_type

Address type of the advertising device


dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

Address of the advertising device


adv_data_len#

uint8_t adv_data_len

Raw advertisement data length


adv_data#

uint8_t adv_data[RSI_MAX_ADV_REPORT_SIZE]

advertisement data


rssi#

int8_t rssi

Signal strength


report_type#

uint8_t report_type

Report type 0x00 Connectable and scannable undirected advertising (ADV_IND) 0x01 Connectable directed advertising (ADV_DIRECT_IND) 0x02 Scannable undirected advertising (ADV_SCAN_IND) 0x03 Non connectable undirected advertising (ADV_NONCONN_IND) 0x04 Scan Response (SCAN_RSP) All other values Reserved for future use