Public Attribute Documentation#
TxPhy#
uint8_t TxPhy
Transmitission phy rate(1 byte) BIT(0) - The Host prefers to use the LE 1M transmitter PHY (possibly among others) BIT(1) - The Host prefers to use the LE 2M transmitter PHY (possibly among others) BIT(2) - The Host prefers to use the LE Coded transmitter PHY (possibly among others) BIT(3) - BIT(7) Reserved for future use
RxPhy#
uint8_t RxPhy
Reception phy rate(1 byte) BIT(0) - The Host prefers to use the LE 1M transmitter PHY (possibly among others) BIT(1) - The Host prefers to use the LE 2M transmitter PHY (possibly among others) BIT(2) - The Host prefers to use the LE Coded transmitter PHY (possibly among others) BIT(3) - BIT(7) Reserved for future use