AT Command Examples#
The AT-Command examples provided in the WiSeConnectâ„¢ SDK are Tera Term scripts that demonstrate basic RS9116W functionality using only a RS9116 Evaluation Kit and a PC. More details can be found in Getting Started with PC using AT Commands
The scripts are found in the WiSeConnectâ„¢ SDK at the path <SDK>/examples/at_commands
Details on the configuration and operation of each example are available in the readme.md file that is found with the example source code and at the following links:
BLE Central
Demonstrates setting up the device as a BLE Central device.
BT SPP Slave
Demonstrates setting up the device as a Bluetooth Serial Port Profile (SPP) Slave.
BT PER
Demonstrates setting up the device as a BT PER Transmit/Receive functionality.
BLE Proximity Profile
Demonstrates setting up the device as a BLE Proximity Profile Device.
Wi-Fi Low Power + BLE
Demonstrates Wi-Fi Station standby associated power save functionality along with BLE advertising.
BLE Peripheral
Demonstrates setting up the device as a BLE Peripheral device.
Wi-Fi Soft AP
Demonstrates setting up the device as a Wi-Fi Access Point and connecting to it from a mobile phone or PC
Wi-Fi Station
Demonstrates connecting to a Wi-Fi access point in station mode.
BLE PER
Demonstrates setting up the device as a BLE Per device.
Wi-Fi Enterprise Authentication
Demonstrates connecting to a Wi-Fi access point in station mode using enterprise authenticarion.
BT SPP Master
Demonstrates setting up the device as a Bluetooth Serial Port Profile (SPP) master.
Wi-Fi Low Power
Demonstrates Wi-Fi Station standby associated power save functionality allowing the user to measure and evaluate the low-power consumption of the device.
BLE Heart Rate Profile
Demonstrates setting up the device as a Bluetooth Low Energy Heart Rate Profile.