Featured Examples#

Featured examples are complete projects that demonstrate a common RS9116 use-case or enable you to perform a key aspect of RS9116 evaluation. The featured examples are found in the WiSeConnectâ„¢ SDK at the path: <SDK>/examples/featured.

Details on the configuration and operation of each featured example are available in the readme.md file that is found with the example source code and at the following links:

BT PER - Transmit and Receive Performance and Regulatory Testing
configure the device with necessary parameters to start transmitting or receiving BT PER packets.

AWS IoT Device Shadow
Creates an AWS IoT 'thing' that connects to the AWS IoT device shadow service using the MQTT protocol

Throughput Test
Measures Wi-Fi transmit/receive throughput performance using a remote iPerf client/server

BLE PER - Transmit and Receive Performance and Regulatory Testing
configure the device with necessary parameters to start transmitting or receiving BLE PER packets.

Firmware Update via TCP Server
Wirelessly updates the RS911x firmware from a remote TCP server

Transmit Performance and Regulatory Testing
Configures the device in a transmit mode that is used for transmit performance and regulatory certification testing (FCC, ETSI, CE, etc.)

Powersave Standby Associated
Connects to a Wi-Fi Access Point in deep-sleep mode and intermittently wakes to send UDP packets