Channel Sounding (CS)#

Channel Sounding.

Distances are calculated by following the steps below:

  1. Initialize a sl_rtl_cs_libitem instance.

  2. Set up the algorithm mode and CS parameters.

  3. Create the estimator.

  4. Process the CS procedure data into distance.

  5. Get distance and/or likeliness estimates.

Supported Combinations

Main Mode: Phase-Based Ranging (PBR), Sub Mode: None

CS Algorithm Mode

Channel Map Preset
HIGH

Channel Map Preset
MEDIUM

Channel Map Preset
LOW

REAL TIME BASIC

yes

yes

yes

STATIC HIGH ACCURACY

yes

no

no

REAL TIME FAST

yes + vel

yes + vel

yes

Main Mode: Round-Trip Time (RTT), Sub Mode: None

CS Algorithm Mode

Channel Map Preset
HIGH

Channel Map Preset
MEDIUM

Channel Map Preset
LOW

REAL TIME BASIC

yes

no

no

STATIC HIGH ACCURACY

(yes)*

no

no

REAL TIME FAST

no

no

no

Main Mode: Phase-Based Ranging (PBR), Sub Mode: Round-Trip Time (RTT)

CS Algorithm Mode

Channel Map Preset
HIGH

Channel Map Preset
MEDIUM

Channel Map Preset
LOW

REAL TIME BASIC

yes

no

no

STATIC HIGH ACCURACY

yes

no

no

REAL TIME FAST

yes + vel

no

no

Refer to Developer's Guide > Channel Sounding Performance Metrics for the channel map preset definitions. Note

  • vel = Velocity is reported.

  • * This mode uses the same implementation as REAL TIME BASIC.

Modules#

sl_rtl_cs_params

sl_rtl_cs_procedure_config

sl_rtl_cs_estimator_param_value

sl_rtl_cs_estimator_param

sl_rtl_cs_mode_calib_data

sl_rtl_cs_mode_rtt_data

sl_rtl_cs_pbr_tone

sl_rtl_cs_mode_pbr_data

sl_rtl_cs_step_data

sl_rtl_cs_subevent_data

sl_rtl_cs_procedure

sl_rtl_cs_log_params

sl_rtl_cs_step_data.__unnamed1__

Enumerations#

enum
SL_RTL_CS_ROLE_INITIATOR = 0
SL_RTL_CS_ROLE_REFLECTOR
}
enum
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC = 0
SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY
SL_RTL_CS_ALGO_MODE_REAL_TIME_FAST
}
enum
SL_RTL_CS_MODE_CALIBRATION = 0
SL_RTL_CS_MODE_RTT = 1
SL_RTL_CS_MODE_PBR = 2
SL_RTL_CS_MODE_NONE = 3
}
enum
SL_RTL_CS_RTT_TYPE_AAONLY = 0
SL_RTL_CS_RTT_TYPE_SS_32BIT = 1
SL_RTL_CS_RTT_TYPE_SS_96BIT = 2
SL_RTL_CS_RTT_TYPE_RS_32BIT = 3
SL_RTL_CS_RTT_TYPE_RS_64BIT = 4
SL_RTL_CS_RTT_TYPE_RS_96BIT = 5
SL_RTL_CS_RTT_TYPE_RS_128BIT = 6
}
enum
SL_RTL_LAST_KNOWN_DISTANCE = 0
SL_RTL_RANGE_MIN = 1
SL_RTL_RANGE_MAX = 2
SL_RTL_REF_TX_POWER = 3
}
enum
SL_RTL_CS_BEST_ESTIMATE = 0
SL_RTL_CS_MAIN_MODE_ESTIMATE
SL_RTL_CS_SUB_MODE_ESTIMATE
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED = 0
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RAW
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_VELOCITY
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS = 0
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE = 0
}

Functions#

sl_rtl_cs_init(sl_rtl_cs_libitem *item)
sl_rtl_cs_deinit(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_algo_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_algo_mode mode)
sl_rtl_cs_set_cs_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_mode main_mode, const sl_rtl_cs_mode sub_mode)
sl_rtl_cs_set_cs_params(sl_rtl_cs_libitem *item, const sl_rtl_cs_params *parameters)
sl_rtl_cs_create_estimator(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_estimator_param(sl_rtl_cs_libitem *item, const sl_rtl_cs_estimator_param *param)
sl_rtl_cs_process(sl_rtl_cs_libitem *item, const uint8_t num_procedures, const sl_rtl_cs_procedure *procedure_data)
sl_rtl_cs_get_distance_estimate(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_type estimate_type, const sl_rtl_cs_distance_estimate_mode estimate_mode, float *distance)
sl_rtl_cs_get_distance_estimate_confidence(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, const sl_rtl_cs_distance_estimate_confidence_mode confidence_mode, float *confidence)
sl_rtl_cs_get_distance_estimate_extended_info(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float *extended_info)
sl_rtl_cs_log_enable(sl_rtl_cs_libitem *item)
sl_rtl_cs_log_disable(sl_rtl_cs_libitem *item)
sl_rtl_cs_log_add_timestamp(sl_rtl_cs_libitem *item, const struct timespec timestamp)
sl_rtl_cs_log_get_instance_id(sl_rtl_cs_libitem *item, uint8_t *instance_id)

Macros#

#define

Number of bits used for indicating I or Q sample in the phase correction term (PCT) in CS step data.

#define

Number of bits used for indicating step mode in CS step data.

#define

Size of the channel map in bytes.

Enumeration Documentation#

sl_rtl_cs_role#

sl_rtl_cs_role
Enumerator
SL_RTL_CS_ROLE_INITIATOR

Initiator role.

SL_RTL_CS_ROLE_REFLECTOR

Reflector role.


sl_rtl_cs_algo_mode#

sl_rtl_cs_algo_mode

Refer to section Supported Combinations for valid parameter combinations with each algorithm mode.

Enumerator
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC

Medium filtering, medium response, medium CPU cost. Suitable for real-time tracking.

SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY

High filtering, high CPU cost, high accuracy. Suitable for static high-accuracy use cases.

SL_RTL_CS_ALGO_MODE_REAL_TIME_FAST

Low filtering, low CPU and RAM cost, basic accuracy. Suitable for real-time tracking with constrained computational resources. This mode is only available for free-running procedures (procedure_count = 0).


sl_rtl_cs_mode#

sl_rtl_cs_mode
Enumerator
SL_RTL_CS_MODE_CALIBRATION

Calibration mode with no distance estimation enabled

SL_RTL_CS_MODE_RTT

Round-trip time based estimation (RTT)

SL_RTL_CS_MODE_PBR

Round-trip phase based estimation (PBR)

SL_RTL_CS_MODE_NONE

No mode is set. This option is used solely to indicate the absence of a sub mode.


sl_rtl_cs_rtt_type#

sl_rtl_cs_rtt_type
Enumerator
SL_RTL_CS_RTT_TYPE_AAONLY

RTT AA Only. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_SS_32BIT

RTT with 32-bit sounding sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_SS_96BIT

RTT with 96-bit sounding sequence.

SL_RTL_CS_RTT_TYPE_RS_32BIT

RTT with 32-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_64BIT

RTT with 64-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_96BIT

RTT with 96-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_128BIT

RTT with 128-bit random sequence. Currently unsupported type.


sl_rtl_cs_estimator_param_type#

sl_rtl_cs_estimator_param_type
Enumerator
SL_RTL_LAST_KNOWN_DISTANCE

Last known distance from the user, if more recent than the last CS measurement.

SL_RTL_RANGE_MIN

Minimum limit for the distance estimation range. This parameter is currently not applied.

SL_RTL_RANGE_MAX

Maximum limit for the distance estimation range. This parameter is currently not applied.

SL_RTL_REF_TX_POWER

Reference RSSI value of the TX-device at 1.0 m distance in dBm. Default value is -45.0 dBm.


sl_rtl_cs_distance_estimate_mode#

sl_rtl_cs_distance_estimate_mode
Enumerator
SL_RTL_CS_BEST_ESTIMATE

The best estimate

SL_RTL_CS_MAIN_MODE_ESTIMATE

Estimate based only on the main mode

SL_RTL_CS_SUB_MODE_ESTIMATE

Estimate based only on the sub mode This option is available only if a valid sub mode is set.


sl_rtl_cs_distance_estimate_type#

sl_rtl_cs_distance_estimate_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED

Distance estimate with built-in post-filtering. Note: The post-filtering would remove any large undesired jumps in the distance reported. However, post-filtering introduces latency in distance reported.

SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI

Distance estimate based on the Packet_RSSI in the calibration (Mode 0) steps

SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RAW

Distance estimate based solely on the most recent procedure input.

SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_VELOCITY

Provides a velocity estimate derived from PCT data. Negative velocity denotes approaching target. This feature is experimental and has limited support. Refer to section Supported Combinations for details.


sl_rtl_cs_distance_estimate_confidence_type#

sl_rtl_cs_distance_estimate_confidence_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS

Likeliness of the distance estimate accuracy, ranging from 0 to 1

SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE

Bit error rate in the RTT random or sounding sequence, ranging from 0 to 1. Only supported for RTT types (see sl_rtl_cs_rtt_type) with random sequence (RS) or sounding sequence (SS).


sl_rtl_cs_distance_estimate_extended_info_type#

sl_rtl_cs_distance_estimate_extended_info_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE

Estimation progress in percentage.

  • Range: 0 to 100.


Typedef Documentation#

sl_rtl_cs_distance_estimate_confidence_mode#

typedef sl_rtl_cs_distance_estimate_mode sl_rtl_cs_distance_estimate_confidence_mode

sl_rtl_cs_libitem#

typedef void* sl_rtl_cs_libitem

CS library item.


Function Documentation#

sl_rtl_cs_init#

enum sl_rtl_error_code sl_rtl_cs_init (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the libitem to be initialized

Initialize the CS libitem instance.

Returns


sl_rtl_cs_deinit#

enum sl_rtl_error_code sl_rtl_cs_deinit (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the libitem to be deinitialized

Deinitialize a libitem instance of the CS estimator.

Returns


sl_rtl_cs_set_algo_mode#

enum sl_rtl_error_code sl_rtl_cs_set_algo_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_algo_mode mode)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_algo_mode[in]mode

Estimator mode as sl_rtl_cs_algo_mode

Set the estimation algorithm mode.

Returns

Set the estimation mode. For example, SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC sets medium filtering. For further description of the modes, see the documentation of::sl_rtl_cs_algo_mode. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_cs_mode#

enum sl_rtl_error_code sl_rtl_cs_set_cs_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_mode main_mode, const sl_rtl_cs_mode sub_mode)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_mode[in]main_mode

main_mode as sl_rtl_cs_mode

const sl_rtl_cs_mode[in]sub_mode

sub_mode as sl_rtl_cs_mode

Set the estimation CS mode.

Returns

Set the desired CS mode for main and sub modes. For example, SL_RTL_CS_MODE_PBR uses round-trip phase based cs_mode. Sub mode should be set to SL_RTL_CS_MODE_NONE if only main mode is enabled in CS ranging. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_cs_params#

enum sl_rtl_error_code sl_rtl_cs_set_cs_params (sl_rtl_cs_libitem * item, const sl_rtl_cs_params * parameters)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_params *[in]parameters

cs_params as sl_rtl_cs_params

Set the estimation CS parameters.

Returns

Set the parameters for the estimator. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_create_estimator#

enum sl_rtl_error_code sl_rtl_cs_create_estimator (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

Create an estimator with the given parameters after initializing the libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_estimator_param#

enum sl_rtl_error_code sl_rtl_cs_set_estimator_param (sl_rtl_cs_libitem * item, const sl_rtl_cs_estimator_param * param)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

const sl_rtl_cs_estimator_param *[in]param

Data structure with the CS algorithm parameter to be set

Set CS algorithm parameters. The function can be called any time before or during the processing calls.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_process#

enum sl_rtl_error_code sl_rtl_cs_process (sl_rtl_cs_libitem * item, const uint8_t num_procedures, const sl_rtl_cs_procedure * procedure_data)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

const uint8_t[in]num_procedures

Number of procedures in the procedure_data array

const sl_rtl_cs_procedure *[in]procedure_data

Data structure with the completed CS procedures

Calculate distance estimate based on CS procedures.

Returns

Calculate the distance estimate from the given procedure data. The function can be called with multiple procedures. Use sl_rtl_cs_get_distance to fetch the latest distance estimate. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_type estimate_type, const sl_rtl_cs_distance_estimate_mode estimate_mode, float * distance)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_type[in]estimate_type

Type of distance estimate

const sl_rtl_cs_distance_estimate_mode[in]estimate_mode

Mode of distance estimate

float *[out]distance

Distance out in meters.

Get distance estimate

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate_confidence#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_confidence (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, const sl_rtl_cs_distance_estimate_confidence_mode confidence_mode, float * confidence)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_confidence_type[in]confidence_type

Type of confidence estimate

const sl_rtl_cs_distance_estimate_confidence_mode[in]confidence_mode

Mode of confidence estimate

float *[out]confidence

Confidence between 0.0 - 1.0 (unlikely - likely) of the estimated distance

Get distance estimate confidence.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate_extended_info#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_extended_info (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float * extended_info)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_extended_info_type[in]extended_info_type

Type of distance estimate extended information

float *[out]extended_info

Extended info value depending on the extedended_info_type selection

Get distance estimate extended information.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_log_enable#

enum sl_rtl_error_code sl_rtl_cs_log_enable (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

Enable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_log_disable#

enum sl_rtl_error_code sl_rtl_cs_log_disable (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

Disable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_log_add_timestamp#

enum sl_rtl_error_code sl_rtl_cs_log_add_timestamp (sl_rtl_cs_libitem * item, const struct timespec timestamp)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Epoch time

const struct timespecN/Atimestamp

Add epoch time to RTL logging data. This function logs a timestamp entry to enhance the logging data. The timestamp should be recorded at the time of receiving the first subevent from the radio. If measurements are stopped and restarted, this function must be invoked again to log a new timestamp.

Returns


sl_rtl_cs_log_get_instance_id#

enum sl_rtl_error_code sl_rtl_cs_log_get_instance_id (sl_rtl_cs_libitem * item, uint8_t * instance_id)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

uint8_t *[out]instance_id

Instance ID of the given CS libitem

Get the instance ID of the given CS libitem.

Returns


Macro Definition Documentation#

SL_RTL_CS_PCT_IQ_BIT_LEN#

#define SL_RTL_CS_PCT_IQ_BIT_LEN
Value:
12

Number of bits used for indicating I or Q sample in the phase correction term (PCT) in CS step data.


SL_RTL_CS_STEP_MODE_BIT_LEN#

#define SL_RTL_CS_STEP_MODE_BIT_LEN
Value:
8

Number of bits used for indicating step mode in CS step data.


SL_RTL_CS_CHANNEL_MAP_SIZE#

#define SL_RTL_CS_CHANNEL_MAP_SIZE
Value:
10

Size of the channel map in bytes.