Public Attributes#

uint32_t

Number of frequencies, 0xFFFFFFFF or 0 if invalid. In case of invalid input, the previously estimated distance shall be returned.

int32_t *

Array of RSSI values from device 1, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.

int32_t *

Array of RSSI values from device 2, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.

int32_t *

Array of time measurements from device 1, enter INVALID_TIME_VALUE for any unavailable time measurement.

int32_t *

Array of time measurements from device 2, enter INVALID_TIME_VALUE for any unavailable time measurement.

Public Attribute Documentation#

num_time_stamps#

uint32_t sl_rtl_abr_rtt_data::num_time_stamps

Number of frequencies, 0xFFFFFFFF or 0 if invalid. In case of invalid input, the previously estimated distance shall be returned.


Definition at line 749 of file /mnt/raid/workspaces/ws.SvQSsephX/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

rssi_d1#

int32_t* sl_rtl_abr_rtt_data::rssi_d1

Array of RSSI values from device 1, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.


Definition at line 750 of file /mnt/raid/workspaces/ws.SvQSsephX/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

rssi_d2#

int32_t* sl_rtl_abr_rtt_data::rssi_d2

Array of RSSI values from device 2, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.


Definition at line 751 of file /mnt/raid/workspaces/ws.SvQSsephX/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

time_d1#

int32_t* sl_rtl_abr_rtt_data::time_d1

Array of time measurements from device 1, enter INVALID_TIME_VALUE for any unavailable time measurement.


Definition at line 752 of file /mnt/raid/workspaces/ws.SvQSsephX/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

time_d2#

int32_t* sl_rtl_abr_rtt_data::time_d2

Array of time measurements from device 2, enter INVALID_TIME_VALUE for any unavailable time measurement.


Definition at line 753 of file /mnt/raid/workspaces/ws.SvQSsephX/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h