Public Attributes#

uint32_t *

Tones that shall be ignored when making a distance estimation.

num_tones elements, null ptr means not used

num_tones elements, null ptr means not used

float *

Array of device 1 I components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.

float *

Array of device 1 Q components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.

float *

Array of device 2 I components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.

float *

Array of device 2 Q components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.

Public Attribute Documentation#

blank_tone_indices#

uint32_t* sl_rtl_abr_rtp_data::blank_tone_indices

Tones that shall be ignored when making a distance estimation.


Definition at line 763 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

num_blank_tone_indices#

uint32_t sl_rtl_abr_rtp_data::num_blank_tone_indices

Definition at line 764 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

tone_qualities_d1#

enum sl_rtl_abr_tone_quality* sl_rtl_abr_rtp_data::tone_qualities_d1

num_tones elements, null ptr means not used


Definition at line 765 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

tone_qualities_d2#

enum sl_rtl_abr_tone_quality* sl_rtl_abr_rtp_data::tone_qualities_d2

num_tones elements, null ptr means not used


Definition at line 766 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

i_samples_d1#

float* sl_rtl_abr_rtp_data::i_samples_d1

Array of device 1 I components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.


Definition at line 767 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

q_samples_d1#

float* sl_rtl_abr_rtp_data::q_samples_d1

Array of device 1 Q components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.


Definition at line 768 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

i_samples_d2#

float* sl_rtl_abr_rtp_data::i_samples_d2

Array of device 2 I components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.


Definition at line 769 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

q_samples_d2#

float* sl_rtl_abr_rtp_data::q_samples_d2

Array of device 2 Q components, enter INVALID_PCT_VALUE for any unavailable PCT measurement.


Definition at line 770 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h