Public Attributes#

bool

If false, all the antenna values are undefined.

uint32_t

Radio channel for the last packet.

float

Apparent supplemental tone frequency.

float

Reference period signal to noise and distortion ratio.

float

Estimated antenna switching clock jitter.

Public Attribute Documentation#

data_available#

bool sl_rtl_clib_iq_sample_qa_dataset_t::data_available

If false, all the antenna values are undefined.


Definition at line 200 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

curr_channel#

uint32_t sl_rtl_clib_iq_sample_qa_dataset_t::curr_channel

Radio channel for the last packet.


Definition at line 201 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

ref_freq#

float sl_rtl_clib_iq_sample_qa_dataset_t::ref_freq

Apparent supplemental tone frequency.


Definition at line 202 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

ref_sndr#

float sl_rtl_clib_iq_sample_qa_dataset_t::ref_sndr

Reference period signal to noise and distortion ratio.


Definition at line 203 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

switching_jitter#

float sl_rtl_clib_iq_sample_qa_dataset_t::switching_jitter

Estimated antenna switching clock jitter.


Definition at line 206 of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h