Channel Sounding (CS)#

Channel Sounding.

Distances are calculated by following the steps below:

  1. Initialize a sl_rtl_cs_libitem instance.

  2. Set up the algorithm mode and CS parameters.

  3. Create the estimator.

  4. Process the CS procedure data into distance.

  5. Get distance and/or likeliness estimates.

Enumerations#

enum
SL_RTL_CS_ROLE_INITIATOR = 0
SL_RTL_CS_ROLE_REFLECTOR
}
enum
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC = 0
SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY = 1
}
enum
SL_RTL_CS_MODE_CALIBRATION = 0
SL_RTL_CS_MODE_RTT = 1
SL_RTL_CS_MODE_PBR = 2
}
enum
SL_RTL_CS_RTT_TYPE_AAONLY = 0
SL_RTL_CS_RTT_TYPE_SS_32BIT = 1
SL_RTL_CS_RTT_TYPE_SS_96BIT = 2
}
enum
SL_RTL_LAST_KNOWN_DISTANCE = 0
SL_RTL_RANGE_MIN = 1
SL_RTL_RANGE_MAX = 2
SL_RTL_REF_TX_POWER = 3
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED = 0
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS = 0
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE = 0
}

Typedefs#

typedef void *

CS library item.

Functions#

typedef(struct { uint32_t max_number_of_frequencies;uint32_t delta_f;}) sl_rtl_cs_params
typedef(struct { uint8_t num_antenna_paths;uint8_t channel_map_repetition;uint32_t main_mode_repetition;uint8_t num_calib_steps;uint8_t T_PM_time;uint8_t T_IP1_time;uint8_t T_IP2_time;uint8_t T_FCS_time;uint8_t channel_selection_type;uint8_t ch3c_shape;uint8_t ch3c_jump;uint32_t subevent_len;uint8_t subevents_per_event;uint16_t subevent_interval;uint16_t event_interval;uint16_t procedure_interval;uint16_t procedure_count;uint8_t cs_sync_phy;sl_rtl_cs_rtt_type rtt_type :8;uint16_t acl_connection_interval;}) sl_rtl_cs_config
typedef(union { float last_known_distance;float range_min;float range_max;float ref_tx_power;}) sl_rtl_cs_estimator_param_value
typedef(struct { sl_rtl_cs_estimator_param_type type :8;sl_rtl_cs_estimator_param_value value;}) sl_rtl_cs_estimator_param
typedef(struct { uint8_t packet_quality;uint8_t packet_rssi;uint8_t packet_antenna;int16_t measured_freq_offset;}) sl_rtl_cs_mode_calib_data
typedef(struct { uint8_t packet_quality;uint8_t packet_nadm;int8_t packet_rssi;int16_t packet_rtt;uint8_t packet_antenna;}) sl_rtl_cs_mode_rtt_data
typedef(struct { uint8_t antenna_permutation_index;1(struct tone { int32_t pct_i:SL_RTL_CS_PCT_IQ_BIT_LEN;int32_t pct_q:SL_RTL_CS_PCT_IQ_BIT_LEN;uint8_t quality_indicator;}) tones[SL_RTL_CS_TONE_ARRAY_LEN];}) sl_rtl_cs_mode_pbr_data
typedef(struct { sl_rtl_cs_mode step_mode :SL_RTL_CS_STEP_MODE_BIT_LEN;uint8_t step_channel;uint8_t step_data_length;1(union { sl_rtl_cs_mode_calib_data mode_calib_step;sl_rtl_cs_mode_rtt_data mode_rtt_step;sl_rtl_cs_mode_pbr_data mode_pbr_step;});}) sl_rtl_cs_step_data
typedef(struct { uint64_t subevent_timestamp_ms;int16_t frequency_compensation;int8_t reference_power_level;uint8_t num_steps;uint16_t step_data_count;uint8_t *step_data;}) sl_rtl_cs_subevent_data
typedef(struct { sl_rtl_cs_config cs_config;uint8_t initiator_subevent_data_count;sl_rtl_cs_subevent_data *initiator_subevent_data;uint8_t reflector_subevent_data_count;sl_rtl_cs_subevent_data *reflector_subevent_data;}) sl_rtl_cs_procedure
typedef(struct { struct timespec timestamp;uint64_t timestamp_ms;}) sl_rtl_cs_log_params
sl_rtl_cs_init(sl_rtl_cs_libitem *item)
sl_rtl_cs_deinit(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_algo_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_algo_mode mode)
sl_rtl_cs_set_cs_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_mode cs_mode)
sl_rtl_cs_set_cs_params(sl_rtl_cs_libitem *item, const sl_rtl_cs_params *parameters)
sl_rtl_cs_create_estimator(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_estimator_param(sl_rtl_cs_libitem *item, const sl_rtl_cs_estimator_param *param)
sl_rtl_cs_process(sl_rtl_cs_libitem *item, const uint8_t procedure_count, const sl_rtl_cs_procedure *procedure_data)
sl_rtl_cs_get_distance_estimate(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_type estimate_type, float *distance)
sl_rtl_cs_get_distance_estimate_confidence(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, float *confidence)
sl_rtl_cs_get_distance_estimate_extended_info(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float *extended_info)
sl_rtl_cs_log_enable(sl_rtl_cs_libitem *item, const sl_rtl_cs_log_params *log_params)
sl_rtl_cs_log_disable(sl_rtl_cs_libitem *item)
uint8_t
sl_rtl_cs_log_get_instance_id(sl_rtl_cs_libitem *item)

Macros#

#define
SL_RTL_CS_PCT_IQ_BIT_LEN 12

Number of bits used for indicating I or Q sample in the phase correction term (PCT) in CS step data.

#define
SL_RTL_CS_STEP_MODE_BIT_LEN 8

Number of bits used for indicating step mode in CS step data.

#define
SL_RTL_CS_TONE_ARRAY_LEN 2

Array length of tones in CS step data. This is calculated as number of antenna paths + 1. Note: Currently, RTL library supports only single antenna path.

Enumeration Documentation#

sl_rtl_cs_role#

sl_rtl_cs_role
Enumerator
SL_RTL_CS_ROLE_INITIATOR

Initiator role.

SL_RTL_CS_ROLE_REFLECTOR

Reflector role.


sl_rtl_cs_algo_mode#

sl_rtl_cs_algo_mode
Enumerator
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC

Suitable for real-time tracking.

SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY

Suitable for ranging between static objects with high-accuracy.


sl_rtl_cs_mode#

sl_rtl_cs_mode
Enumerator
SL_RTL_CS_MODE_CALIBRATION

Calibration mode with no distance estimation enabled.

SL_RTL_CS_MODE_RTT

Round-trip time based estimation (RTT).

SL_RTL_CS_MODE_PBR

Round-trip phase based estimation (PBR).


sl_rtl_cs_rtt_type#

sl_rtl_cs_rtt_type
Enumerator
SL_RTL_CS_RTT_TYPE_AAONLY
SL_RTL_CS_RTT_TYPE_SS_32BIT
SL_RTL_CS_RTT_TYPE_SS_96BIT

sl_rtl_cs_estimator_param_type#

sl_rtl_cs_estimator_param_type
Enumerator
SL_RTL_LAST_KNOWN_DISTANCE

Last known distance from the user, if more recent than the last CS measurement.

SL_RTL_RANGE_MIN

Minimum limit for the distance estimation range.

SL_RTL_RANGE_MAX

Maximum limit for the distance estimation range.

SL_RTL_REF_TX_POWER

Reference RSSI value of the TX-device at 1.0 m distance in dBm. Default value is -45.0 dBm.


sl_rtl_cs_distance_estimate_type#

sl_rtl_cs_distance_estimate_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI

sl_rtl_cs_distance_estimate_confidence_type#

sl_rtl_cs_distance_estimate_confidence_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE

Bit error rate is only supported for RTT with RTT types SS_32BIT and SS_96BIT.


sl_rtl_cs_distance_estimate_extended_info_type#

sl_rtl_cs_distance_estimate_extended_info_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE

Estimation progress in percentage.

  • Range: 0 to 100.


Typedef Documentation#

sl_rtl_cs_libitem#

typedef void* sl_rtl_cs_libitem

CS library item.


Function Documentation#

typedef#

typedef (struct { uint32_t max_number_of_frequencies;uint32_t delta_f;} )
Parameters
TypeDirectionArgument NameDescription
struct { uint32_t max_number_of_frequencies;uint32_t delta_f;}N/A

typedef#

typedef (struct { uint8_t num_antenna_paths;uint8_t channel_map_repetition;uint32_t main_mode_repetition;uint8_t num_calib_steps;uint8_t T_PM_time;uint8_t T_IP1_time;uint8_t T_IP2_time;uint8_t T_FCS_time;uint8_t channel_selection_type;uint8_t ch3c_shape;uint8_t ch3c_jump;uint32_t subevent_len;uint8_t subevents_per_event;uint16_t subevent_interval;uint16_t event_interval;uint16_t procedure_interval;uint16_t procedure_count;uint8_t cs_sync_phy;sl_rtl_cs_rtt_type rtt_type :8;uint16_t acl_connection_interval;} )
Parameters
TypeDirectionArgument NameDescription
struct { uint8_t num_antenna_paths;uint8_t channel_map_repetition;uint32_t main_mode_repetition;uint8_t num_calib_steps;uint8_t T_PM_time;uint8_t T_IP1_time;uint8_t T_IP2_time;uint8_t T_FCS_time;uint8_t channel_selection_type;uint8_t ch3c_shape;uint8_t ch3c_jump;uint32_t subevent_len;uint8_t subevents_per_event;uint16_t subevent_interval;uint16_t event_interval;uint16_t procedure_interval;uint16_t procedure_count;uint8_t cs_sync_phy;sl_rtl_cs_rtt_type rtt_type :8;uint16_t acl_connection_interval;}N/A

typedef#

typedef (union { float last_known_distance;float range_min;float range_max;float ref_tx_power;} )
Parameters
TypeDirectionArgument NameDescription
union { float last_known_distance;float range_min;float range_max;float ref_tx_power;}N/A

typedef#

typedef (struct { sl_rtl_cs_estimator_param_type type :8;sl_rtl_cs_estimator_param_value value;} )
Parameters
TypeDirectionArgument NameDescription
struct { sl_rtl_cs_estimator_param_type type :8;sl_rtl_cs_estimator_param_value value;}N/A

typedef#

typedef (struct { uint8_t packet_quality;uint8_t packet_rssi;uint8_t packet_antenna;int16_t measured_freq_offset;} )
Parameters
TypeDirectionArgument NameDescription
struct { uint8_t packet_quality;uint8_t packet_rssi;uint8_t packet_antenna;int16_t measured_freq_offset;}N/A

typedef#

typedef (struct { uint8_t packet_quality;uint8_t packet_nadm;int8_t packet_rssi;int16_t packet_rtt;uint8_t packet_antenna;} )
Parameters
TypeDirectionArgument NameDescription
struct { uint8_t packet_quality;uint8_t packet_nadm;int8_t packet_rssi;int16_t packet_rtt;uint8_t packet_antenna;}N/A

typedef#

typedef (struct { uint8_t antenna_permutation_index;1(struct tone { int32_t pct_i:SL_RTL_CS_PCT_IQ_BIT_LEN;int32_t pct_q:SL_RTL_CS_PCT_IQ_BIT_LEN;uint8_t quality_indicator;}) tones[SL_RTL_CS_TONE_ARRAY_LEN];} )
Parameters
TypeDirectionArgument NameDescription
struct { uint8_t antenna_permutation_index;1(struct tone { int32_t pct_i:SL_RTL_CS_PCT_IQ_BIT_LEN;int32_t pct_q:SL_RTL_CS_PCT_IQ_BIT_LEN;uint8_t quality_indicator;}) tones[SL_RTL_CS_TONE_ARRAY_LEN];}N/A

typedef#

typedef (struct { sl_rtl_cs_mode step_mode :SL_RTL_CS_STEP_MODE_BIT_LEN;uint8_t step_channel;uint8_t step_data_length;1(union { sl_rtl_cs_mode_calib_data mode_calib_step;sl_rtl_cs_mode_rtt_data mode_rtt_step;sl_rtl_cs_mode_pbr_data mode_pbr_step;});} )
Parameters
TypeDirectionArgument NameDescription
struct { sl_rtl_cs_mode step_mode :SL_RTL_CS_STEP_MODE_BIT_LEN;uint8_t step_channel;uint8_t step_data_length;1(union { sl_rtl_cs_mode_calib_data mode_calib_step;sl_rtl_cs_mode_rtt_data mode_rtt_step;sl_rtl_cs_mode_pbr_data mode_pbr_step;});}N/A

typedef#

typedef (struct { uint64_t subevent_timestamp_ms;int16_t frequency_compensation;int8_t reference_power_level;uint8_t num_steps;uint16_t step_data_count;uint8_t *step_data;} )
Parameters
TypeDirectionArgument NameDescription
struct { uint64_t subevent_timestamp_ms;int16_t frequency_compensation;int8_t reference_power_level;uint8_t num_steps;uint16_t step_data_count;uint8_t *step_data;}N/A

typedef#

typedef (struct { sl_rtl_cs_config cs_config;uint8_t initiator_subevent_data_count;sl_rtl_cs_subevent_data *initiator_subevent_data;uint8_t reflector_subevent_data_count;sl_rtl_cs_subevent_data *reflector_subevent_data;} )
Parameters
TypeDirectionArgument NameDescription
struct { sl_rtl_cs_config cs_config;uint8_t initiator_subevent_data_count;sl_rtl_cs_subevent_data *initiator_subevent_data;uint8_t reflector_subevent_data_count;sl_rtl_cs_subevent_data *reflector_subevent_data;}N/A

typedef#

typedef (struct { struct timespec timestamp;uint64_t timestamp_ms;} )
Parameters
TypeDirectionArgument NameDescription
struct { struct timespec timestamp;uint64_t timestamp_ms;}N/A

sl_rtl_cs_init#

enum sl_rtl_error_code sl_rtl_cs_init (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the libitem to be initialized

Initialize the CS libitem instance.

Returns


sl_rtl_cs_deinit#

enum sl_rtl_error_code sl_rtl_cs_deinit (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the libitem to be deinitialized

Deinitialize a libitem instance of the CS estimator.

Returns


sl_rtl_cs_set_algo_mode#

enum sl_rtl_error_code sl_rtl_cs_set_algo_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_algo_mode mode)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_algo_mode[in]mode

Estimator mode as sl_rtl_cs_algo_mode

Set the estimation algorithm mode.

Returns

Set the estimation algorithm mode. For further description of the modes, see the documentation of::sl_rtl_cs_algo_mode. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_cs_mode#

enum sl_rtl_error_code sl_rtl_cs_set_cs_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_mode cs_mode)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_mode[in]cs_mode

cs_mode as sl_rtl_cs_mode

Set the estimation CS mode.

Returns

Set the desired cs_mode. For example, SL_RTL_CS_MODE_PBR uses round-trip phase based cs_mode. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_cs_params#

enum sl_rtl_error_code sl_rtl_cs_set_cs_params (sl_rtl_cs_libitem * item, const sl_rtl_cs_params * parameters)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_params *[in]parameters

cs_params as ::sl_rtl_cs_params

Set the estimation CS parameters.

Returns

Set the parameters for the estimator. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_create_estimator#

enum sl_rtl_error_code sl_rtl_cs_create_estimator (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

Create an estimator with the given parameters after initializing the libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


sl_rtl_cs_set_estimator_param#

enum sl_rtl_error_code sl_rtl_cs_set_estimator_param (sl_rtl_cs_libitem * item, const sl_rtl_cs_estimator_param * param)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

const sl_rtl_cs_estimator_param *[in]param

Data structure with the CS algorithm parameter to be set

Set CS algorithm parameters. The function can be called any time before or during the processing calls.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_process#

enum sl_rtl_error_code sl_rtl_cs_process (sl_rtl_cs_libitem * item, const uint8_t procedure_count, const sl_rtl_cs_procedure * procedure_data)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized and configured CS libitem

const uint8_t[in]procedure_count

Number of procedures in the procedure_data array

const sl_rtl_cs_procedure *[in]procedure_data

Data structure with the completed CS procedures

Calculate distance estimate based on CS procedures.

Returns

Calculate the distance estimate from the given procedure data. The function can be called with multiple procedures. Use sl_rtl_cs_get_distance to fetch the latest distance estimate. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_type estimate_type, float * distance)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_type[in]estimate_type

Type of distance estimate

float *[out]distance

Distance out in meters.

Get distance estimate

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate_confidence#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_confidence (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, float * confidence)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_confidence_type[in]confidence_type

Type of confidence estimate

float *[out]confidence

Confidence between 0.0 - 1.0 (unlikely - likely) of the estimated distance

Get distance estimate confidence.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_get_distance_estimate_extended_info#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_extended_info (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float * extended_info)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the initialized CS libitem

const sl_rtl_cs_distance_estimate_extended_info_type[in]extended_info_type

Type of distance estimate extended information

float *[out]extended_info

Extended info value depending on the extedended_info_type selection

Get distance estimate extended information.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


sl_rtl_cs_log_enable#

enum sl_rtl_error_code sl_rtl_cs_log_enable (sl_rtl_cs_libitem * item, const sl_rtl_cs_log_params * log_params)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

const sl_rtl_cs_log_params *[in]log_params

Pointer to the log initialisation parameters

Enable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED.


sl_rtl_cs_log_disable#

enum sl_rtl_error_code sl_rtl_cs_log_disable (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

Disable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED.


sl_rtl_cs_log_get_instance_id#

uint8_t sl_rtl_cs_log_get_instance_id (sl_rtl_cs_libitem * item)
Parameters
TypeDirectionArgument NameDescription
sl_rtl_cs_libitem *[in]item

Pointer to the CS libitem

Get the instance ID of the given CS libitem.

Returns

  • Instance ID of the given CS libitem. The value 0 is returned, if the libitem is not initialized.