Locator item which contains the position and orientation of the locator array.
Public Attributes#
float
X-axis coordinate of the locator.
float
Y-axis coordinate of the locator.
float
Z-axis coordinate of the locator.
float
X-axis rotation of the locator (Euler angles) in degrees.
float
Y-axis rotation of the locator (Euler angles) in degrees.
float
Z-axis rotation of the locator (Euler angles) in degrees.
Public Attribute Documentation#
coordinate_x#
float sl_rtl_loc_locator_item::coordinate_x
X-axis coordinate of the locator.
Definition at line
1308
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
coordinate_y#
float sl_rtl_loc_locator_item::coordinate_y
Y-axis coordinate of the locator.
Definition at line
1309
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
coordinate_z#
float sl_rtl_loc_locator_item::coordinate_z
Z-axis coordinate of the locator.
Definition at line
1310
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
orientation_x_axis_degrees#
float sl_rtl_loc_locator_item::orientation_x_axis_degrees
X-axis rotation of the locator (Euler angles) in degrees.
Definition at line
1311
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
orientation_y_axis_degrees#
float sl_rtl_loc_locator_item::orientation_y_axis_degrees
Y-axis rotation of the locator (Euler angles) in degrees.
Definition at line
1312
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
orientation_z_axis_degrees#
float sl_rtl_loc_locator_item::orientation_z_axis_degrees
Z-axis rotation of the locator (Euler angles) in degrees.
Definition at line
1313
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h