Utility Functionality#
Utility Functionality.
These functions provide supporting functionality such as conversions, additional filtering, diagnostics, and setup functions.
Enumerations#
Typedefs#
Utility library item.
Functions#
Enumeration Documentation#
sl_rtl_util_parameter#
sl_rtl_util_parameter
Util parameter.
Enumerator | |
---|---|
SL_RTL_UTIL_PARAMETER_AMOUNT_OF_FILTERING | Amount of filtering in range [0.0f, 1.0f]. |
1842
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
Typedef Documentation#
sl_rtl_util_libitem#
typedef void* sl_rtl_util_libitem
Utility library item.
1839
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
Function Documentation#
sl_rtl_util_init#
enum sl_rtl_error_code sl_rtl_util_init (sl_rtl_util_libitem * item)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the libitem to be initialized |
Initialize the Util libitem instance.
Returns
SL_RTL_ERROR_SUCCESS if successful
1852
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_deinit#
enum sl_rtl_error_code sl_rtl_util_deinit (sl_rtl_util_libitem * item)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the libitem to be deinitialized |
Deinitialize a Util libitem instance.
Returns
SL_RTL_ERROR_SUCCESS if successful
1860
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_set_parameter#
enum sl_rtl_error_code sl_rtl_util_set_parameter (sl_rtl_util_libitem * item, enum sl_rtl_util_parameter parameter, float value)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
enum sl_rtl_util_parameter | [in] | parameter | Parameter to change |
float | [in] | value | Value of the parameter |
Set util parameters.
Returns
SL_RTL_ERROR_SUCCESS if successful
1870
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_filter#
enum sl_rtl_error_code sl_rtl_util_filter (sl_rtl_util_libitem * item, float value_in, float * value_out)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
float | [in] | value_in | Value to be fed to the filter |
float * | [out] | value_out | Pointer to the filtered value |
Filter a value using the moving average.
Returns
SL_RTL_ERROR_SUCCESS if successful
1880
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_rssi2distance#
enum sl_rtl_error_code sl_rtl_util_rssi2distance (float tx_power, float rssi, float * distance_out)
Type | Direction | Argument Name | Description |
---|---|---|---|
float | [in] | tx_power | Reference RSSI value of the TX-device at 1.0 m distance in dBm, for example -45.0f |
float | [in] | rssi | Measured RSSI from the receiver |
float * | [out] | distance_out | Distance in meters |
Convert an RSSI-value to distance in meters.
Returns
SL_RTL_ERROR_SUCCESS if successful
1890
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_setup#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_setup (sl_rtl_util_libitem * item, uint32_t level, uint32_t num_antennas, bool raw_samples)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | level | Analysis level |
uint32_t | [in] | num_antennas | The number of antennas in the array |
bool | [in] | raw_samples | Data contains raw samples instead of picked ones |
Set up the IQ sample quality analysis.
Returns
SL_RTL_ERROR_SUCCESS if successful
1901
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_set_parameters#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_parameters (sl_rtl_util_libitem * item, uint32_t sample_rate, uint8_t sample_offset, uint8_t samples_in_slot, uint8_t number_of_channels)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | sample_rate | The sampling rate |
uint8_t | [in] | sample_offset | The offset for the picked sample in the sampling slot |
uint8_t | [in] | samples_in_slot | Number of samples in the sampling slot |
uint8_t | [in] | number_of_channels | Number of radio channels |
Set up parameters for the IQ sample quality analysis.
Returns
SL_RTL_ERROR_SUCCESS if successful
1913
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_set_downsampling_factor#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_downsampling_factor (sl_rtl_util_libitem * item, float dsf)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
float | [in] | dsf | The downsampling factor |
Set up IQ sample QA downsampling ratio.
Set the downsampling factor used during the antenna samples (related to the sampling rate of the reference period)
Returns
SL_RTL_ERROR_SUCCESS if successful
1925
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_set_data_offset#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_data_offset (sl_rtl_util_libitem * item, uint32_t offset)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | offset | The data samples' offset |
Set data samples offset.
Set the offset for the data samples from the start of the reference period. The use of this function is optional and, if not given, the default values are used.
Returns
SL_RTL_ERROR_SUCCESS if successful
1938
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_set_switch_pattern#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_switch_pattern (sl_rtl_util_libitem * item, uint32_t size, uint32_t * pattern)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | size | The size of the switch pattern |
uint32_t * | [in] | pattern | Array of integers representing the switch pattern |
Set the switch pattern for the IQ sample quality.
Returns
SL_RTL_ERROR_SUCCESS if successful
1948
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_add_reference#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_add_reference (sl_rtl_util_libitem * item, uint32_t num_samples, float * i_samples, float * q_samples)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | num_samples | The size of data |
float * | [in] | i_samples | I-part of the sample data |
float * | [in] | q_samples | Q-part of the sample data |
Feed the IQ sample quality analysis the reference period data.
Returns
SL_RTL_ERROR_SUCCESS if successful
1959
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_add_data#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_add_data (sl_rtl_util_libitem * item, uint32_t num_snapshots, float ** i_samples, float ** q_samples, uint8_t channel)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint32_t | [in] | num_snapshots | The size of the data |
float ** | [in] | i_samples | I-part of the sample data |
float ** | [in] | q_samples | Q-part of the sample data |
uint8_t | [in] | channel | Radio channel the packet is using. |
Feed the IQ sample quality analysis the antenna data.
Returns
SL_RTL_ERROR_SUCCESS if successful
1970
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_get_results#
uint32_t sl_rtl_util_iq_sample_qa_get_results (sl_rtl_util_libitem * item)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
Get the overall results of the IQ sample quality analysis.
Returns
Bitmask of the failing tests, zero if everything passed
1979
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_get_details#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_get_details (sl_rtl_util_libitem * item, sl_rtl_clib_iq_sample_qa_dataset_t * iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t * antenna_data)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
sl_rtl_clib_iq_sample_qa_dataset_t * | [out] | iq_sample_qa_results | The data structure with data related to the previous data packet |
sl_rtl_clib_iq_sample_qa_antenna_data_t * | [out] | antenna_data | The array of antenna-specific results |
Get the detailed results of the IQ sample quality analysis.
Returns
SL_RTL_ERROR_SUCCESS if successful
1989
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_get_channel_details#
enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_get_channel_details (sl_rtl_util_libitem * item, uint8_t channel, sl_rtl_clib_iq_sample_qa_dataset_t * iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t * antenna_data)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_rtl_util_libitem * | [in] | item | Pointer to the initialized Util libitem |
uint8_t | [in] | channel | Radio channel to show results for. |
sl_rtl_clib_iq_sample_qa_dataset_t * | [out] | iq_sample_qa_results | The data structure with data related to the last data packet using the requested channel |
sl_rtl_clib_iq_sample_qa_antenna_data_t * | [out] | antenna_data | The array of antenna specific results |
Get the detailed results of the IQ sample quality analysis for the specified radio channel.
Returns
SL_RTL_ERROR_SUCCESS if successful
2000
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_iq_sample_qa_code2string#
char * sl_rtl_util_iq_sample_qa_code2string (char * buf, int size, uint32_t code)
Type | Direction | Argument Name | Description |
---|---|---|---|
char * | [in] | buf | Buffer for the results to be written |
int | [in] | size | Size of the buffer |
uint32_t | [in] | code | The results previously received from the sl_rtl_util_iq_sample_qa_get_results() |
Write the IQ sample quality analysis code as human readable strings in the provided buffer.
Returns
pointer to the buffer containing data, or to a constant string
2010
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h
sl_rtl_util_validate_bluetooth_cs_channel_map#
enum sl_rtl_error_code sl_rtl_util_validate_bluetooth_cs_channel_map (const sl_rtl_cs_mode cs_mode, const sl_rtl_cs_algo_mode algo_mode, const uint8_t channel_map)
Type | Direction | Argument Name | Description |
---|---|---|---|
const sl_rtl_cs_mode | [in] | cs_mode | Channel sounding mode (see the CS API) |
const sl_rtl_cs_algo_mode | [in] | algo_mode | Channel sounding algorithm mode (see the CS API) |
const uint8_t | [in] | channel_map | Bluetooth channel bitmap to validate |
Validate Bluetooth channel map for Channel Sounding (CS) measurement based on the user input parameters. The function will return SL_RTL_ERROR_SUCCESS if the requested channel map is compatible with the algorithm and the selected mode settings. Otherwise an error will be returned. This function does not check for any Bluetooth-related constraints (for example skipping of the advertisement channels).
Returns
SL_RTL_ERROR_SUCCESS if successful
2025
of file /mnt/raid/workspaces/ws.PnjKN2fAf/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h