Public Attribute Documentation#

num_antenna_paths#

uint8_t sl_rtl_cs_config::num_antenna_paths

Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.


channel_map_repetition#

uint8_t sl_rtl_cs_config::channel_map_repetition

main_mode_repetition#

uint32_t sl_rtl_cs_config::main_mode_repetition

Number of main modes repeated from previous subevent (0, 1, 2, 3).


num_calib_steps#

uint8_t sl_rtl_cs_config::num_calib_steps

T_PM_time#

uint8_t sl_rtl_cs_config::T_PM_time

T_IP1_time#

uint8_t sl_rtl_cs_config::T_IP1_time

T_IP2_time#

uint8_t sl_rtl_cs_config::T_IP2_time

T_FCS_time#

uint8_t sl_rtl_cs_config::T_FCS_time

channel_selection_type#

uint8_t sl_rtl_cs_config::channel_selection_type

ch3c_shape#

uint8_t sl_rtl_cs_config::ch3c_shape

ch3c_jump#

uint8_t sl_rtl_cs_config::ch3c_jump

subevent_len#

uint32_t sl_rtl_cs_config::subevent_len

subevents_per_event#

uint8_t sl_rtl_cs_config::subevents_per_event

subevent_interval#

uint16_t sl_rtl_cs_config::subevent_interval

event_interval#

uint16_t sl_rtl_cs_config::event_interval

procedure_interval#

uint16_t sl_rtl_cs_config::procedure_interval

procedure_count#

uint16_t sl_rtl_cs_config::procedure_count

cs_sync_phy#

uint8_t sl_rtl_cs_config::cs_sync_phy

rtt_type#

sl_rtl_cs_rtt_type sl_rtl_cs_config::rtt_type

acl_connection_interval#

uint16_t sl_rtl_cs_config::acl_connection_interval