AI-Assisted Project#
Use Simplicity AI SDK and your configured Model Context Protocol (MCP) servers to create and work with an AI-assisted project.
Prerequisites#
Complete the Installation Overview for your operating system and IDE, or complete the equivalent setup for your agent.
Visual Studio Code or Cursor with an AI agent enabled.
A supported Silicon Labs board connected to your PC, if you plan to build and flash.
Generate an Example Project#
Generate your first AI-assisted example project with a simple prompt. For example:
Generate a simple BLE example into my current workspace that is compatible with the board that I have connected to my PC.
Bluetooth Low Energy (BLE) examples are a common starting point for wireless projects.
Modify the Project#
Explain what you want to implement in natural language as clearly as you can. For example:
Modify the project so that the onboard LED is blinking with a 1s interval when no device is connected, and it turns on continuously when a BLE device is connected to it. When disconnected, the LED should start blinking again.
Ask Questions#
Use the agent to inspect hardware and wiring. For example:
How much RAM does my currently connected board have?
To which PINs should I connect my I2C temperature sensor on the board that I have connected?
Inter-Integrated Circuit (I2C) is a common interface for sensors.
Start Debugging#
Start a debug session when you hit runtime errors. For example:
I am getting an assertion error when a BLE device is attempting to connect. Start a debug session and locate the issue. Prompt me to connect to the device to reproduce the issue.
Iterate on the Output#
Ask the agent to explain findings and fixes. For example:
Elaborate on the issue you identified. What was the root cause? Why did your modifications resolve the issue?