Mfg917 Commands#

Note: Since Simplicity Commander version 1.16.3, the manufacturing keyword has been changed to mfg917. The manufacturing alias is still available, but it is considered deprecated and may therefore be removed without notice in any future release of Simplicity Commander.

Simplicity Commander provides tools for provisioning SiWx91x devices with initial configuration and keys for signing/encryption. The tools are suitable for use in a manufacturing setting and can be used to write and read data to and from regions related to both M4 and NWP(TA) cores.

For writing/erasing manufacturing data, or running the key provisioning processes (including its initialization), Simplicity Commander depends on custom RAM code being loaded to the device. Loading this code can be skipped by providing the --skipload flag. This option must only be provided if you are completely certain that the RAM code is already loaded and running on your device, and the use of the --skipload flag is therefore generally discouraged.

In case an external flash configuration is used, the flash pinset index can be set using the --pinset option.

For configuring radio-/network co-processor (RCP/NCP) devices, Simplicity Commander communicates via a proprietary serial protocol to an interface device, which in turn communicates with the RCP/NCP device via serial peripheral interface (SPI) or secure digital input output (SDIO) commands. In this case, Simplicity Commander requires that you also provide the --serialinterface option along with the --device option. In case you are running multiple mfg917 commands in sequence and without resetting the target device in between, you may also provide the --skipinit option to skip initializing the target device's SPI/SDIO interface.

Note: mfg917 commands are currently only supported on SiWx917 devices.

List Available Memory Regions#

Simplicity Commander can be used to read/write/erase certain memory regions, including but not limited to:

  • M4 and NWP (TA) master boot records (MBR)

  • Efuse

  • Boot descriptors

  • Keys

  • User data

To see the available memory regions on your device as well as their ability for producing JSON output, provide the --list option with either of the commands read, write, or erase.

Command Line Syntax

$ commander mfg917 read|write|erase --list

Command Line Input Example

$ commander mfg917 read --list

This command line lists all available memory regions that can be read using the manufacturing commands.

Command Line Output Example

Region name          JSON supported   Description
bfc                  No               Bootloader firmware controller
certs                No               Certificates
efuse                Yes              Efuse
efusecopy            Yes              Efuse copy
efuseipmu            Yes              Efuse intelligent power management unit
keydesctable         No               Key descriptor table
m4efusemapversioncf  No               M4 Efuse map version (common flash)
m4efusemapversiondf  No               M4 Efuse map verion (dual flash)
m4fmccf              No               M4 core flash memory controller (common flash)
m4fmcdf              No               M4 core flash memory controller (dual flash)
m4ipmucf             Yes              M4 core intelligent power management unit (common flash)
m4ipmudf             Yes              M4 core intelligent power management unit (dual flash)
m4mbrcf              Yes              M4 core master boot record (common flash)
m4mbrdf              Yes              M4 core master boot record (dual flash)
m4ptinfocf           No               M4 production information (common flash)
m4ptinfodf           No               M4 production information (dual flash)
pufactkey            No               PUF activation key
rompatch             No               ROM patches
signature            No               Signature
statickeys           No               Static keys
storeconf            No               Store configuration
tafmc                No               NWP flash memory controller
tafwimg              No               NWP firmware image
taipmu               Yes              NWP core intelligent power management unit
tambr                Yes              NWP core master boot record
userdata             No               User data
DONE

Read Memory Region Data From Device#

The read data can be output to the terminal or saved to a raw binary file. For supported regions, the output data can also be stored in a human-readable JSON file. If JSON output is supported and desired, provide an output filename with '.json' extension. If you want to read the region data from a certain offset relative to the start address of that region, you can provide that offset using the --position option.

Command Line Syntax

$ commander mfg917 read <region> [--out <filename> --position <offset>]

Command Line Input Example

$ commander mfg917 read tambr --out device-mbr.json

This command line reads the tambr region of the device and stores the data output to the file 'device-mbr.json' in JSON format.

Command Line Output Example

Reading data from region: tambr
Reading 496 bytes from 0x04000000
Writing JSON...
Manufacturing data saved to file 'device-mbr.json'
DONE

Read Specific Fields From Memory Region#

If you are interested in reading only certain data fields from a JSON-supported region, singular values can be extracted by providing the --property option along with which field and/or sub-field to read from. The --property option can be provided multiple times, and the fields/sub-fields are given on the format field:sub-field. If you provide only the field name for a data field that also contains named sub-fields, all the sub-fields will be included in the output.

If JSON output is supported and desired, provide an output filename with '.json' extension to store the selected fields in a JSON file.

Command Line Syntax

$ commander mfg917 read <region> [--out <filename>] [--property <field name[:sub-field name]>]

Command Line Input Example

$ commander mfg917 read tambr --property m4_clk_configs --property flash_size --property psram_misc_configs:spi_mode

This command line reads the selected fields from the tambr region of the device.

Command Line Output Example

Reading data from region: tambr
Reading 496 bytes from 0x04000000
flash_size = 64
m4_clk_configs:clk_source = 0
m4_clk_configs:div_factor = 0
psram_misc_configs:spi_mode = 2
DONE

Read Address Range From Device#

Arbitrary address ranges (except any addresses inside the Efuse/OTP area) can be read from the device by omitting the region name and instead providing the --range option. The --range option accepts input as either <startaddress:endaddress> or as <startaddress:+length>. Hexadecimal values can be provided using the '0x' prefix.

Command Line Syntax

$ commander mfg917 read --range <startaddress>:[<endaddress> OR +<length>]

Command Line Input Example

$ commander mfg917 read --range 0x04000002:+13

This command line reads 13 bytes from the target device from start address 0x04000002 and prints the data to the console.

Command Line Output Example

Reading data from range 0x04000002:0x0400000F...
{address:  0  1  2  3  4  5  6  7  8  9  A  B  C  D  E  F}
04000000: -- -- 00 00 38 02 00 00 A8 72 EB 28 31 7A 03 --
DONE

Write Memory Region Data to Device#

Manufacturing data that is to be written to a memory region of the device must be provided in either binary format (.s37 and .hex also supported), or, for eligible memory regions, as a JSON file.

Note: Proceed with caution when writing manufacturing data to your device; writing unsupported/erroneous data/configurations may result in your device being rendered unrecoverable!

If the provided data is a binary file, the data is written to the device verbatim.

If a JSON file is provided, the region data is instead updated; the memory region is first read from the device, and the fields present in the JSON file are then used to update the corresponding region data. Lastly, the updated region data is written back to the device. If applicable, Simplicity Commander will by default also update the region's CRCs/integrity checks when changes have been made. This can be omitted by providing the --nocrc option.

If you want to write the data starting from a certain offset relative to the start address of that region, you can provide that offset using the --position option. This is only supported if you are writing binary data; not if you are providing a JSON file.

The --dryrun flag can be added to output the new region data to the terminal instead of writing it to the device.

This command provides no safeguards as to what data is written to the device; it is generally not recommended to write TA (NWP) MBR data to the device using this command; use the mfg917 provision command for that instead.

Command Line Syntax

$ commander mfg917 write <region> --data <filename> [--pinset <index>] [--position <offset>] [--skipload] [--nocrc] [--dryrun]

Command Line Input Example

$ commander mfg917 write tambr --data mbr-updates.json

This command line writes an updated tambr to the device by first reading the tambr region of the device, applying the changes from the fields provided in the 'mbr-updates.json' JSON file, and finally writing this updated tambr data back to the device.

Command Line Output Example

Reading 496 bytes from 0x00400000...
Reading JSON...
Writing data to region: tambr
<process output shortened for documentation>
Data loaded successfully
Region 'tambr' was successfully written to device.
DONE

Write Data to Address#

Simplicity Commander supports writing data to arbitrary memory addresses (except addresses inside Efuse/OTP areas and MBR regions) by omitting the region name and instead providing the --address option. If you are providing an .s37 or .hex-formatted data file, the --address option is ignored and Commander will instead infer the address from the address encoded in the data file.

Command Line Syntax

$ commander mfg917 write --data <filename> [--address <address>]

Command Line Input Example

$ commander mfg917 write --data data.bin --address 0x043F7000

This command line will write the contents of 'data.bin' to address 0x043F7000.

Command Line Output Example

Parsing file data.bin...
Writing data to range 0x047CF000:0x047CF020
<process output shortened for documentation>
Data was successfully written to device.
DONE

Erase Memory Region Data From Device#

Simplicity Commander can be used to erase the data in a memory region, using the mfg917 erase command.

If you want to erase the region data starting from a certain offset relative to the start address of that region, you can provide that offset using the --position option.

Command Line Syntax

$ commander mfg917 erase <region> [--position <offset>] [--pinset <index>] [--skipload]

Command Line Input Example

$ commander mfg917 erase efusecopy

This command line erases the contents in the efusecopy region of the device.

Command Line Output Example

Writing data to region: efusecopy
<process output shortened for documentation>
Data loaded successfully
Region 'efusecopy' was successfully erased.
DONE

Erase Address Range From Device#

Simplicity Commander supports erasing arbitrary memory ranges (except addresses inside Efuse/OTP areas and MBR regions) by omitting the region name and instead providing the --range option.

The --range option accepts input as either <startaddress:endaddress> or as <startaddress:+length>. Hexadecimal values can be provided using the '0x' prefix.

Command Line Syntax

$ commander mfg917 erase --range <startaddress>:[<endaddress> OR +<length>]

Command Line Input Example

$ commander mfg917 erase --range 0x047CF000:+32

This command line starts erases a 32 byte range starting from address 0x047CF000.

Command Line Output Example

Erasing data in range 0x047CF000:0x047CF020...
<process output shortened for documentation>
Range was successfully erased.
DONE

Dump Configuration Data of Device#

Simplicity Commander supports dumping all data regions containing configuration data to a zip archive, using the mfg917 dump command.

Note: For zip file compression functionality, the mfg917 dump command requires Microsoft PowerShell version 5.0 or above on Windows, and the zip and unzip system utilities on Linux/Mac

Command Line Syntax

$ commander mfg917 dump <zip archive filename>

Command Line Input Example

$ commander mfg917 dump device_data.zip

This command line reads and dumps all data regions containing configuration data into the 'device_data.zip' archive file.

Command Line Output Example

Reading 40960 bytes from 0x0400f000
Reading 184320 bytes from 0x047cf000
Reading 1024 bytes from 0x40012000
Reading 1024 bytes from 0x040003e0
Reading 58 bytes from 0x40012181
Reading 88 bytes from 0x04000300
Reading 496 bytes from 0x04000000
Reading 1024 bytes from 0x041c0000
Reading 496 bytes from 0x04000000
Reading 58 bytes from 0x041b0258
Reading 496 bytes from 0x04000000
Reading 496 bytes from 0x041b0000
Reading 496 bytes from 0x04000000
Reading 3 bytes from 0x041b0292
Reading 1192 bytes from 0x04002000
Reading 200 bytes from 0x04000238
Reading 72 bytes from 0x040001f0
Reading 4096 bytes from 0x04005000
Reading 3072 bytes from 0x04010400
Reading 1024 bytes from 0x04010000
Reading 58 bytes from 0x04000561
Reading 496 bytes from 0x04000000
Zip archive created at "path/to/device_data.zip".
DONE

Initialize PUF And Generate Activation Code#

To enable security features (encryption/MIC integrity check/signing) on your SiWx917 device, the device's PUF first needs to be initialized and an activation code must be generated on the device. This can be done via the mfg917 init command.

Providing an NWP (TA) MBR binary file using --mbr is optional. The file specifies the destination address for the activation code. If required, you can update the NWP MBR by providing a JSON file using --mbrdata. If you omit --mbr, Commander uses the default activation code address. To use the default NWP MBR for your device, specify --mbr 'default' and provide the device part number using --device.

Note: After the mfg917 init command has been run, the device needs to be power cycled for any changes to take effect.

Command Line Syntax

$ commander mfg917 init [--mbr <filename|'default'>] [--mbrdata <filename>] [--pinset <index>] [--skipload]

Command Line Input Example

$ commander mfg917 init --mbr default --device SiWG917M111LGTBA

This command line initializes the device's PUF and generates an activation code, using a default NWP MBR for the device part number 'SiWG917M111LGTBA'.

Command Line Output Example

Using default MBR for SiWG917M111LGTBA...
<process output shortened for documentation>
Activation code generated successfully
DONE

Provision Security Keys to the Device#

Provisioning device keys is done using the mfg917 provision command, by providing a key configuration JSON file containing the keys you want to store on your device with the --keys option. Supported keys for storing on the device are M4/NWP (TA) public keys and M4/NWP OTA keys. In addition, a private attestation key is required for the provisioning sequence.

If you don't want to provision any keys during the provisioning sequence, the --keys option may be omitted.

If required, you can update the NWP MBR before writing it to the device by providing a JSON file using the --mbrdata option.

Note: After the mfg917 provision command has been run, the device needs to be power cycled for any changes to take effect.

Command Line Syntax

$ commander mfg917 provision --keys <filename> [--mbr <filename|'default'>] [--mbrdata <filename>] [--pinset <index>] [--skipload]

Command Line Input Example

$ commander mfg917 provision --keys keys.json

This command line provisions the keys contained in the JSON file 'keys.json' to the device.

Command Line Output Example

Reading MBR from the connected device...
Found valid activation code address in MBR: 0x00002000
Intrinsic keys generated successfully.
Programming NWP OTA Key...
Key successfully stored
Programming M4 OTA Key...
Key successfully stored
Programming NWP Public Key...
Key successfully stored
Programming M4 Public Key...
Key successfully stored
Programming attestation Key...
Key successfully stored
Programming NWP MBR...
Data loaded successfully
Programming key descriptor table...
Data loaded successfully
DONE

Provision OTP Security Keys to the Device#

Provisioning one-time programmable (OTP) keys is done using the mfg917 provisionotpkeys command. Symmetric (AES) and public (ECDSA) keys can be provided via the --symmetrickey and --publickey options, respectively. These keys can be used later for enabling MIC and signature-based write protection of the device configuration (see Protection Device Configuration).

The symmetric key must be provided as a .bin file, or as a hex-encoded string in a .txt file. The public key must be provided as a DER-formatted binary file (.der), or as a .pem file. Alternatively, both options accept a key configuration JSON file, as long as the relevant OTP keys are available in the JSON file.

Note: Writing OTP keys is a permanent action and cannot be reverted.

Command Line Syntax

$ commander mfg917 provisionotpkeys [--symmetrickey <filename>] [--publickey <filename>] [--noprompt]

Command Line Input Example

$ commander mfg917 provisionotpkeys --symmetrickey aeskey.bin --publickey key.pem

This command line reads the symmetric key 'aeskey.bin' and the public key 'key.pem' and writes them into the OTP of the device.

Command Line Output Example

Reading OTP symmetric key from file 'aeskey.bin'...
Reading OTP public key from file 'key.pem'...
The provided data can be applied to the current Efuse.
Determining which OTP words need updating...
Writing 112 bytes to OTP...
Data was successfully written to the device's OTP.
DONE

Provision NWP MBR and Efuse data to the Device#

Use the mfg917 provision command with the --mbr, --mbrdata, --efuse, and --efusedata options to provision NWP MBR and OTP Efuse data to the device. Silicon Labs recommends using the provision command instead of the write command because it considers both MBR and OTP Efuse data together when updating the device.

The --mbr and --efuse options accept binary files as input, while --mbrdata and --efusedata accept JSON files. Commander applies the changes specified in the JSON files to the corresponding region data before writing it to the device.

If you provide --mbrdata without --mbr, or --efusedata without --efuse, Commander reads the corresponding NWP MBR or OTP Efuse data from the device, applies the changes specified in the JSON file, and writes the updated data back to the device.

Note: If you provide --efuse or --efusedata, the command also writes data to the device's OTP Efuse. This action is permanent and cannot be reversed. You can use --noprompt to skip the confirmation prompt, but use this option with caution.

Command Line Syntax

$ commander mfg917 provision [--mbr <filename|'default'>] [--mbrdata <filename>] [--efuse <filename>] [--efusedata <filename>] [--noprompt]

Command Line Input Example

$ commander mfg917 provision --mbr mbr.bin --mbrdata mbrdata.json --efuse efuse.bin --efusedata efusedata.json

This command provisions the NWP MBR data from mbr.bin and the OTP Efuse data from efuse.bin to the device. Before writing the data to the device, Commander applies the partial updates specified in mbrdata.json and efusedata.json to their corresponding memory regions.

Command Line Output Example

Updating OTP Efuse fields...
Reading JSON...
Updating MBR fields...
Reading JSON...
Loading RAM code (321776 bytes)...
Starting RAM code...
Programming ROM patch...
Data loaded successfully
Programming NWP MBR...
Data loaded successfully
Programming M4 MBR...
Data loaded successfully
Programming IPMU data...
Data loaded successfully
Programming M4 Efuse map version...
Data loaded successfully
Programming OTP Efuse...
Data loaded successfully
DONE

List Available Device Profiles#

Simplicity Commander can be used to store and apply frequently used device configuration JSON files, referred to as 'profiles'. A list of the available profiles can be produced using the mfg917 provision --listprofiles command. Along with this list, the location of user-defined profiles is also shown, including instructions on how to add such custom profiles.

Command Line Syntax

$ commander mfg917 provision --listprofiles

Command Line Input Example

$ commander mfg917 provision --listprofiles

This command line displays the available profiles on your system, along with the location of custom user-defined profiles.

Command Line Output Example

Profile name        Affected regions
enable-secure-boot  efuse, tambr
fallback            tambr
giga                tambr
macronix            tambr
xmc                 tambr
Custom profiles can be added by placing them in the directory at
'/Users/username/Library/Preferences/SiliconLabs/commander/ProfileStore/Si91x/'.
The name of the files must be in the format '<profile name>_<region>.json'.
DONE

The enable-secure-boot profile is a custom profile, and is shown alongside the built-in profiles.

Provision Device Profile to the Device#

Applying a device profile is done through the mfg917 provision command, using the --profile option.

Note: You can only apply TA (NWP) MBR and (OTP) Efuse data through a profile.

You can use profiles to quickly switch between configurations, such as secure and non-secure device configurations, or to apply the same set of changes to multiple devices in a production environment.

You can provide profiles with any combination of the --mbr, --mbrdata, --efuse, and --efusedata options. Commander applies the changes specified in the profiles as the final step before writing the data to the device.

Command Line Syntax

$ commander mfg917 provision --profile <name> [--mbr <filename|'default'>] [--mbrdata <filename>] [--efuse <filename>] [--efusedata <filename>] [--noprompt]

Command Line Input Example

$ commander mfg917 provision --profile enable-secure-boot

This command line applies the custom profile 'enable-secure-boot' to the device's TA (NWP) MBR and OTP Efuse and provisions it to the device.

Command Line Output Example

Using OTP Efuse from the connected device...
Using MBR from the connected device...
Applying profile 'enable-secure-boot' to efuse...
Reading JSON...
Applying profile 'enable-secure-boot' to tambr...
Reading JSON...
The OTP Efuse data has been modified and will be written to the device.
Loading RAM code (321776 bytes)...
Starting RAM code...
Programming ROM patch...
Data loaded successfully
Programming NWP MBR...
Data loaded successfully
Programming M4 MBR...
Data loaded successfully
Programming IPMU data...
Data loaded successfully
Programming M4 Efuse map version...
Data loaded successfully
Programming OTP Efuse...
Data loaded successfully
DONE

Because this command writes OTP data to the device, Commander displays a confirmation prompt. The prompt is omitted from this example for brevity.

Protect Device Configuration#

Simplicity Commander can be used to write-protect the device configuration using the mfg917 protectconfig command. This protection is permanent and is applied over a user-specified length, starting from address 0x04000000 (the start of the NWP (TA) configuration region). Note that only certain protection lengths are supported, ranging from 1024-65536 bytes. Commander will provide suggestions of the nearest allowed lengths if the provided length is not supported.

Two types of protection are available: message integrity check (MIC)-based protection and signature-based protection. MIC-based protection requires a 16 byte AES key as a .bin file or as a hex-encoded string in a .txt file, provided with the --symmetrickey option. Signature-based protection requires a private ECDSA key, either as a DER-formatted binary file (.der), or as a .pem file, provided with the --privatekey option. Alternatively, both options accept a key configuration JSON file, as long as the relevant OTP keys are available in the JSON file.

When enabling signature-based protection, the public key counterpart of the provided private key must be present on the device. If there is no such public key stored in the device, Commander will extract the public key from the provided private key and store it on the device before proceeding.

Note: Enabling configuration protection is permanent and cannot be reverted. Any subsequent attempts at writing new configurations to a protected device will fail and/or may render your device unrecoverable.

Command Line Syntax

$ commander mfg917 protectconfig <protection> --protectlength <length> [--privatekey <filename> --sha <SHA-xxx>] [--symmetrickey <filename>] [--noprompt]

Command Line Input Example

$ commander mfg917 protectconfig mic --protectlength 49152 --symmetrickey key.bin

This command line will enable MIC based protection of 49152 bytes of the device configuration, using 'key.bin' as the key for the MIC computation.

Command Line Output Example

OTP Efuse might not be up to date with the MBR configuration. Copying MBR configuration data into Efuse...
Storing the provided symmetric key in the OTP Efuse...
Computing MIC...
Using default IV...
The provided data can be applied to the current Efuse.
Determining which OTP words need updating...
Writing 68 bytes to OTP...
Data was successfully written to the device's OTP.
DONE

Command Line Input Example

$ commander mfg917 protectconfig signature --protectlength 16384 --privatekey key.pem

This command line enables signature-based protection of the first 16384 bytes of the device configuration, using the private ECDSA key 'key.pem' for generating the signature. The signature is placed at the end of the protected region.

Command Line Output Example

OTP Efuse might not be up to date with the MBR configuration. Copying MBR configuration data into Efuse...
Computing signature...
The provided data can be applied to the current Efuse.
Determining which OTP words need updating...
Writing 128 bytes to OTP...
Data was successfully written to the device's OTP.
DONE

Get Information About Device Configuration#

Key information about the device configuration can be extracted using the mfg917 info command. Simplicity Commander will read certain regions of your device (including the NWP (TA) MBR and the Efuse regions), parse the information, and present key information like the device's MAC address, flash size, and current security parameters.

Command Line Syntax

$ commander mfg917 info

Command Line Input Example

$ commander mfg917 info

This command line extracts information about the current configuration of the target device.

Command Line Output Example

Reading 1024 bytes from 0x040003e0
OPN                                         : SiWG917M111MGTBA
WiFi MAC address                            : 6C5CB1C43F90
BLE MAC address                             : 6C5CB1C43F92
Flash size                                  : 8MB
NWP firmware version                        : 1711.2.10.1.3.0.7
MBR variant                                 : 0x1F (1.8 MB)
Manufacturing SW version                    : 2.4 (36)
Application region start address            : 0x081f0000
Application code start address              : 0x08202000
Application region end address              : 0x0840ffff
Flash configuration                         : Common flash
Mode                                        : SOC
Integrity protection active                 : None
NWP roll-back prevention                    : Disabled
NWP digital signature validation            : Disabled
NWP firmware encryption                     : Disabled
NWP secure boot                             : Disabled
Application roll-back prevention            : Disabled
Application digital signature validation    : Disabled
Application code encryption                 : Disabled
Application secure boot                     : Disabled
DONE

Setting up a Serial Interface Device#

To simplify the setup of supported EFR32 devices as serial interface devices, Simplicity Commander provides the mfg917 setupinterface command. This command flashes the required firmware to the device, enabling it to operate as a serial interface device for communication with an RCP or NCP device over the Serial Peripheral Interface (SPI).

As of this version, the following radio boards are supported as serial interface devices:

  • BRD4118

  • BRD4120

  • BRD4121

  • BRD4186

  • BRD4187

  • BRD4188

  • BRD4197

  • BRD4198

Command Line Syntax

$ commander mfg917 setupinterface

Command Line Input Example

$ commander mfg917 setupinterface

This command line sets up the device as a serial interface device.

Command Line Output Example

Parsing file /path/to/commander/Resources/jlink/Si917/interface_firmware/BRD4187.hex...
Serial interface successfully set up.
DONE