Util Commands#
Key Generation#
Generates a keyfile to be used for encryption and decryption and outputs the keyfile to the specified filename.
Command Line Syntax
$ commander util genkey --type aes-ccm --outfile <filename>
Command Line Input Example
$ commander util genkey --type aes-ccm --outfile key.txt
Command Line Output Example
Using /dev/random for random number generation Gathering sufficient entropy... (may take up to a minute)... DONE
Generating a Signing Key#
Creates an EDCSA-P256 key pair and outputs the result to the specified private and public key files. For more information, see UG266: Silicon Labs Gecko Bootloader User's Guide for GSDK 3.x and Lower or UG489: Silicon Labs Gecko Bootloader User's Guide for GSDK 4.0 and Higher.
Command Line Syntax
$ commander util genkey --type ecc-p256 --privkey <filename> --pubkey <filename> [--tokenfile <filename>]
Command Line Input Example
$ commander util genkey --type ecc-p256 --privkey signing_key.pem --pubkey signing_pubkey.pem
Command Line Output Example
Generating ECC P256 key pair... Writing private key file in PEM format to signing_key.pem Writing public key file in PEM format to signing_pubkey.pem DONE
Key to Token#
Creates a token text file containing an Elliptic Curve Cryptography (ECC) public key suitable for flashing to a device. For more information, see UG266: Silicon Labs Gecko Bootloader User's Guide for GSDK 3.x and Lower or UG489: Silicon Labs Gecko Bootloader User's Guide for GSDK 4.0 and Higher.
Command Line Syntax
$ commander util keytotoken <input file> --outfile <filename>
Command Line Input Example
$ commander util keytotoken my_pubkey.pem --outfile keytokens.txt
Command Line Output Example
Writing EC tokens to keytokens.txt... DONE
Key Config Generation#
Generates a key configuration file to the specified file name. This command is only available for SiWx91x devices, so the device options is required. The output file is used as input to the Provision Security Keys to the Device and Provision OTP Security Keys to the Device command, among others. The file contains the following keys:
ATTESTATION_PRIVATE_KEY
ATTESTATION_PUBLIC_KEY
M4_OTA_KEY
M4_PRIVATE_KEY
M4_PUBLIC_KEY
OTA_KEY
NWP_PRIVATE_KEY
NWP_PUBLIC_KEY
OTP_AES_KEY
OTP_PRIVATE_KEY
OTP_PUBLIC_KEY
Command Line Syntax
$ commander util genkeyconfig --outfile <filename> --device <device>
Command Line Input Example
$ commander util genkeyconfig --outfile keys.json --device Si917
This example generates a file, keys.json, containing the key configuration for a Si917 device.
Command Line Output Example
Generating symmetric key... Generating symmetric key... Generating symmetric key... Generating ECC P256 key pair... Generating ECC P256 key pair... Generating ECC P256 key pair... Generating ECC P256 key pair... Key configuration written to keys.json DONE
Generate Certificate#
The process of signing files can be done using an intermediate certificate. These certificates can be generated with the util gencert command. There are currently two available certificate types: GBL certificates and Secure Boot certificates. If rollback prevention is enabled, the device will not boot if it has seen a certificate with a higher version number. This is set by the --cert-version option. The private key corresponding to the --cert-pubkey is used to sign the image. The certificate may either be signed directly by providing a signing key with the --sign option or unsigned by providing the --extsign option.
Command Line Syntax
$ commander util gencert --cert-type <cert type> --cert-version <version> --cert-pubkey <key file> [--sign <key file>|--extsign] --outfile <filename>
Command Line Input Example
$ commander util gencert --cert-type secureboot --cert-version 1 --cert-pubkey cert_pubkey.pem --sign signing_key.pem --outfile secureboot_cert.bin
In this example, the signing key is provided and the certificate is signed directly.
Command Line Output Example
Successfully signed certificate DONE
Command Line Input Example
$ commander util gencert --cert-type gbl --cert-version 1 --cert-pubkey cert_pubkey.pem --extsign --outfile gbl_cert.bin
In this example, an unsigned certificate is created. The signature for the certificate can be created, for example, by a Hardware Security Module (HSM). The certificate can be signed by passing the unsigned certificate and the HSM generated signature to the util signcert command.
Command Line Output Example
DONE
Sign Certificate#
Sign a certificate with an externally created signature. You can use the optional --verify option to verify the signature by providing the public key corresponding to the private key used to create the signature.
Command Line Syntax
$ commander util signcert <cert filename> --cert-type <type> --signature <signature> [--verify <public key file>] --outfile <filename>
Command Line Input Example
$ commander util signcert gbl_cert.bin.extsign --cert-type gbl --signature gbl_signature.bin --verify signing_pubkey.pem --outfile signed_cert.bin
Command Line Output Example
Successfully verified signature Successfully signed certificate DONE
Verify Signature#
When secure boot is enabled, all code running on the device must be signed. This command can be used as a check to verify that the file was correctly signed, which may help in debugging in case secure boot fails, or as a verification before flashing the image. If the file is signed using an intermediate certificate, the certificate key is used to check the signature of the file. The key given by the --verify option is used to verify the signature of the certificate.
Command Line Syntax
$ commander util verifysign <input file> --verify <public key file>
Command Line Input Example
$ commander util verifysign my_application.bin --verify signing_pubkey.pem
Command Line Output Example
Parsing file my_application.bin... Found application properties at 0x00000e78 Found certificate in image at location 0x0000b3a4 Successfully verified certificate signature with verification key. Using certificate key to verify application signature. Found signature at 0x0000b42c Successfully verified application signature. DONE
Application Information#
Get all available information about an application by parsing the ApplicationProperties_t struct in the image. If the file does not have application properties, no information can be extracted from the file.
Command Line Syntax
$ commander util appinfo <filename>
Command Line Input Example
$ commander util appinfo my_application.bin
Command Line Output Example
Parsing file my_application.bin... Found application properties in image. Application properties info: Signature location : 0x0000b42c Signature type : ECDSA-P256 Long token section address : Not set (0x00000000) Application data info: If rollback prevention is enabled, the device will not boot if the device has seen an application with a higher version number. App type : The application is an MCU application App version : 0x00000000 Product ID : 0x53455f555047524144455f4150500000 Application certificate info: If rollback prevention is enabled, the device will not boot if the device has seen a certificate with a higher version number. Certificate located at : 0x0000b3a4 Certificate version : 0x00000001 Certificate key : 0x249919c28b28156f19d2e03379b968c8a931aa9b195258e2741da28b686983dd71d0140e9a7b0d7e39de43f592163b8aa38d4e0871f5d2d88b57556dbe87f89b Certificate signature : 0x013f2adc310f10f1426db74b503f3612a46ab85c7ce86c967eb965b10f7d24267101192513d9481c49c0eb0b61c1f73392cc6f6d1cd1209a9d58e761884aac4e DONE
Print Section Header Information from an ELF File#
Parse and print the section header information from an Executable and Linkable Format (ELF) file.
Command Line Syntax
$ commander util elfinfo <filename>
Command Line Input Example
$ commander util elfinfo my_bootloader.out
Displays section header information of ELF file my_bootloader.out.
Command Line Output Example
Index Name Size Address Type 1 .shstrtab 0x00000111 0x00000000 STRTAB 2 .strtab 0x0001e169 0x00000000 STRTAB 3 .symtab 0x000243a0 0x00000000 SYMTAB 4 HEADERS 0x000000ac 0x00000000 PROGBITS 5 APP ro 0x0002ddf4 0x00000200 PROGBITS 6 SIMEE&LOCKBITS 0x00009000 0x000f7000 NOBITS 7 ResetHeap 0x00001490 0x20000000 NOBITS 8 Guard 0x00000030 0x20001490 NOBITS 9 APP rw 0x00002148 0x2003dce0 NOBITS 10 .debug_abbrev 0x00006325 0x00000000 PROGBITS 11 .debug_aranges 0x000037ac 0x00000000 PROGBITS 12 .debug_frame 0x0003a2f5 0x00000000 PROGBITS 13 .debug_info 0x00063435 0x00000000 PROGBITS 14 .debug_line 0x00064f5c 0x00000000 PROGBITS 15 .debug_loc 0x00010fe3 0x00000000 PROGBITS 16 .debug_macinfo 0x00009941 0x00000000 PROGBITS 17 .debug_pubnames 0x00007132 0x00000000 PROGBITS 18 .debug_ranges 0x00003778 0x00000000 PROGBITS 19 .iar.debug_frame 0x00015349 0x00000000 PROGBITS 20 .iar.debug_line 0x00020199 0x00000000 PROGBITS 21 .comment 0x001d394a 0x00000000 PROGBITS 22 .iar.rtmodel 0x00000032 0x00000000 PROGBITS 23 .ARM.attributes 0x0000002e 0x00000000 DONE
Get RAM and Flash Usage of an ELF Application#
Calculate the static RAM usage and the flash storage usage of an application from an Executable and Linkable Format (ELF) file, and print usage details of the RAM sections.
To also report the available RAM and flash and their usage as a percentage of the total available memory, provide one or more of the following: a map file using --map, a linker script using --linkerscript, or a device part number using --device. If you provide multiple options, Commander uses the first valid source in the following order:
If you provide a valid map file using
--map, Commander uses the available RAM and flash sizes specified in the map file.If you provide a valid linker script using
--linkerscript, Commander uses the available RAM and flash sizes specified in the linker script.If you specify a device part number using
--device, Commander connects to the device to determine the available RAM and flash sizes.
Note: Any changes you might have introduced to the memory regions on your specific device will not be reflected if you are using the
--deviceoption.
Command Line Syntax
$ commander util usage <filename> [--map <filename>] [--linkerscript <filename>] [--device <device part no.>] [--include-section <ELF section>] [--exclude-section <ELF section>]
Command Line Input Example
$ commander util usage my_elf.out --map my_mapfile.map
Command Line Output Example
Ram usage : 262144 / 262144 B (100.00 %) .bss : 3344 B ( 1.28 %) .data : 152 B ( 0.06 %) .heap : 254552 B ( 97.10 %) .stack : 4096 B ( 1.56 %) Flash usage : 23884 / 1564672 B ( 1.53 %) DONE
Print Header Information of an RPS File#
Parse and print the information contained in the header of an RPS file. The printed information includes (but is not limited to) security settings, signature data, bootloader instructions, flash address, image type, and image size. If the provided RPS file is a combined RPS image, the data for all constituent images is printed sequentially. If the image is encrypted, the bootloader instructions will be unavailable.
RPS files for on-device key upgrades are also supported by this command.
Command Line Syntax
$ commander util rpsinfo <filename>
Command Line Input Example
$ commander util rpsinfo image.rps
This command line prints the information contained in the header of 'image.rps'.
Command Line Output Example
RPS application image Application info: Combined image bit set : No Image type : TA application Image size : 0x001986A0 (1672864 B) Flash address : 0x00011000 Firmware version : 0x020101BF Firmware version ext. : 0x1610ABFF Counter : 0x00000000 (0) PSRAM : No Security settings: Integrity check : CRC CRC : 0x844D33FA (2219652090) Encrypted : No Signed : No Boot descriptor info: Boot desc. offset : 0x0080 IVT offset : 0x00000000 3 boot descriptor entries found: Length : 0x000140 (320) Destination : 0x00000000 Length : 0x000CFC (3324) Destination : 0x00000B04 Length : 0x01A984 (108932) Destination : 0x0000E948 DONE