Simplicity Machine Learning Version 1.2.0-beta Release Notes (Oct 14, 2026)#

The Artificial Intelligence and Machine Learning (AI/ML) tools include Simplicity Machine Learning, the model graph viewer, and the model converter. Use these tools to prepare, convert, quantize, and profile models on the host system.

Release Summary#

Key Features | Bug Fixes | Chip Enablement

Key Features#

Added in 1.2.0-beta#

  • Added model quantization, including full integer (INT8) quantization using calibration data.

  • Added the sml-compile CLI and sml.compile() Python API for compiling TFLite models.

  • Added Ultralytics YOLO model support to the ML Model Converter.

Added in 1.1.0#

  • The "ML Profiler" tool was renamed to "Simplicity Machine Learning".

  • Added an option to choose kernels when profiling a model.

  • Improved central processing unit (CPU) and accelerator cycle counts in the profiler.

  • Added a model graph viewer to Simplicity Machine Learning based on Model Explorer.

  • Added an alpha release of the ML Model Converter to convert PyTorch and Open Neural Network Exchange (ONNX) models to TensorFlow Lite (TFLite).

Bug Fixes#

Fixed in 1.2.0-beta#

  • Fixed a Windows issue when resolving the Silicon Labs Device Manager executable.

  • Fixed missing Ultralytics and PyTorch dependencies in the packaged model converter.

  • Added a clear error message when the model selected for profiling is not in TFLite format.

Fixed in 1.1.0#

None.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable application programming interfaces (APIs), examples, software variants, modes, hardware, and host interfaces for each feature.

New Features#

Added in 1.2.0-beta#

  • Model quantization: Added quantization support to model conversion, including full INT8 quantization using calibration data. Calibration files can be selected from the GUI or provided through the CLI.

  • Dynamic INT8 conversion: Added an ONNX fallback path for dynamic INT8 conversion of PyTorch models.

  • ML Model Compiler: Added the sml-compile CLI and sml.compile() Python API for compiling TFLite models.

Added in 1.1.0#

  • Simplicity Machine Learning profiler: Renamed from "ML Profiler" to "Simplicity Machine Learning". This host-side tool profiles ML models on target hardware.

  • Kernel selection: Added an option to choose kernels when profiling a model.

  • Model graph viewer: Integrated a model graph viewer in Simplicity Machine Learning based on Model Explorer. Linux and macOS are supported natively; Windows is supported through Windows Subsystem for Linux (WSL).

  • ML Model Converter: Added a unified graphical user interface (GUI) and command-line interface (CLI) to convert PyTorch and ONNX models to TFLite.

  • manifest.json output: When --save-manifest command line argument is passed on the CLI, a manifest.json file is saved with conversion metadata including conversion time, conversion ratio, input shape, and output shape. The GUI generates this file every time.

Enhancements#

Added in 1.2.0-beta#

  • Unified conversion command: Updated the umbrella sml CLI to invoke sml-convert directly for model conversion.

  • Compiler output: Simplified the sml-compile CLI to always stage the compiled model and emit a model header.

  • Compiler workspace cleanup: Restored the clean-workspace CLI option in the sml-compileCLI.

  • Profiling output: Updated the profiler output directory structure.

  • Profiling firmware: Updated Simplicity Machine Learning to use profiling firmware version 1.1.2.

  • Model file handling: Standardized support for .tflite, .pt, .pth, and .onnx model extensions across the GUI and CLI.

Added in 1.1.0#

  • Profiler metrics: Improved CPU and accelerator cycle count reporting in Simplicity Machine Learning.

Removed Features#

Removed in 1.2.0-beta#

None.

Removed in 1.1.0#

None.

Deprecated Features#

Deprecated in 1.1.0#

Deprecated Feature

Planned Removal Date

"ML Profiler" tool

Superseded by Simplicity Machine Learning

The "ML Profiler" tool will not receive any updates. In Simplicity Studio, search for Simplicity Machine Learning (GUI) or Simplicity Machine Learning (CLI).

Bug Fixes#

Fixed in 1.2.0-beta#

  • Fixed a Windows issue by resolving the Silicon Labs Device Manager executable as sdm or sdm.exe, depending on the host operating system.

  • Fixed missing Ultralytics and PyTorch dependencies in the packaged model converter.

  • Added a clear error message when a model selected for profiling is not a .tflite file.

Fixed in 1.1.0#

None.

Chip Enablement#

None.

Known Issues and Limitations#

Refer to the ML Profiler Troubleshooting section for known issues and their solutions.

Refer to the ML Model Converter Troubleshooting section for known issues and their solutions.

  • The model graph viewer is not supported natively on Windows; use WSL to launch the GUI tool.

  • The model converter is not supported natively on Windows; use WSL to launch the GUI tool.

    • ONNX models are converted using onnx2tf. Non-self-contained ONNX models with external weights are rejected with a clear message

    • PyTorch models with dynamic graphs require an explicit input shape input.

    • Full INT8 quantization requires representative calibration data. Provide representative calibration data when using full INT8 quantization.

Installation and Use#

Refer to the Getting Started guide for installation and usage instructions.

For information about Secure Vault Integration, see Secure Vault.

Help and Feedback#

Feature Matrix#

Supported Features | Unsupported Features

Supported Features#

Feature Name Description Quality Related API Names Supported Software Variants, Hardware, Modes, Host Interfaces Related Example Names
ML Model profiler Profile ML models on target hardware. Choose kernels when profiling. Improved CPU and accelerator cycle counts. Beta
  • Host tool
  • EFR32 (BRD2601A, BRD2608A), SiWG917 (BRD2605A)
  • None
Model graph viewer Integrated model graph viewer in Simplicity Machine Learning based on Model Explorer. Beta
  • Host tool (native support for Linux and macOS. Windows supported through WSL)
  • None
ML Model converter Convert PyTorch, Ultralytics YOLO, and ONNX models to TFLite on the host. Supports dynamic INT8 and full INT8 quantization using calibration data, and optional manifest.json output with conversion metadata. Alpha
  • Host tool (native support for Linux and macOS. Windows supported through WSL)
  • None
ML Model compiler Compile TFLite models using a host CLI or Python API. The compiler stages the compiled model and generates a model header. Beta
  • sml-compile
  • sml.compile()
  • Host tool
  • CLI and Python API
  • None
Data capture and visualization tools Communicate with devices, capture data, visualize image and audio data, create synthetic keyword datasets, generate audio features, and train audio classifiers. Beta
  • sml-device-io
  • sml-capture-data
  • sml-visualize-image
  • sml-visualize-audio
  • sml-audio-feature-generator
  • Host CLI tools
  • Audio classifier supported on Windows
  • None

Unsupported Features#

  • The model graph viewer is not supported natively on Windows. Use WSL to launch the GUI tool.

  • The model converter is not supported natively on Windows. Use WSL to launch the GUI tool.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.