Overview and Resources#
Simplicity Studio® 5 (SSv5) offers a number of tools that can be used to test and debug application functionality, power consumption, and network behavior.
Tools include:
The built-in debugger
In addition, a number of SDKs provide example applications that can be used for testing, such as:
NodeTest (Zigbee EmberZNet SDK) (See AN1019: Using the NodeTest Application)
RAILtest (Proprietary Flex SDK) (see UG409: RAILtest User's Guide)
Finally, Silicon Labs provides a number of other documentation resources related to testing such as:
AN1267: Radio Frequency Physical Layer Evaluation in Bluetooth® SDK v3.x
UG104: Testing and Debugging Applications for the Silicon Labs EM35x and EFR32MG Platforms (Zigbee)