Silicon Labs ML SDK Version 2.2.2 - Release Notes (May 4, 2026)#
The Silicon Labs ML SDK is provided as an extension to the Simplicity SDK. It enables AI/ML development on Series 2 (EFR and SiWG917) devices using the Tensorflow Lite for Microcontrollers (TFLM) framework.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 2.2.2#
Improved profiler CPU cycle and inference time calculation on EFR32 platform.
Added in 2.2.1#
Improved calculation of CPU clocks utilization and inference time in ML Model Profiler.
Added in 2.2.0#
New ML Model Profiler helps developers understand the execution performance of their ML models on the target device and within existing applications. It is available in 2 formats:
ML Model Profiler Tool: run
.tflitemodel on Series 2 devices to analyze performance before integration.ML Model Profiler Component: integrate profiling directly within an existing application to capture model performance during normal execution.
New sample applications are available for Profiling ML Models, Data Capture from IMU, and Device Tampering Detection.
Changed sample application names.
Demos for more EFR and SiWG917 boards.
API Changes#
None.
Bug Fixes#
Fixed in 2.2.2#
Fixed arena size calculation for small models with arena < 1 in the ML Model Profiler.
Fixed in 2.2.1#
Fixed firmware built with debug symbols instead of a release build.
Fixed in 2.2.0#
Blink app behaves differently when running on Series 2, compared to SiWG917.
Blink and Voice Control applications now support BRD4338a and similar SiWG917 radio boards.
Flatbuffer converter tool documentation updated to reflect latest changes.
Misleading error on macOS for applications built using software optimizations for ML models.
Removed invalid link to I2S pin configuration for SiWG917 voice-based applications.
Chip Enablement#
Added in 2.2.2#
None.
Added in 2.2.1#
None.
Added in 2.2.0#
EFR32MG24B310F1536IM48
EFR32MG24B210F1536IM48
EFR32MG24B220F1536IM48
EFR32MG26B510F3200IM68
EFR32MG26B410F3200IM48
EFR32MG26B420F3200IM48
EFR32MG26B510F3200IL136
EFR32MG26B410F3200IM68
EFR32MG26B420F3200IM68
EFR32MG26B510F3200IM48
EFR32ZG28B312F1024IM48
EFR32ZG28B312F1024IM68
EFR32ZG28B322F1024IM68
EFR32ZG28B312F1024IM68
SiWG917M111MGTBA
SiWG917M141XGTBA
SiWG917Y111MGNBA
SiWG917Y111MGAB4
SiWG917Y121MGNB4
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces for each feature.
New Features#
Added in 2.2.2#
None.
Added in 2.2.1#
None.
Added in 2.2.0#
New tool, ML Model Profiler, to profile
.tflitemodels. For details, see documentation here. This tool currently only supports EFR devices from the Series 2 family. SiWG917 support is forthcoming.New component, ML Model Profiler, to enable profiling of
.tflitemodels in existing customer applications. Adding the "ML Model Profiler" component to an application or theml-profilercomponent to the.slcpfile of an application will enable this feature. This is not be confused with the ML Model Profiler Tool. This component will eventually be a part of the tool as well. The purpose of keeping this component separate is to allow flexibility to profile ML models in user's existing applications alongside other stacks.New sample applications:
AI/ML - ML Model Profiler Firmware: Profiling ML Models built for Tensorflow Lite for Microcontrollers.
AI/ML - SoC Anomaly Detection for EFR32: Device Tampering Detection by using IMU data and time-series analysis of that data.
AI/ML - SoC Data Capture for EFR32 Baremetal: Data Capture from IMU into a CSV file. This app requires JLink on the user's workstation.
Enhancements#
Added in 2.2.2#
Improved profiler CPU cycle and inference time calculation on EFR32 platform.
Added in 2.2.1#
Improved CPU clocks utilization calculation and inference time in the ML Model Profiler.
Added in 2.2.0#
Changed sample app names from
ml_<app_name>_<platform>pattern toaiml_[sub_technology_]<soc|rcp|ncp|host>_<app_name>_<platform>_<os|baremetal>. This was done to allow quicker segregation of apps based on their capabilities.Pre-built demo binaries are now available for more EFR and SiWG917 boards. Newly added demos are:
BRD2601B
AI/ML - SoC Anomaly Detection EFR32 Baremetal
AI/ML - SoC Data Capture EFR32 Baremetal
AI/ML - SoC Profiler Firmware EFR32 Baremetal
BRD2608A
AI/ML - SoC Anomaly Detection EFR32 Baremetal
AI/ML - SoC Data Capture EFR32 Baremetal
AI/ML - SoC Profiler Firmware EFR32 Baremetal
BRD4186C
AI/ML - SoC Blink EFR32 Baremetal
AI/ML - SoC Model Profiler EFR32 Baremetal
BRD4187C
AI/ML - SoC Blink EFR32 Baremetal
AI/ML - SoC Model Profiler EFR32 Baremetal
BRD4338A
AI/ML - SoC Audio Classifier SiWG917 Baremetal
AI/ML - SoC Blink SiWG917 Baremetal
AI/ML - SoC Model Profiler SiWG917 Baremetal
AI/ML - SoC Voice Control Light SiWG917 Baremetal
BRD4339A
AI/ML - SoC Model Profiler SiWG917 Baremetal
BRD4340B
AI/ML - SoC Model Profiler SiWG917 Baremetal
BRD4342A
AI/ML - SoC Model Profiler SiWG917 Baremetal
BRD4343A
AI/ML - SoC Model Profiler SiWG917 Baremetal
BRD4343B
AI/ML - SoC Model Profiler SiWG917 Baremetal
BRD4343Q
AI/ML - SoC Model Profiler SiWG917 Baremetal
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 2.2.2#
Fixed arena size calculation for small models with arena < 1 in the ML Model Profiler.
Fixed in 2.2.1#
None.
Fixed in 2.2.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1567613 1463269 | Blink app behaves differently when running on Series 2, compared to SiWG917. The LED has a baseline brightness on SiWG917 while blinking but it turns off completely on Series 2. This is due to the different LED driver implementations on the two chip families. | None. |
|
| 1479985 | Blink and Voice Control applications now support BRD4338a and similar SiWG917 radio boards. | None. |
|
| 1438989 | Flatbuffer converter tool documentation updated to reflect latest changes. | None. |
|
| 1479970 | Misleading error on macOS for applications built using software optimizations for ML models. | None. |
|
| 1497650 | Removed invalid link to I2S pin configuration for SiWG917 voice-based applications. | None. |
|
Chip Enablement#
Added in 2.2.2#
None.
Added in 2.2.1#
None.
Added in 2.2.0#
| Chip Family | OPNs / Boards / OPN Combinations | Supported Software Variants (if applicable) | Supported Modes | Supported Host Interfaces |
|---|---|---|---|---|
| Chip |
|
Standard | SoC |
|
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
Added in 2.2.2#
None.
Added in 2.2.1#
None.
Added in 2.2.0#
| Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
AI/ML - ML Model Profiler Firmware |
Profiling ML Models built for Tensorflow Lite for Microcontrollers. | Standard | SoC |
|
|
|
AI/ML - SoC Anomaly Detection for EFR32 |
Device Tampering Detection by using IMU data and time-series analysis of that data. | Standard | SoC |
|
|
|
AI/ML - SoC Data Capture for EFR32 Baremetal |
Data Capture from IMU into a CSV file. This app requires JLink on the user's workstation. | Standard | SoC |
|
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
Refer to the ML Model Profiler Troubleshooting section for known issues and their solutions.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
Improved profiler CPU cycle and inference time calculation on EFR32 platform and fixed arena size calculation for small models with arena < 1 in the ML Model Profiler.
Compatible Software#
| Software | Compatible Version or Variant |
|---|---|
| Software Development Kit (SDK) |
|
Installation and Use#
To upgrade your existing software with the latest features included in this release, update Simplicity Studio to the latest version, Simplicity SDK to v2025.12.3, WiSeConnect SDK to v4.0.2, and ML SDK to v2.2.2 using Studio installation manager. Alternatively, download the SDKs from the links listed in the Compatible Software section above.
To update the ML SDK, see the AI/ML SDK Setup guide.
To run your first demo, see our Getting Started
To kick start your development, see our Developer's Guide
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
To learn more about the software in this release, dive into our online documentation
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
Feature Matrix#
Supported Features | Unsupported Features
Supported Features#
None.
Unsupported Features#
SiWG917 does not use the built-in TensorFlow component directly; instead, support is provided through automatic code generation handled by advanced configurators.
Series 2 devices do not support new software optimizations. However, due to their architecture, they are still at least as efficient as SiWG917.
MVP Compiler is not supported on macOS natively, recommend using a linux container environment.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.